Hello,
We are using a custom board and we are using Gmac0 controller on M core.
We are able to establish communication with the remote node using Gmac0 controller during this time the receive interrupt, GMAC0_CH0_RX_IRQHandler is hitting fine. But after a while the host stops acknowledging to the messages sent by remote node and when we check, at this time the receive interrupt, GMAC0_CH0_RX_IRQHandler is not hitting and the communication is stopping as the host stopped acknowledging to the messages sent by remote node.
Attaching the snippet of canoe trace for reference.
We tried the same activity for transmission via host and we see that the transmission is not stopping and is working fine.
Could you please support us to resolve the issue with the Gmac.
Regards,
Winston Lewis