Start Linux form M7_0 Failed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Start Linux form M7_0 Failed

ソリューションへジャンプ
26,181件の閲覧回数
StanleyShen
Contributor IV

Hi there

Since both start M core(APP) and A core still no good, and refer to the attatched document,

I want to start  Linux form M7_0 bootloader all lone (not include M7 APP).

I did following steps, but there was not any info output from the  UART0,

 

Could you tell me where the problem is?

Prepare images for Cortex-A53 cores

  • 1:download binaries_auto_linux_bsp33.0_s32g2_pfe.tgz and extract it 
  • 2:dd if=binaries_auto_linux_bsp33.0_s32g2_pfe/s32g274ardb2/fsl-image-auto-s32g274ardb2.sdcard of=/dev/sdc bs=1M status=progress && sync
    • (by this, SD mode startup OK)
  • 3:checkout release/bsp33.0-2020.04 and build it
  • 4:checkout arm-trusted-firmware (release/bsp33.0-2.5) and buid it (`FIP_ALIGN := 64` and unset LDFLAS because I had a "aarch64-fsl-linux-ld.bfd: unrecognized option '-Wl,-O1'" error)
  • 5:Build the ATF  and got a fip.32 the address info as blow:
    • IVT Location: SD/eMMC
    • Load address: 0x342fc580
    • Entry point: 0x34302000
  • 6:renew fip.32 

dd if=fip.s32 of=/dev/sdb skip=512 seek=512 iflag=skip_bytes oflag=seek_bytes conv=fsync,notrunc

Prepare bootloader for Cortex-A7_0 core

  • 1:load Integration_Reference_Examples bootloder to EB
  • 2:disable RM Eep MemDal CryptoDal Crypto plugin and releated options
    • (In my Env the SDHC and HSE is still abnormal)
  • 3:Bootloader(…)->Bootloader->General  Software breakpoint enable uncheck
  • 4:boot option like blow:
    • StanleyShen_0-1673437225845.pngStanleyShen_1-1673437237244.pngStanleyShen_2-1673437254729.png
  • 5:generate project and build bootloader.bin
  • 6:Generate S32G Boot Image Using S32DS IVT_TOOL
    • StanleyShen_3-1673437372927.png
  • 7:Deploy the bootloader(with IVT) and fip.32 to QSPI(NOR Flash) with s32ft.exe
    • bootlader 0x0000_0000
    • fip.32 0x0010_0000

After above operations, set RDB2 to QSPI boot mode.

 

 

 

0 件の賞賛
返信
1 解決策
26,009件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

No worries. Before going to debugging the multicore application, we would like to confirm if you can boot-up Linux from NOR Flash using the A53 core. This can be done directly from S32DS and by following Section 4 from AN13750.

The fip file that needs to be modified on the BSP provided by NXP is the fip.s32. The fip.bin is the one that needs to be flashed into NOR Flash. We can say is the "application bootloader" that you flash into the IVT of S32DS for our scenario of booting from A53. This will let us know if your files are working correctly.

Please, let us know.

元の投稿で解決策を見る

0 件の賞賛
返信
28 返答(返信)
3,151件の閲覧回数
StanleyShen
Contributor IV

但是在执行部分,板子的状态应该是SW10-1 ON ,SW10-2 OFF,SW-3 ON,SW4-all OFF(这就以为这是从Nor Flash起)是吗? 还是说,不用这样拨动开关,直接起SW4-7 ON,从SD卡起进入U-boot,然后在通过指令运行app? 

从NorFlash启动,

然后M核的BootLoader会加载fip.bin,然后M核的BootLoader启动A53,

后面就是A53执行fip.bin->u-boot->linux了。

0 件の賞賛
返信
3,717件の閲覧回数
maiwl
Contributor I

好的,谢谢,我想知道你一开始遇到的问题是什么,然后修改哪个地方就调通了?

0 件の賞賛
返信
3,690件の閲覧回数
StanleyShen
Contributor IV

主要就是fip.bin的烧录问题,如果烧写了fip.32那就有问题了

0 件の賞賛
返信
4,079件の閲覧回数
maiwl
Contributor I

我最近按照AN13750的文档进行M核引导A核的操作也遇到同样的问题,希望能得到你的帮助。

0 件の賞賛
返信
4,401件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Good to know you got it working.

As for support, we may recommend talking to your local NXP representative, for them to channel the support for your current region.

As for us knowing, we may not be the correct person, we do apologize for this.

Please, help us reaching your local NXP contact and surely they will find some local support for your project.

0 件の賞賛
返信
4,394件の閲覧回数
StanleyShen
Contributor IV

Hi Daniel 

Thank you very much.

I got it.

Pls allow me to close this issue.

0 件の賞賛
返信
4,377件の閲覧回数
StanleyShen
Contributor IV

- Have you tried (at this point in time) to boot up linux (without M7 into the equation) from NOR Flash?

Yes I did and juest the yesterday's thread, the result as blow, beacuse I didn't burn the zImage to QSPI flash, U-Boot -> Linux start NG, but I think the from NOR Flash start Linux was OK.

 

 

NOTICE:  BL2: v2.5(release):bsp33.0-2.5-dirty
NOTICE:  BL2: Built : 08:08:26, Jan 13 2023
NOTICE:  BL2: Booting BL31


U-Boot 2020.04 (Jan 13 2023 - 16:06:18 +0800)

CPU:   NXP S32G274A rev. 2.0
Model: NXP S32G274A-RDB2
DRAM:  3.5 GiB
MMC:   FSL_SDHC: 0
Loading Environment from SPI Flash... SF: Detected mx25uw51245g with page size 256 Bytes, erase size 64 KiB, total 64 MiB
*** Warning - bad CRC, using default environment

Using external clock for PCIe0, CRNS
Configuring PCIe0 as RootComplex(x2)
Using external clock for PCIe1, CRNS
Frequency 125Mhz configured for PCIe1
Configuring PCIe1 as SGMII(x2) [XPCS0 2.5G, XPCS1 OFF]
Setting PCI Device and Vendor IDs to 0x4002:0x1957
PCIe0: Failed to get link up
Pcie0: LINK_DBG_1: 0x00000000, LINK_DBG_2: 0x00000800 (expected 0x000000d1)
DEBUG_R0: 0x00189900, DEBUG_R1: 0x08200000
PCI: Failed autoconfig bar 20
PCI: Failed autoconfig bar 24
PCIe1: Not configuring PCIe, PHY not configured
In:    serial@401c8000
Out:   serial@401c8000
Err:   serial@401c8000
Board revision: RDB2/GLDBOX Revision D
Net:   EQOS phy: rgmii @ 1

Warning: eth_eqos (eth0) using random MAC address - 12:e8:6d:ee:63:42
eth0: eth_eqos PFE: emac0: sgmii emac1: none emac2: rgmii
## No elf image at address 0xffdc92f8
PFEng firmware file '<NULL>@0x03000000:<NULL>' loading failed: -22

Hit any key to stop autoboot:  0
## No elf image at address 0xffdc9048
PFEng firmware file '<NULL>@0x03000000:<NULL>' loading failed: -22
 PFE: emac0: sgmii emac1: none emac2: rgmii
pfeng_cfg_mode_enable: Invalid PFE device
Booting from flash...
device 0 offset 0x1f0000, size 0xe00000
SF: 14680064 bytes @ 0x1f0000 Read: OK
device 0 offset 0xff0000, size 0x100000
SF: 1048576 bytes @ 0xff0000 Read: OK
device 0 offset 0x10f0000, size 0x2000000
SF: 33554432 bytes @ 0x10f0000 Read: OK
Bad Linux ARM64 Image magic!
=>
=>

 

 

 

 

 

 

 

 

 - From the first point you mentioned "...and fip.32-sdcard to QSPI Flash, the Linux can start normally in QSPI mode." and also "...I hexdumped the  fip.32-sdcard and you can the IVT image is on the 0x1000." we understand you tried this option, but it is not explicitly mentioned.

 - We suspect you got your platform to boot up from the SD (not QSPI), which is expected from the steps you mentioned (and files you used).

Maybe I didn't explain my process in detail enough, in my boot sequence, The used IVT is included in M7_ 0_ Bootloader, not fip, and in M7_ 0_ Bootloader.bin the offset of the IVT image is 0x0.

(means that the fip.32 was called by M7_0 bootloader, not by BOOTROOM)

I don't know if you have read the attachment I added [Enabling Multicore Application on S32G2 .pdf]

the deployment as blow:

StanleyShen_0-1673662355487.png

As I said in before thread, the actual boot flow is:

  • BOOTROM -> M-core bootloader(with IVT in NOR Flash) -> M-core APP

                                 |-------A-core FIP(in NOR Flash but load and start by M-core bootloader) -> A-Core U-Boot(in SD-Card)->A-Core Linux(in SD-Card)

StanleyShen_0-1673684684060.png

 

Therefore, the FIP image must be in SD-Card mode because it needs to read U-boot from SD card.

Please focus on document I was attached [Enabling Multicore Application on S32G2 .pdf]

I refer to this document in depth and have the following differences from it:

1: don't use IPC(both Linux and MCAL)

2:use Uart_TS_T40D11M30I2R0(RTD_4.4_3.0.2) replace to IPCF_Example

3:disable crypto and SDHC on bootloader

So now I'm puzzled why the UART of M-core can start normally, but the U-Boot and Linux of A-core can't start(maybe start OK but can't output to UART...).

Is it the reason that my bootloader does not contain crypto and SDHC?

In addition, I debugged the bootloader and found that FIP was loaded and executed normally without any error

 

bootloader.c
 - main()
   - Bl_Run()
     - Bl_BootApplications()
       - Bl_LoadApplication()
         - Bl_FetchApplication()
           - Bl_LoadAndAuthFromQspi()
             - Bl_StartDmaTransfer()
         // Fetch application image and copy to RAM OK
       - Bl_StartAllApplications()
         - Bl_StartApplication()
           // run FIP image(BL2) OK
         - Bl_StartApplicationOnCurrentCore()
           // run UART sample OK

 

- update CST 2023/01/14 21:43

Just refer to the [Enabling Multicore Application on S32G2 .pdf], I rebuild the bootloader with SDHC and HSE

So, for now, the only difference from the document is that I use UART instead of IPCF to verify M7's actions.

But still work abnormal.

To facilitate understanding, I clean up  my boot flow as blow:

StanleyShen_0-1673703793241.png

 

 

 

 

0 件の賞賛
返信
4,307件の閲覧回数
StanleyShen
Contributor IV

Hi

Can somebody help me ?

0 件の賞賛
返信