Slower LPDDR4

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Slower LPDDR4

2,976件の閲覧回数
Daniel_Wax
NXP Employee
NXP Employee

My customer Cruise is starting an new S32g3 design and they want to use slower speed grade

The S32G399 Reference board has a -053 speed grade LPDDR4 part. But they are planning to use a -46 speed grade part.

 

What needs to change in order to boot linux from this slower LPDDR4?

Or is it mandatory to use a -053 speed grade?

 

Daniel_Wax_0-1643065334371.png

 

0 件の賞賛
返信
2 返答(返信)

2,934件の閲覧回数
Bulat
NXP Employee
NXP Employee

You seem to mix up speed grades, -046 is a faster memory than -053. In that sense -046 is ok of course.

On the other hand the S32G3 supports DDR4LP at up to 3200MT/s speed, both speed grade parts meet this speed. No change in sw setup is required.

Regards,

Bulat

 

0 件の賞賛
返信

2,962件の閲覧回数
Daniel_Wax
NXP Employee
NXP Employee
0 件の賞賛
返信