Sensor compatibility

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Sensor compatibility

1,723 Views
akhil_k_appu
Contributor III

Hi team,

could you please tell me the list of sensors that are compatible with NXP S32G274A (Goldbox) and what type of ECU data is collected by S32G while using inside the vehicle ??.

And also the please suggest the documents that are used to connect the Gold Box with Blue and Green Box for development purposes.

0 Kudos
Reply
2 Replies

1,707 Views
akhil_k_appu
Contributor III

Thank you @Daniel-Aguirre 

0 Kudos
Reply

1,711 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

As for the sensors compatible with S32G274A, this is dependent on what interface the sensor is using and if S32G is compatible with it. S32G is a specialized platform dedicated to communication protocols, having a wide variety of supported protocols.

Related to the ECU data, could be that we are misunderstanding the question, but this is directly related to the application the client needs implemented in the platform. As to the application implemented on the GOLDBOX firmware, we recommend reading through the documentation to understand the behavior of the same.

At this point in time, there is no application note regarding the interconnections between the different boxes that NXP provides, this is a possibility that the customer can implement, but no guidelines are provided by NXP (again, at this point in time).

For a more diverse information regarding S32G2 platform, we recommend to visit the NXP site to review the different application notes given. Below will be a link to this page.

S32G2 Safe and Secure Vehicle Network Processor | NXP Semiconductors

A personal recommendation is to read the Product Brief of S32G2 to understand the capabilities and possibilities of the platform.

Please, let us know if this information was helpful or not.