Scheck - SAF SRAM ECC

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Scheck - SAF SRAM ECC

跳至解决方案
950 次查看
Harish_R
Contributor III

Hi team,

 

I was working on Scheck SRAM test. Test target side i found there are 2 SRAM_ECC like 

SRAM_0_ECC and SRAM_0_ECC_LITE (LITE version provides faster execution time at cost of lower diagnostic coverage (number of test vectors is significantly reduced). i couldnt understand much about this info. so ECC test is like checking memory as per ECC logic (on Single bit error/double bit error) so less diagnostic coverage actually means??

if someone could drop some more information it would be helpful.

 

BR,

Harish R

0 项奖励
回复
1 解答
899 次查看
chenyin_h
NXP Employee
NXP Employee

Hello, @Harish_R 

Thanks fo your post and sorry for late response.

From my understanding, the less diagnostic coverage here may mean that some errors may go unnoticed, and/or some of the noticed fault may not be corrected/handled, which is caused by the number of test vectors is significantly reduced.

 

BR

Chenyin

 

 

在原帖中查看解决方案

0 项奖励
回复
1 回复
900 次查看
chenyin_h
NXP Employee
NXP Employee

Hello, @Harish_R 

Thanks fo your post and sorry for late response.

From my understanding, the less diagnostic coverage here may mean that some errors may go unnoticed, and/or some of the noticed fault may not be corrected/handled, which is caused by the number of test vectors is significantly reduced.

 

BR

Chenyin

 

 

0 项奖励
回复