Safety Sboot CMU FC testing - plugin HFREF and LFREF ref values are not as per the calculations

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Safety Sboot CMU FC testing - plugin HFREF and LFREF ref values are not as per the calculations

2,541 Views
Irshad2225
Contributor III


Hi, 

For CMU_FC_14, CMU_FC_15, and CMU_FC_21, the reference LFREF and HFREF values are too high to match the calculated values.
In sBoot_PtocmuFcArray, LFREF starts with zero.
I have observed that, with the minimum frequency as zero, LFREF can be 3. not zero.

Providing below reference values from the debugger.
sBoot_PtocmuFcArray values - where the calculated HFREF(sBoot_maxFreqsArray ) & LFREF(Boot_minFreqsArray) are being compared with .

image.png

Providing HFREF & LFREF calculations below.

 clock monotorFIRC_CLFFref ~%F ref MHzMonitored clockFmon ~%BusClockF mon,F bus MHz RCCR[REF_CNT]Fmon_var_MaxFmon_var_MinFref_var_MaxFref_var_MinHTCR[HFREF]LTCR[LFREF]
10CMU_FC_14_GMAC0_TX_CLKFXOSC_CLK0.00540GMAC0_TX_CLK5GMAC0_TX_CLK9.68010.089.1240.00239.9982415
11CMU_FC_15_GMAC_TS_CLKFXOSC_CLK0.00540GMAC0_TS_CLK5GMAC0_TS_CLK9.68010.089.1240.00239.9982415
16CMU_FC_21_GMAC0_RX_CLKFXOSC_CLK0.00540GMAC0_RX_CLK5GMAC0_RX_CLK258026.2523.7540.00239.9985644

Above are the HFREF and LFREF values as per my calculations.

Table. Comparison between calculated values vs sBoot_PtocmuFcArray 

Calculated valuessBoot_PtocmuFcArray values
HFREFLFREFHFREFLFREF
2415167772150
2415167772150
5644167772150


The reference values cannot be achieved even with the higher frequencies.

This might not be a calculation issue, as the same formula has been applied to the remaining CMU_FCs and those got passed.

Is this an issue in plugins/configurations???


Tags (5)
0 Kudos
Reply
7 Replies

2,502 Views
Joey_z
NXP Employee
NXP Employee

Hi, Irshad2225

Thank you for contacting us.

Refer to your picture, it is unable for current CMU if the FCE=0. In addition, The REF_CNT value is 0.

BR

Joey

 

0 Kudos
Reply

2,494 Views
Irshad2225
Contributor III
Hi Joey,

Even when the REF_CNT = 100 or 80 is configured, the above-mentioned CMUs' LFREF and HFREF remain the same with REF_CNT=0, only to the CMU_FC_14, CMU_FC_15, and CMU_FC_21.



0 Kudos
Reply

2,492 Views
Irshad2225
Contributor III
I have enabled FCE too, in the code, as it was not getting enabled automatically.
Mentioned in the below thread:
https://community.nxp.com/t5/S32G/Safety-Sboot-CMU-FC-testing-Not-enabling-CMU-FC-check-before/m-p/2...
0 Kudos
Reply

2,491 Views
Irshad2225
Contributor III

Irshad2225_0-1750691808708.png

 

0 Kudos
Reply

2,441 Views
Joey_z
NXP Employee
NXP Employee

hi, Irshad2225

Thank you for your information.

I understand what you mean. Since these API in Safety are for customers to use, in order to better support you in debugging and identifying problems, could you share your code?

You can provide this information easier by creating a new case at: https://support.nxp.com.

Can attach this link: Safety Sboot CMU FC testing - plugin HFREF and LFREF ref values are not as per the calculations - NX... inter to the new ticket. 

BR

Joey

0 Kudos
Reply

2,415 Views
Irshad2225
Contributor III
Hi Joey,

Does sboot require, pheripheral initialisations before testing configurations?.

Below subchapter is mentioned from sboot_UM.pdf.
6.5.1 Function Calls during Start-up
The sBoot software does not require any initialisation function to be called during start.

Regards,
Irshad
0 Kudos
Reply

2,406 Views
Joey_z
NXP Employee
NXP Employee

hi,Irshad2225

Thank you for your information.

According to The manual, The sBoot software does not require any initialization function to be called during start_up. However, Software drivers for the PMIC and it's communication interface must be present in the system and properly initialized before sBoot can start testing the FCCU error output
pins.

Joey_z_0-1750924452355.png

Hope it can help you.

BR

Joey

 

0 Kudos
Reply