SAF-Scheck Ahb Test - s32g3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SAF-Scheck Ahb Test - s32g3

1,587 Views
Harish_R
Contributor III

Hi Team,

im trying to perform Ahb test in sCheck. but the test exits with error.

while debugging i found that while clearing faults. basicaly it checks for error that is report while fualt injection. but the fault is not reported. 

Harish_R_0-1750138213259.png

so this memory w.r.t to cm7Ahbp memory has this issue. other top 4 memory does report error. 

Harish_R_1-1750138315769.png

does it require separate configuration. and the test address mentioned above is like registers address?

if someone could drop some hint it would be helpfull.

BR,

Harish R

Tags (1)
0 Kudos
Reply
4 Replies

1,541 Views
Joey_z
NXP Employee
NXP Employee

hi,

Thank you for contacting us.

Refer to the UM of S32G_SAF_SCHECK_UM.pdf, test accesses the TCM memory using backdoor access for read and write accesses.  sCheck AHB CM7 tests access memory addresses outside the memory sections defined in the Table 62 of S32G_SAF_SCHECK_UM.pdf. See table below to determine address ranges used for AHB CM7 testing.

Joey_z_0-1750233524663.png

Hope it can help you.

BR

Joey

 

0 Kudos
Reply

1,521 Views
Harish_R
Contributor III

Hi @Joey_z 

Thanks for the info!

i have mapped the section of TCM memory through linker. but still, there's the same issue.

i think the AHB test doesn't only perform AHB test but also AXI test. so, address range are proper for AHB bus. as mentioned in the First screenshot earlier.

is it like should be enabled or something. im not sure. if you could provide more information, it would be helpful.

BR,

Harish R

0 Kudos
Reply

1,497 Views
Joey_z
NXP Employee
NXP Employee

hi,Harish_R

Thank you for your reply.

I understand what you mean. Could you share your code or tell me how to reproduce your problem?

You can provide this information easier by creating a new case at https://support.nxp.com. Can attach this link: SAF-Scheck Ahb Test - s32g3 - NXP Community. I will try my best to help you.

 

BR

Joey

0 Kudos
Reply

1,555 Views
Joey_z
NXP Employee
NXP Employee

hi,Harish_R

Thank you for contacting us.

I will help you to check the issues, I will reply to you if I get the result.

BR

Joey

0 Kudos
Reply