SAF-Scheck Ahb Test - s32g3

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SAF-Scheck Ahb Test - s32g3

1,589件の閲覧回数
Harish_R
Contributor III

Hi Team,

im trying to perform Ahb test in sCheck. but the test exits with error.

while debugging i found that while clearing faults. basicaly it checks for error that is report while fualt injection. but the fault is not reported. 

Harish_R_0-1750138213259.png

so this memory w.r.t to cm7Ahbp memory has this issue. other top 4 memory does report error. 

Harish_R_1-1750138315769.png

does it require separate configuration. and the test address mentioned above is like registers address?

if someone could drop some hint it would be helpfull.

BR,

Harish R

タグ(1)
0 件の賞賛
返信
4 返答(返信)

1,543件の閲覧回数
Joey_z
NXP Employee
NXP Employee

hi,

Thank you for contacting us.

Refer to the UM of S32G_SAF_SCHECK_UM.pdf, test accesses the TCM memory using backdoor access for read and write accesses.  sCheck AHB CM7 tests access memory addresses outside the memory sections defined in the Table 62 of S32G_SAF_SCHECK_UM.pdf. See table below to determine address ranges used for AHB CM7 testing.

Joey_z_0-1750233524663.png

Hope it can help you.

BR

Joey

 

0 件の賞賛
返信

1,523件の閲覧回数
Harish_R
Contributor III

Hi @Joey_z 

Thanks for the info!

i have mapped the section of TCM memory through linker. but still, there's the same issue.

i think the AHB test doesn't only perform AHB test but also AXI test. so, address range are proper for AHB bus. as mentioned in the First screenshot earlier.

is it like should be enabled or something. im not sure. if you could provide more information, it would be helpful.

BR,

Harish R

0 件の賞賛
返信

1,499件の閲覧回数
Joey_z
NXP Employee
NXP Employee

hi,Harish_R

Thank you for your reply.

I understand what you mean. Could you share your code or tell me how to reproduce your problem?

You can provide this information easier by creating a new case at https://support.nxp.com. Can attach this link: SAF-Scheck Ahb Test - s32g3 - NXP Community. I will try my best to help you.

 

BR

Joey

0 件の賞賛
返信

1,557件の閲覧回数
Joey_z
NXP Employee
NXP Employee

hi,Harish_R

Thank you for contacting us.

I will help you to check the issues, I will reply to you if I get the result.

BR

Joey

0 件の賞賛
返信