S32g274a Multi-Core boot Demos_RDB2 issue by DS3.4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32g274a Multi-Core boot Demos_RDB2 issue by DS3.4

5,570 Views
guojunfeng
Contributor I

I am working on the multi-core startup configuration of S32G274A 

The demo program used is:S32g274a Multi-Core boot Demos_RDB2.exe

IDE:S32 Design Studio for S32 Platform 3.4

I loaded the freertos project according to the method in the operation document, and generated the code. There will be many errors, and some files can not be generated, and many errors will occur when compiling again.

If you don’t make any changes, just compile directly, and a lot of errors will be reported.

Screenshot has been added

I used some not-so-good methods to finally compile the freertos project. I can be sure that the startup assembly file and the configuration file of the ld memory allocation have not changed, and the settings in the demo project are retained.

But it can’t be started when it’s put into SD,I compared the bin file provided in the demo project with my bin file

S32g274a Multi-Core boot Demos_RDB2\pre-build binaries\Multiboot_linux_freertos\freertos_s32g274a_rdb.bin

I found that the start address of the bin file in the demo is 0x34500000

But the boot address in the demo code is 0x34800000

I hope you can give some help, how to configure the bin program to start

0 Kudos
Reply
1 Reply

5,554 Views
bpe
NXP Employee
NXP Employee

The software package you are asking about is distributed under NDA. For this reason, we cannot discuss it in a public Forum, sorry. If you need help with it, please open a Support Case. Please not not discuss NDA materials here.

 

Best Regards,
Platon

 

0 Kudos
Reply