S32g2 kernel clock init (adc\lspi)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32g2 kernel clock init (adc\lspi)

ソリューションへジャンプ
2,610件の閲覧回数
youke
Contributor III

Hi, nxp

We are using the S32G2 with the linux_bsp_42 version, booting the M7_0 and A53 cores using the M-core bootloader;
We are currently encountering an issue where the M7_0 core requires access to the ADC and LSPI functions. During the power-on process leading to the U-Boot boot, the ADC and LSPI are available. However, after U-Boot jumps to the kernel, these two modules become unavailable for a period of time. After the kernel has been executing for approximately 2 seconds, the two modules become available again. How can this issue be resolved?
We are currently considering that the kernel may have disabled the ADC and LSPI modules' clocks during startup. After the kernel initialises the ADC and LSPI, these two modules become available. How can this issue be resolved?

thanks,

タグ(3)
0 件の賞賛
返信
1 解決策
2,525件の閲覧回数
Joey_z
NXP Employee
NXP Employee

hi,youke

Thank you for your information.

I have understood your question and discussed it with the internal experts. I will reply to you as soon as there is a result.

BR

Joey

元の投稿で解決策を見る

0 件の賞賛
返信
7 返答(返信)
2,587件の閲覧回数
Joey_z
NXP Employee
NXP Employee

hi,youke

Thank you for contacting us.

There might be the reinitialization of the clock or peripherals related to ADC and LSPI modules, resulting in the suspension of ADC and LSPI. Should you avoid these operations in the kernel as much as possible, or does running ADC and LSPI functions after the Kernel starts meet the requirements?

BR

Joey

0 件の賞賛
返信
2,531件の閲覧回数
youke
Contributor III

Hi,joey

Please disregard my previous description and correct it again.
Hardware-wise, the llce_can0 peripheral is connected to the CAN transceiver (LSPI-controlled). This morning, I noticed that there were no messages for 1.5 seconds after the kernel booted up, and I mistakenly assumed that the LSPI-controlled CAN transceiver was faulty. This was incorrect. I found that the llce_can4 without the LSPI CAN transceiver was also unavailable, and the CAN-to-CAN forwarding logic configured on the M core was also disconnected.
This indicates that the entire llce_can functionality is unavailable within the first 1.5 seconds after kernel boot;
Do you have any solutions for this? We believe this is a fundamental issue related to multi-core boot for the LLCE module. Please assist in troubleshooting this issue;

 

thanks,

0 件の賞賛
返信
2,526件の閲覧回数
Joey_z
NXP Employee
NXP Employee

hi,youke

Thank you for your information.

I have understood your question and discussed it with the internal experts. I will reply to you as soon as there is a result.

BR

Joey

0 件の賞賛
返信
2,386件の閲覧回数
youke
Contributor III

Hi,joey

Thanks for your help. I've solved the problem.
I found that u-boot closed some modules before jumping to the kernel. After modifying that part of the code, it works fine now.
Thanks again.

0 件の賞賛
返信
2,373件の閲覧回数
Joey_z
NXP Employee
NXP Employee

hi,youke

Thank you for sharing the experience.

BR

Joey

0 件の賞賛
返信
2,554件の閲覧回数
youke
Contributor III

Hi,joey

The UART used in u-boot can be used directly in the kernel jump (clk: 125M). Can my ADC and LSPI modules be configured in the same way? How should they be configured?

thanks,

0 件の賞賛
返信
2,564件の閲覧回数
youke
Contributor III

Hi,joey

Thank you for your reply.
These modules are used by the M core and cannot wait for the kernel to start before being used, as this takes too long.
These modules are available during the u-boot stage. How can we reuse these states when the kernel starts up so that they do not have to be initialised from scratch? Do you have any suggestions?

0 件の賞賛
返信