S32ds NXP build

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32ds NXP build

2,419 Views
nancb
Contributor II

I'm running a build from the command line and it generates the following errors

 

Managed Build system manifest file error: Unable to resolve the superClass identifier ghs.managedmake.arm.executable.toolchain in the toolChain com.nxp.s32ds.cle.arm.mbs.ghs.toolchain.debug.

Managed Build system manifest file error: Unable to resolve the superClass identifier ghs.managedmake.arm.executable.toolchain in the toolChain com.nxp.s32ds.cle.arm.mbs.ghs.toolchain.release.

Managed Build system manifest file error: Unable to resolve the superClass identifier ghs.managedmake.arm.executable.toolchain in the toolChain com.nxp.s32ds.cle.arm.mbs.ghs.toolchain.debug.ram.

Managed Build system manifest file error: Unable to resolve the superClass identifier ghs.managedmake.arm.executable.toolchain in the toolChain com.nxp.s32ds.cle.arm.mbs.ghs.toolchain.release.ram.

Managed Build system manifest file error: Unable to resolve the superClass identifier ghs.managedmake.arm.static_library.toolchain in the toolChain com.nxp.s32ds.cle.arm.mbs.ghs.toolchain.debug.lib.

Managed Build system manifest file error: Unable to resolve the superClass identifier ghs.managedmake.arm.static_library.toolchain in the toolChain com.nxp.s32ds.cle.arm.mbs.ghs.toolchain.release.lib.

 

However everything builds correctly.  When I run this in an Azure DevOps pipeline it picks these up as errors, which I would prefer it didn't.

 

I'm not sure where to even start looking for these, other than these look similar to the original build configuration names which we changed.

Tags (1)
0 Kudos
Reply
3 Replies

2,406 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Can you let us know which S32 platform are you using? Also, which S32DS version are you working with?

Please, let us know.

0 Kudos
Reply

2,400 Views
nancb
Contributor II

Hi Daniel Aguirre,

I use the S32DS_ARM_v2.2 platform, using this tool to compile my project is normal without error, but I use the command line to call NXP/S32DS_ARM_v2.2/eclipse.exe compilation will report the above error

Thank you.

0 Kudos
Reply

2,392 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Thanks for your feedback.

Given the S32DS version you are using, it seems that this community might not be the correct one, since we mainly support S32G and related S32DS versions. We do apologize.

Help us open this same request under the following community:

S32 Design Studio - NXP Community

Since in there you should receive the correct support. We also recommend detailing which S32 product you are using as well as if you are using any example or if it is only happening under non-NXP code.

Again, we apologize.

Please, let us know.

0 Kudos
Reply