S32G399A-RDB3 QNX PFE Driver Problems

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32G399A-RDB3 QNX PFE Driver Problems

563 Views
Seneca
Contributor I

Greetings,

we try to get PFE running on a S32G399A-RDB3 board with QNX. As far as I can tell, this is a valid combination:

BSP 37.0
PFE-FW_S32G_1.7.0
PFE-DRV-S32G_A53_QNX_1.4.0

It ends with a no carrier error on all network interfaces. Plugging the cable into different ethernet ports changes nothing. 

It used to work with gmac0.

Any ideas?

io pkt call:

io-pkt-v6-hc -p tcpip -d pfe-2 pfe0_mac=000a0b0c0d66,pfe1_mac=001a1b1c1d66,pfe2_mac=002a2b2c2d66,class_fw=/proc/boot/s32g_pfe_class.fw,no_reset,mode0=sgmii,phy0=0,mode1=sgmii,phy1=1

Uboot parameters:

Uboot is the same as from the Linux sdcard image with modified parmeters for qnx boot. 

setenv hwconfig "pcie0:mode=rc,clock=ext;pcie1:mode=sgmii,clock=ext,fmhz=125,xpcs_mode=2G5"
setenv pfeng_mode 'enable,sgmii,sgmii,rgmii'
setenv s32cc_gmac_mode disable
setenv pfeng enable; s32ccgmac disable; s32ccgmac enable;
setenv boot_qnx_atf 'mmc dev 0; fatload mmc 0:1 0x83e00000 s32g399a-rdb3.dtb; pfeng enable; s32ccgmac disable; s32ccgmac enable; fatload mmc 0:1 0x80080000 ifs-s32g399a-rdb.ui; bootm 0x80080000 - 0x83E00000'
setenv bootcmd 'run boot_qnx_atf'
saveenv

 

Log:

U-Boot 2020.04+g156b168010 (Jun 09 2023 - 10:14:25 +0000)
 
CPU:   NXP S32G399A rev. 1.1
Model: NXP S32G399A-RDB3
DRAM:  3.5 GiB
MMC:   FSL_SDHC: 0
Loading Environment from MMC... OK
Configuring PCIe0 as RootComplex
PCIe0: Failed to get link up
PCI: Failed autoconfig bar 1c
In:    serial@401c8000
Out:   serial@401c8000
Err:   serial@401c8000
Board revision: RDB3 Revision F
Net:   EQOS phy: rgmii @ 1
 
Warning: eth_eqos (eth0) using random MAC address - 26:e4:e6:43:15:ad
eth0: eth_eqosFailed to get speed of XPCS for emac1_xpcs PFE: emac0: sgmii emac1: sgmii emac2: rgmii
, eth1: eth_pfeng
Hit any key to stop autoboot:  3  2  1  0 
switch to partitions #0, OK
mmc0 is current device
50640 bytes read in 17 ms (2.8 MiB/s)
11948752 bytes read in 540 ms (21.1 MiB/s)
## Booting kernel from Legacy Image at 80080000 ...
   Image Name:   
   Image Type:   AArch64 Linux Kernel Image (uncompressed)
   Data Size:    11948688 Bytes = 11.4 MiB
   Load Address: 80080000
   Entry Point:  80080000
   Verifying Checksum ... OK
## Flattened Device Tree blob at 83e00000
   Booting using the fdt blob at 0x83e00000
   Loading Kernel Image
   Using Device Tree in place at 0000000083e00000, end 0000000083e0f5cf
   fixup: pfe0 set to 00:01:be:be:ef:11
   fixup: pfe1 set to 00:01:be:be:ef:22
   fixup: pfe1: update phy addr to 0x8
   fixup: pfe2 set to 00:01:be:be:ef:33
 
Starting kernel ...
 
Reserving RAM region for PFE driver on EVB/RDB
Done.
ClockCycles samples:
 0 43600679
 1 43600679
 2 43600678
 3 43600679
 4 43600678
 5 43600678
 6 43600678
 7 43600679
All ClockCycles offsets within tolerance
Welcome to QNX Neutrino 7.1.0 on the NXP S32G399A RDB Board!!
Starting watchdog...
Starting serial driver ...
Starting Networking driver (/dev/socket)...
 
Process 4107 (ifconfig) exited status=0.
 
Process 10 (sh) exited status=0.
 
Process 9 (dhclient) exited status=0.
cp: Can't open source file.  (/proc/boot/libfci_cli)
 
Process 20489 (cp) exited status=1.
Starting SPI driver (/dev/spi0,1,2,3,4,5)...
Starting I2C 0/1/2/3/4 driver (/dev/i2c0,1,2,3,4)...
Starting USDHC0 memory card driver...
[00]     SIM="SDMMC" HBA="imx"
[00,0,0] type=00 ver=05 resp=00                       SDMMC:
 
Process 24596 (chkqnx6fs) exited status=0.
 
Process 28692 (mount) exited status=0.
Starting QSPI Flash driver...
Starting USB host driver (/dev/usb/*)
Detected QSPI Flash: Macronix MX25UW512, JEDEC 0xC2 - 0x813A, Size: 0x4000000
Launching devb-umass for /dev/usb/* ...
Process 36891 (sleep) exited status=0.
sh: /var/cetitec2/startup.sh: No such file or directory
 
Process 45081 (sh) terminated signo=0 code=0 by process 0 value=0.
slog2info
 
Jan 01 00:00:00.023                       random.4                  low*     0  qcrypto: loading configuration file '/etc/qcrypto.conf' [qcrypto_common.c(190)]
Jan 01 00:00:00.024                    random.4..0                 slog*   700  Random is using the Fortuna PRNG
Jan 01 00:00:00.031                       random.4                  low      0  qcrypto: 'openssl' plugin loaded [qcrypto_plugins.c(354)]
Jan 01 00:00:00.031                    random.4..0                 slog    700  Selecting timer as an entropy source
Jan 01 00:00:00.032                    random.4..0                 slog    700  Registered path names
Jan 01 00:00:00.032                    random.4..0                 slog    700  random: starting resmgr
Jan 01 00:00:00.032                    random.4..0                 slog    700  random: Daemonizing the process
Jan 01 00:00:00.042             devc_serlinflexd.7                 slog*     0  serlinflexd_interrupt_attach: Attaching to interrupt 114
Jan 01 00:00:00.047                        iopkt.8          main_buffer*     0  tcpip starting
Jan 01 00:00:00.047                        iopkt.8          main_buffer      0  smmu support is disabled
Jan 01 00:00:00.049                        iopkt.8          main_buffer      0  initializing IPsec...
Jan 01 00:00:00.049                        iopkt.8          main_buffer      0   done
 
Jan 01 00:00:00.049                        iopkt.8          main_buffer      0  IPsec: Initialized Security Association Processing.
 
Jan 01 00:00:00.051                        iopkt.8          main_buffer      0  devnp-pfe-2.so pfe0_mac=000a0b0c0d66,pfe1_mac=001a1b1c1d66,pfe2_mac=002a2b2c2d66,class_fw=/proc/boot/s32g_pfe_class.fw,pfe0_mode=sgmii,pfe0_phy=0,pfe1_mode=sgmii,pfe1_phy=1
Jan 01 00:00:00.052                 io_pkt_v6_hc.8                 slog*     0  INF[src/pfe_drv.c:1377]: VERSION INFO
Driver version: 1.4.0
Driver commit hash: 2f3265a49ac18f94ba5e48254c8f870fe7bfc511
PFE_CFG_MULTI_INSTANCE_SUPPORT: 0
PFE_CFG_LOCAL_IF: 6
PFE_CFG_MASTER_IF: 6
PFE_CFG_SC_HIF: 1
PFE_CFG_HIF_RING_LENGTH: 256
PFE_CFG_PFE0_PROMISC: 1
PFE_CFG_PFE1_PROMISC: 1
PFE_CFG_PFE2_PROMISC: 1
 
 
Jan 01 00:00:00.052                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:1384]: --- Safe IRQ enabled. No InterrupAttach() or InterruptAttach_r() allowed.
 
Jan 01 00:00:00.052                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_fw.c:83]: 42792 bytes read
 
Jan 01 00:00:00.053                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_fw.c:89]: Loaded firmware file: /proc/boot/s32g_pfe_class.fw
 
Jan 01 00:00:00.053                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:1477]: MII mode configuration for pfe0/EMAC0 not found. Using SGMII.
 
Jan 01 00:00:00.053                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:1477]: MII mode configuration for pfe1/EMAC1 not found. Using SGMII.
 
Jan 01 00:00:00.053                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:1477]: MII mode configuration for pfe2/EMAC2 not found. Using RGMII.
 
Jan 01 00:00:00.053                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:1495]: Issuing PFE peripheral reset...
 
Jan 01 00:00:00.274                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:1496]: PFE reset OK.
 
Jan 01 00:00:00.274                 io_pkt_v6_hc.8                 slog      0  INF[hw/s32g/pfe_platform_master.c:3519]: PFE CBUS p0x46000000 mapped @ v0x38f2e23000
 
Jan 01 00:00:00.274                 io_pkt_v6_hc.8                 slog      0  INF[hw/s32g/pfe_platform_master.c:3524]: HW version 0x101
 
Jan 01 00:00:00.274                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_hw_feature.c:95]: Silicon S32G3
 
Jan 01 00:00:00.274                 io_pkt_v6_hc.8                 slog      0  WRN[hw/s32g/pfe_platform_master.c:3536]: Fail-Stop mode disabled
 
Jan 01 00:00:00.275                 io_pkt_v6_hc.8                 slog      0  INF[hw/s32g/pfe_platform_master.c:2687]: PFE_ERRORS:Parity instance created
 
Jan 01 00:00:00.275                 io_pkt_v6_hc.8                 slog      0  INF[hw/s32g/pfe_platform_master.c:2702]: PFE_ERRORS:Watchdog instance created
 
Jan 01 00:00:00.275                 io_pkt_v6_hc.8                 slog      0  INF[hw/s32g/pfe_platform_master.c:2718]: PFE_ERRORS:Bus Error instance created
 
Jan 01 00:00:00.275                 io_pkt_v6_hc.8                 slog      0  INF[hw/s32g/pfe_platform_master.c:2731]: PFE_ERRORS:FW Fail Stop instance created
 
Jan 01 00:00:00.275                 io_pkt_v6_hc.8                 slog      0  INF[hw/s32g/pfe_platform_master.c:2744]: PFE_ERRORS:Host Fail Stop instance created
 
Jan 01 00:00:00.275                 io_pkt_v6_hc.8                 slog      0  INF[hw/s32g/pfe_platform_master.c:2757]: PFE_ERRORS:Fail Stop instance created
 
Jan 01 00:00:00.275                 io_pkt_v6_hc.8                 slog      0  INF[hw/s32g/pfe_platform_master.c:2770]: PFE_ERRORS:ECC Err instance created
 
Jan 01 00:00:00.275                 io_pkt_v6_hc.8                 slog      0  INF[hw/s32g/pfe_platform_master.c:1766]: BMU1 buffer base: p0xc0000000
 
Jan 01 00:00:00.277                 io_pkt_v6_hc.8                 slog      0  INF[hw/s32g/pfe_platform_master.c:1810]: BMU2 buffer base: p0x83000000 (0x200000 bytes)
 
Jan 01 00:00:00.279                 io_pkt_v6_hc.8                 slog      0  INF[src/oal_irq_qnx.c:117]: PFE BMU IRQ Worker started (IRQ ID: 226)
 
Jan 01 00:00:00.279                 io_pkt_v6_hc.8                 slog      0  WRN[hw/s32g/pfe_platform_master.c:2194]: The option 'g2_ordered_class_writes' is disabled.
 
Jan 01 00:00:00.279                 io_pkt_v6_hc.8                 slog      0  INF[hw/s32g/pfe_bmu_csr.c:96]: BMU_EMPTY_INT (BMU @ p0x88000). Pool ready.
 
Jan 01 00:00:00.279                 io_pkt_v6_hc.8                 slog      0  INF[hw/s32g/pfe_bmu_csr.c:96]: BMU_EMPTY_INT (BMU @ p0x8c000). Pool ready.
 
Jan 01 00:00:00.281                 io_pkt_v6_hc.8                 slog      0  INF[hw/s32g/pfe_platform_master.c:2239]: Firmware .elf detected
 
Jan 01 00:00:00.281                 io_pkt_v6_hc.8                 slog      0  INF[hw/s32g/pfe_platform_master.c:2248]: Uploading CLASS firmware
 
Jan 01 00:00:00.281                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_pe.c:609]: Selected FW loading OPs to load 8 PEs in parallel
 
Jan 01 00:00:00.285                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_pe.c:1945]: pfe_ct.h file version"92367c0e25f21f49217a9b08168ad2c8"
 
Jan 01 00:00:00.288                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_pe.c:2422]: [FW VERSION] 1.7.0, Build: Jun  2 2023, 13:48:57 (nogitaaa), ID: 0x31454650
 
Jan 01 00:00:00.406                 io_pkt_v6_hc.8                 slog      0  WRN[hw/s32g/pfe_platform_master.c:2312]: VLAN ID incorrect or not set. Using default VLAN ID = 0x01.
 
Jan 01 00:00:00.406                 io_pkt_v6_hc.8                 slog      0  WRN[hw/s32g/pfe_platform_master.c:2318]: VLAN stats size incorrect or not set. Using default VLAN stats size = 20.
 
Jan 01 00:00:00.406                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_l2br.c:1181]: Software vlan hash table @ p0x20001228
 
 
Jan 01 00:00:00.406                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_l2br.c:1286]: Fall-back bridge domain @ 0x20000a7c (class)
 
Jan 01 00:00:00.406                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_l2br.c:1287]: Default bridge domain @ 0x20000a74 (class)
 
Jan 01 00:00:00.406                 io_pkt_v6_hc.8                 slog      0  INF[hw/s32g/pfe_platform_master.c:2412]: Routing table created, Hash Table @ p0x80014000, Pool @ p0x8001c000 (65536 bytes)
 
Jan 01 00:00:00.407                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_hif_chnl.c:1997]: Initializing RX buffer pool. Depth: 256; Buffer Size: 2048; Cache Line Size: 64
 
Jan 01 00:00:00.408                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_hif_chnl.c:1997]: Initializing RX buffer pool. Depth: 256; Buffer Size: 2048; Cache Line Size: 64
 
Jan 01 00:00:00.409                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_hif_chnl.c:1997]: Initializing RX buffer pool. Depth: 256; Buffer Size: 2048; Cache Line Size: 64
 
Jan 01 00:00:00.508                 io_pkt_v6_hc.8                 slog      0  INF[hw/s32g/pfe_platform_master.c:3705]: Feature err051211_workaround: DISABLED
 
Jan 01 00:00:00.509                        iopkt.8          main_buffer      0  pfe0
 
Jan 01 00:00:00.509                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2152]: pfe0: Using PHY mode: MDIO=0, ADDR=0, CLAUSE=0, RESET=0
 
Jan 01 00:00:00.509                 io_pkt_v6_hc.8                 slog      0  INF[src/oal_irq_qnx.c:117]: PFE HIF0 IRQ Worker started (IRQ ID: 222)
 
Jan 01 00:00:00.509                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:1795]: Adding 00:0a:0b:0c:0d:66 to pfe0
 
Jan 01 00:00:00.511                        iopkt.8          main_buffer      0  pfe1
 
Jan 01 00:00:00.511                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2298]: Speed/duplex configuration for pfe0 not found. Using 1 Gbps/full-duplex.
 
Jan 01 00:00:00.511                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_hif_drv_sc.c:336]: Attempt to register HIF client: 0
 
Jan 01 00:00:00.511                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_hif_drv_sc.c:1189]: HIF driver started
 
Jan 01 00:00:00.511                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2363]: New PFE device: 0, ID: 0
 
Jan 01 00:00:00.511                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2152]: pfe1: Using PHY mode: MDIO=1, ADDR=0, CLAUSE=0, RESET=0
 
Jan 01 00:00:00.511                 io_pkt_v6_hc.8                 slog      0  INF[src/oal_irq_qnx.c:117]: PFE HIF1 IRQ Worker started (IRQ ID: 223)
 
Jan 01 00:00:00.511                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:1795]: Adding 00:1a:1b:1c:1d:66 to pfe1
 
Jan 01 00:00:00.513                        iopkt.8          main_buffer      0  pfe2
 
Jan 01 00:00:00.513                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2298]: Speed/duplex configuration for pfe1 not found. Using 1 Gbps/full-duplex.
 
Jan 01 00:00:00.513                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_hif_drv_sc.c:336]: Attempt to register HIF client: 1
 
Jan 01 00:00:00.513                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_hif_drv_sc.c:1189]: HIF driver started
 
Jan 01 00:00:00.513                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2363]: New PFE device: 1, ID: 2
 
Jan 01 00:00:00.513                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2145]: pfe2: Using static PHY mode, RESET=0
 
Jan 01 00:00:00.513                 io_pkt_v6_hc.8                 slog      0  INF[src/oal_irq_qnx.c:117]: PFE HIF2 IRQ Worker started (IRQ ID: 224)
 
Jan 01 00:00:00.513                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:1795]: Adding 00:2a:2b:2c:2d:66 to pfe2
 
Jan 01 00:00:00.515                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2298]: Speed/duplex configuration for pfe2 not found. Using 1 Gbps/full-duplex.
 
Jan 01 00:00:00.515                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_hif_drv_sc.c:336]: Attempt to register HIF client: 2
 
Jan 01 00:00:00.515                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_hif_drv_sc.c:1189]: HIF driver started
 
Jan 01 00:00:00.515                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2363]: New PFE device: 2, ID: 4
 
Jan 01 00:00:00.530                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2702]: Adding 00:0a:0b:0c:0d:66 to pfe0
 
Jan 01 00:00:00.530                 io_pkt_v6_hc.8                 slog      0  WRN[src/pfe_drv.c:2707]: Unable to assign MAC address 00:0a:0b:0c:0d:66 to the pfe0
 
Jan 01 00:00:00.530                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2663]: pfe0: Disabling promiscuous mode
 
Jan 01 00:00:00.538                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_mdio.c:427]: pfe0: PHY @ bus 0 addr 0 not found. Switching to static mode.
 
Jan 01 00:00:00.538                 io_pkt_v6_hc.8                 slog      0  WRN[src/pfe_drv.c:2829]: EMAC speed change for SGMII is currently not supported.
 
Jan 01 00:00:00.538                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2443]: Adding 33:33:ff:0c:0d:66 to emac0
 
Jan 01 00:00:00.540                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2663]: pfe0: Disabling promiscuous mode
 
Jan 01 00:00:00.540                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2443]: Adding 33:33:00:00:00:01 to emac0
 
Jan 01 00:00:00.542                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2443]: Adding 33:33:ff:0c:0d:66 to emac0
 
Jan 01 00:00:00.542                 io_pkt_v6_hc.8                 slog      0  WRN[src/pfe_drv.c:2450]: unable to add 33:33:ff:0c:0d:66 into emac0: 17
 
Jan 01 00:00:00.542                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2663]: pfe0: Disabling promiscuous mode
 
Jan 01 00:00:00.542                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2443]: Adding 33:33:00:00:00:01 to emac0
 
Jan 01 00:00:00.542                 io_pkt_v6_hc.8                 slog      0  WRN[src/pfe_drv.c:2450]: unable to add 33:33:00:00:00:01 into emac0: 17
 
Jan 01 00:00:00.542                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2443]: Adding 33:33:ff:0c:0d:66 to emac0
 
Jan 01 00:00:00.542                 io_pkt_v6_hc.8                 slog      0  WRN[src/pfe_drv.c:2450]: unable to add 33:33:ff:0c:0d:66 into emac0: 17
 
Jan 01 00:00:00.542                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2663]: pfe0: Disabling promiscuous mode
 
Jan 01 00:00:00.542                 io_pkt_v6_hc.8                 slog      0  WRN[src/pfe_drv.c:2829]: EMAC speed change for SGMII is currently not supported.
 
Jan 01 00:00:00.542                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2443]: Adding 01:00:5e:00:00:01 to emac0
 
Jan 01 00:00:00.544                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2443]: Adding 33:33:00:00:00:01 to emac0
 
Jan 01 00:00:00.544                 io_pkt_v6_hc.8                 slog      0  WRN[src/pfe_drv.c:2450]: unable to add 33:33:00:00:00:01 into emac0: 17
 
Jan 01 00:00:00.544                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2443]: Adding 33:33:ff:0c:0d:66 to emac0
 
Jan 01 00:00:00.544                 io_pkt_v6_hc.8                 slog      0  WRN[src/pfe_drv.c:2450]: unable to add 33:33:ff:0c:0d:66 into emac0: 17
 
Jan 01 00:00:00.544                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2663]: pfe0: Disabling promiscuous mode
 
Jan 01 00:00:00.554               spi_master.24585               normal*     0  Starting spi-master resource manager
Jan 01 00:00:00.558               spi_master.24587               normal*     0  Starting spi-master resource manager
Jan 01 00:00:00.561               spi_master.24588               normal*     0  Starting spi-master resource manager
Jan 01 00:00:00.565               spi_master.24589               normal*     0  Starting spi-master resource manager
Jan 01 00:00:00.582          devb_sdmmc_mx8x.24595                 slog*  1800  devb-sdmmc-mx8x 1.00A (Jun 23 2026 09:45:48)
Jan 01 00:00:00.583          devb_sdmmc_mx8x.24595                 slog      0  libcam.so (Jun 22 2020 21:33:15) bver 7010003
Jan 01 00:00:00.594          devb_sdmmc_mx8x.24595                 slog   1800  sdio_cd:  insertion path 0, cd state 0x1
Jan 01 00:00:00.644          devb_sdmmc_mx8x.24595                 slog   1800  SD CID:
Jan 01 00:00:00.644          devb_sdmmc_mx8x.24595                 slog   1800    MID 0x27, OID 0x5048, PNM SD32G
Jan 01 00:00:00.644          devb_sdmmc_mx8x.24595                 slog   1800    PRV 0x62, PSN 0x6c62d132, MDT 4-2023
Jan 01 00:00:00.644          devb_sdmmc_mx8x.24595                 slog   1800  SD CSD:
Jan 01 00:00:00.644          devb_sdmmc_mx8x.24595                 slog   1800    CSD_STRUCTURE 1, SPEC_VERS 0, CCC 0x5b5
Jan 01 00:00:00.644          devb_sdmmc_mx8x.24595                 slog   1800    TAAC 14, NSAC 0, TRAN_SPEED 50
Jan 01 00:00:00.644          devb_sdmmc_mx8x.24595                 slog   1800    C_SIZE 59023, C_SIZE_MULT 0
Jan 01 00:00:00.644          devb_sdmmc_mx8x.24595                 slog   1800    READ_BL_LEN 9, WRITE_BL_LEN 9
Jan 01 00:00:00.644          devb_sdmmc_mx8x.24595                 slog   1800    ERASE GRP_SIZE 0, GRP_MULT 0, SIZE 127
Jan 01 00:00:00.644          devb_sdmmc_mx8x.24595                 slog   1800    blksz 512, sectors 60440576, dtr 25000000
Jan 01 00:00:00.644          devb_sdmmc_mx8x.24595                 slog   1800  SD SW CAPS:
Jan 01 00:00:00.644          devb_sdmmc_mx8x.24595                 slog   1800    bus mode 0x3, cmd sys 0x1
Jan 01 00:00:00.644          devb_sdmmc_mx8x.24595                 slog   1800    drv type 0x1, curr limit 0x1
Jan 01 00:00:00.644          devb_sdmmc_mx8x.24595                 slog   1800    dtr 50000000
Jan 01 00:00:00.644          devb_sdmmc_mx8x.24595                 slog   1800  CFG:  Timing HS, DTR 50000000, Bus Width 4 bit
 
Jan 01 00:00:00.645          devb_sdmmc_mx8x.24595                 slog    100  cam-disk.so (Jun 22 2020 21:33:17)
Jan 01 00:00:00.647          devb_sdmmc_mx8x.24595                 slog      0  scsi_interpret_sense (sdmmc ptl-0:0:0):  cam_status=c4, scsi_status=2, flag=00000040, vuflag=0008, cmd=1a, error=70, sense=5, asc=24, ascq=0
Jan 01 00:00:00.647          devb_sdmmc_mx8x.24595                 slog      0  scsi_interpret_sense (sdmmc ptl-0:0:0):  cam_status=c4, scsi_status=2, flag=00000040, vuflag=0008, cmd=5a, error=70, sense=5, asc=24, ascq=0
Jan 01 00:00:00.647          devb_sdmmc_mx8x.24595                 slog      0  scsi_interpret_sense (sdmmc ptl-0:0:0):  cam_status=c4, scsi_status=2, flag=00000040, vuflag=0008, cmd=5a, error=70, sense=5, asc=24, ascq=0
Jan 01 00:00:01.827          devb_sdmmc_mx8x.24595                 slog   1000  fs-qnx6: Allocation strategy 0
Jan 01 00:00:01.827          devb_sdmmc_mx8x.24595                 slog   1000  fs-qnx6: Use btree directory 0
Jan 01 00:00:01.828          devb_sdmmc_mx8x.24595                 slog   1000  fs-qnx6: fs-qnx6: trim (0,1048576,2) was not requested, and is NOT supported
Jan 01 00:00:01.833               io_usb_otg.36885                 slog*     0  main(453)[tid:1]: io-usb-otg (Jun 13 2020 20:10:17) args: -d hcd-ehci-mx28 ioport=0x44064100,irq=243,ulpi,no_stream,verbose=5 
Jan 01 00:00:01.835           devf_qspi_s32g.36884                 slog*     0  (devf  t1::f3s_qspi_ident:73) Page size: 256
Jan 01 00:00:01.835           devf_qspi_s32g.36884                 slog      0  (devf  t1::f3s_qspi_ident:74) Total chip size: 0x4000000, Unit size: 0x10000
Jan 01 00:00:01.839               io_usb_otg.36885                 slog      0  ehci_init: Initialiaing with sever version: 2 
Jan 01 00:00:01.839               io_usb_otg.36885                 slog      0  ehci_controller_init(4303): devu-hcd-ehci-mx28.so (Apr 19 2024 13:44:54):  args ulpi,no_stream,verbose=5
Jan 01 00:00:01.840               io_usb_otg.36885                 slog      8  usb_enum_port(94)[tid:1]: busno 0, parent -1, port 0, High speed
Jan 01 00:00:01.840               io_usb_otg.36885                 slog     11  usb_client_descriptor_get(198)[tid:1]: (type 1, index 0, length
Jan 01 00:00:01.840               io_usb_otg.36885                 slog     12  usb_device_set_address(245)[tid:1]: b:0 devno 0
Jan 01 00:00:01.840               io_usb_otg.36885                 slog     11  usb_client_descriptor_get(198)[tid:1]: (type 1, index 0, length 18)
Jan 01 00:00:01.841               io_usb_otg.36885                 slog     11  usb_client_descriptor_get(198)[tid:1]: (type 2, index 0, length 9)
Jan 01 00:00:01.841               io_usb_otg.36885                 slog     11  usb_client_descriptor_get(198)[tid:1]: (type 2, index 0, length 25)
Jan 01 00:00:01.841               io_usb_otg.36885                 slog      8  usb_enum_port(141)[tid:1]: vid 0x0000, did 0x0000 enumerated(busno 0, devno 0:0)
Jan 01 00:00:01.841               io_usb_otg.36885                 slog     11  hub_state_inserted(569)[tid:1]: bdentry 0, dentry 0 0
Jan 01 00:00:01.841               io_usb_otg.36885                 slog     13  hub_configuration_enable(263)[tid:1]: 1
Jan 01 00:00:01.943               io_usb_otg.36885                 slog      0  usbh_timeout_init(203)[tid:1]: Complete
Jan 01 00:00:01.954               io_usb_otg.36885                 slog      0  read_vid_pid: ULPI VID 0x0424 PID 0x0009
Jan 01 00:00:01.954               io_usb_otg.36885                 slog      0  s32g_phy_set_vbus: set_vbus off
Jan 01 00:00:01.968               io_usb_otg.36885                 slog      0  s32g_phy_set_vbus: set_vbus on
Jan 01 00:00:01.979               io_usb_otg.36885                 slog      0  ehci_get_port_status(3568 0x44064100): port=0, tpstatus 10100 e_pstatus 8c001000
Jan 01 00:00:01.979               io_usb_otg.36885                 slog      8  usb_enum_port_extract(172)[tid:7]: (busno 0, pdevno 0, portno 1)
Jan 01 00:00:01.979               io_usb_otg.36885                 slog      8  usb_enum_port_extract(192)[tid:7]: status (2)
Jan 01 00:00:01.983               devb_umass.36886                 slog*   900  devb-umass 1.00A (Jun 22 2020 21:33:41)
Jan 01 00:00:01.984               devb_umass.36886                 slog      0  libcam.so (Jun 22 2020 21:33:15) bver 7010003
Jan 01 00:00:01.985               io_usb_otg.36885                 slog      0  usbdi_client_connect(58)[tid:5]: pid 36886 proc=proc/boot/devb-umass usbdi_client 32eebb9a80
Jan 01 00:00:01.986               io_usb_otg.36885                 slog      0  usbdi_resmgr_connect(310)[tid:5]: usbdi_resmgr_connect: pid 36886 usbdi_client 32eebb9a80 
Jan 01 00:00:01.986               devb_umass.36886                 slog      0  usbdi debug path /pps/usb/debug/ doesn't exist
 
Process 49177 (slog2info) exited status=0.
# ifconfig
 
lo0: flags=8049<UP,LOOPBACK,RUNNING,MULTICAST> mtu 33136
inet 127.0.0.1 netmask 0xff000000
inet6 ::1 prefixlen 128
inet6 fe80::1%lo0 prefixlen 64 scopeid 0x1
pfe0: flags=8843<UP,BROADCAST,RUNNING,SIMPLEX,MULTICAST> mtu 1500
capabilities=1f<IP4CSUM,TCP4CSUM,UDP4CSUM,TCP6CSUM,UDP6CSUM>
enabled=0
address: 00:0a:0b:0c:0d:66
media: Ethernet none (1000baseT full-duplex)
status: active
inet 0.0.0.0 netmask 0xff000000 broadcast 255.255.255.255
inet6 fe80::20a:bff:fe0c:d66%pfe0 prefixlen 64 scopeid 0x11
pfe1: flags=8802<BROADCAST,SIMPLEX,MULTICAST> mtu 1500
capabilities=1f<IP4CSUM,TCP4CSUM,UDP4CSUM,TCP6CSUM,UDP6CSUM>
enabled=0
address: 00:1a:1b:1c:1d:66
media: Ethernet none (1000baseT full-duplex)
status: no carrier
pfe2: flags=8802<BROADCAST,SIMPLEX,MULTICAST> mtu 1500
capabilities=1f<IP4CSUM,TCP4CSUM,UDP4CSUM,TCP6CSUM,UDP6CSUM>
enabled=0
address: 00:2a:2b:2c:2d:66
media: Ethernet none (1000baseT full-duplex)
status: no carrier
 
Process 57369 (ifconfig) exited status=0.
0 Kudos
Reply
13 Replies

517 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @Seneca 

Thanks for your post.

By default, the S32G PFE QNX Driver Version 1.4.0 is compatible with S32G PFE Firmware Standard Version 1.6.0, would you mind testing it again with this PFE FW version instead?

 

BR

Chenyin

0 Kudos
Reply

507 Views
Seneca
Contributor I

Ok, so I replaced s32g_pfe_class.fw and s32g_pfe_util.fw with the files from PFE-FW_S32G_1.6.0.zip here:

https://nxp.flexnetoperations.com/control/frse/download?agree=Accept&element=14074877

 

Uboot parameters:

setenv boot_qnx_atf 'mmc dev 0; fatload mmc 0:1 0x83e00000 s32g399a-rdb3.dtb; run atf_fdt_0to3; run atf_fdt_4to7; fatload mmc 0:1 0x80080000 ifs-s32g399a-rdb.ui; pfeng enable; s32ccgmac disable; s32ccgmac enable; bootm 0x80080000 - 0x83E00000'
setenv atf_fdt_0to3 'fdt addr 0x83e00000; fdt resize; fdt set /cpus/cpu@1 cpu-release-addr <0x0 0xa0000010>; fdt set /cpus/cpu@100 cpu-release-addr <0x0 0xa0000010>; fdt set /cpus/cpu@101 cpu-release-addr <0x0 0xa0000010>;'
setenv atf_fdt_4to7 'fdt set /cpus/cpu@2 cpu-release-addr <0x0 0xa0000010>; fdt set /cpus/cpu@3 cpu-release-addr <0x0 0xa0000010>; fdt set /cpus/cpu@102 cpu-release-addr <0x0 0xa0000010>; fdt set /cpus/cpu@103 cpu-release-addr <0x0 0xa0000010>;'
setenv release_cpus 'run cpu_trap; mp 1 release 0xa0000000; mp 2 release 0xa0000000; mp 3 release 0xa0000000; mp 4 release 0xa0000000; mp 5 release 0xa0000000; mp 6 release 0xa0000000; mp 7 release 0xa0000000;'
setenv cpu_trap 'dcache off; mw.l 0xa0000000 0xd503205f; mw.l 0xa0000004 0x58000060; mw.l 0xa0000008 0xb4ffffc0; mw.l 0xa000000C 0xd61f0000; mw.q 0xa0000010 0x00000000; dcache on;'
setenv bootcmd 'run boot_qnx_atf'
setenv hwconfig "pcie0:mode=rc,clock=ext;pcie1:mode=sgmii,clock=ext,fmhz=125,xpcs_mode=2G5"
setenv pfeng_mode 'enable,sgmii,sgmii,rgmii'
setenv s32cc_gmac_mode disable
saveenv

Note: I removed the release_cpus command from boot_qnx_atf because then I would havef a cpu 1 error.

 

Doesn't look much better to me:

NOTICE:  BL2: v2.5(release):bsp37.0_rc6-2.5
NOTICE:  BL2: Built : 09:12:21, Jun 13 2023
NOTICE:  BL2: Booting BL31
 
 
U-Boot 2020.04+g156b168010 (Jun 09 2023 - 10:14:25 +0000)
 
CPU:   NXP S32G399A rev. 1.1
Model: NXP S32G399A-RDB3
DRAM:  3.5 GiB
MMC:   FSL_SDHC: 0
Loading Environment from MMC... OK
Configuring PCIe0 as RootComplex
PCIe0: Failed to get link up
PCI: Failed autoconfig bar 1c
In:    serial@401c8000
Out:   serial@401c8000
Err:   serial@401c8000
Board revision: RDB3 Revision F
Net:   EQOS phy: rgmii @ 1
 
Warning: eth_eqos (eth0) using random MAC address - 16:ec:a0:4e:1d:7c
eth0: eth_eqosFailed to get speed of XPCS for emac1_xpcs PFE: emac0: sgmii emac1: sgmii emac2: rgmii
, eth1: eth_pfeng
Hit any key to stop autoboot:  3  2  1  0 
switch to partitions #0, OK
mmc0 is current device
50640 bytes read in 17 ms (2.8 MiB/s)
11950600 bytes read in 534 ms (21.3 MiB/s)
## Booting kernel from Legacy Image at 80080000 ...
   Image Name:   
   Image Type:   AArch64 Linux Kernel Image (uncompressed)
   Data Size:    11950536 Bytes = 11.4 MiB
   Load Address: 80080000
   Entry Point:  80080000
   Verifying Checksum ... OK
## Flattened Device Tree blob at 83e00000
   Booting using the fdt blob at 0x83e00000
   Loading Kernel Image
   Using Device Tree in place at 0000000083e00000, end 0000000083e0ffff
   fixup: pfe0 set to 00:01:be:be:ef:11
   fixup: pfe1 set to 00:01:be:be:ef:22
   fixup: pfe1: update phy addr to 0x8
   fixup: pfe2 set to 00:01:be:be:ef:33
 
Starting kernel ...
 
Reserving RAM region for PFE driver on EVB/RDB
Done.
ClockCycles samples:
 0 43642864
 1 43642864
 2 43642864
 3 43642864
 4 43642864
 5 43642864
 6 43642864
 7 43642864
All ClockCycles offsets within tolerance
Welcome to QNX Neutrino 7.1.0 on the NXP S32G399A RDB Board!!
Starting watchdog...
Starting serial driver ...
Starting Networking driver (/dev/socket)...
 
Process 4107 (ifconfig) exited status=0.
 
Process 10 (sh) exited status=0.
 
Process 9 (dhclient) exited status=0.
cp: Can't open source file.  (/proc/boot/libfci_cli)
 
Process 20489 (cp) exited status=1.
Starting SPI driver (/dev/spi0,1,2,3,4,5)...
Starting I2C 0/1/2/3/4 driver (/dev/i2c0,1,2,3,4)...
Starting USDHC0 memory card driver...
[00]     SIM="SDMMC" HBA="imx"
[00,0,0] type=00 ver=05 resp=00                       SDMMC:
 
Process 24596 (chkqnx6fs) exited status=0.
 
Process 28692 (mount) exited status=0.
Starting QSPI Flash driver...
Starting USB host driver (/dev/usb/*)
Detected QSPI Flash: Macronix MX25UW512, JEDEC 0xC2 - 0x813A, Size: 0x4000000
Launching devb-umass for /dev/usb/* ...
# ifconfig
 
lo0: flags=8049<UP,LOOPBACK,RUNNING,MULTICAST> mtu 33136
inet 127.0.0.1 netmask 0xff000000
inet6 ::1 prefixlen 128
inet6 fe80::1%lo0 prefixlen 64 scopeid 0x1
pfe0: flags=8843<UP,BROADCAST,RUNNING,SIMPLEX,MULTICAST> mtu 1500
capabilities=1f<IP4CSUM,TCP4CSUM,UDP4CSUM,TCP6CSUM,UDP6CSUM>
enabled=0
address: 00:0a:0b:0c:0d:66
media: Ethernet none (1000baseT full-duplex)
status: active
inet 0.0.0.0 netmask 0xff000000 broadcast 255.255.255.255
inet6 fe80::20a:bff:fe0c:d66%pfe0 prefixlen 64 scopeid 0x11
pfe1: flags=8802<BROADCAST,SIMPLEX,MULTICAST> mtu 1500
capabilities=1f<IP4CSUM,TCP4CSUM,UDP4CSUM,TCP6CSUM,UDP6CSUM>
enabled=0
address: 00:1a:1b:1c:1d:66
media: Ethernet none (1000baseT full-duplex)
status: no carrier
pfe2: flags=8802<BROADCAST,SIMPLEX,MULTICAST> mtu 1500
capabilities=1f<IP4CSUM,TCP4CSUM,UDP4CSUM,TCP6CSUM,UDP6CSUM>
enabled=0
address: 00:2a:2b:2c:2d:66
media: Ethernet none (1000baseT full-duplex)
status: no carrier
 
Process 40985 (ifconfig) exited status=0.
Process 36891 (sleep) exited status=0.
sh: /var/cetitec2/startup.sh: No such file or directory
 
Process 53273 (sh) terminated signo=0 code=0 by process 0 value=0.
 
# ifconfig 
 
lo0: flags=8049<UP,LOOPBACK,RUNNING,MULTICAST> mtu 33136
inet 127.0.0.1 netmask 0xff000000
inet6 ::1 prefixlen 128
inet6 fe80::1%lo0 prefixlen 64 scopeid 0x1
pfe0: flags=8843<UP,BROADCAST,RUNNING,SIMPLEX,MULTICAST> mtu 1500
capabilities=1f<IP4CSUM,TCP4CSUM,UDP4CSUM,TCP6CSUM,UDP6CSUM>
enabled=0
address: 00:0a:0b:0c:0d:66
media: Ethernet none (1000baseT full-duplex)
status: active
inet 0.0.0.0 netmask 0xff000000 broadcast 255.255.255.255
inet6 fe80::20a:bff:fe0c:d66%pfe0 prefixlen 64 scopeid 0x11
pfe1: flags=8802<BROADCAST,SIMPLEX,MULTICAST> mtu 1500
capabilities=1f<IP4CSUM,TCP4CSUM,UDP4CSUM,TCP6CSUM,UDP6CSUM>
enabled=0
address: 00:1a:1b:1c:1d:66
media: Ethernet none (1000baseT full-duplex)
status: no carrier
pfe2: flags=8802<BROADCAST,SIMPLEX,MULTICAST> mtu 1500
capabilities=1f<IP4CSUM,TCP4CSUM,UDP4CSUM,TCP6CSUM,UDP6CSUM>
enabled=0
address: 00:2a:2b:2c:2d:66
media: Ethernet none (1000baseT full-duplex)
status: no carrier
 

# slog2info | grep pfe

Jan 01 00:00:00.051 iopkt.8 main_buffer 0 devnp-pfe-2.so pfe0_mac=000a0b0c0d66,pfe1_mac=001a1b1c1d66,pfe2_mac=002a2b2c2d66,class_fw=/proc/boot/s32g_pfe_class.fw
Jan 01 00:00:00.052 io_pkt_v6_hc.8 slog* 0 INF[src/pfe_drv.c:1377]: VERSION INFO
Jan 01 00:00:00.052 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:1384]: --- Safe IRQ enabled. No InterrupAttach() or InterruptAttach_r() allowed.
Jan 01 00:00:00.052 io_pkt_v6_hc.8 slog 0 INF[src/pfe_fw.c:83]: 49480 bytes read
Jan 01 00:00:00.052 io_pkt_v6_hc.8 slog 0 INF[src/pfe_fw.c:89]: Loaded firmware file: /proc/boot/s32g_pfe_class.fw
Jan 01 00:00:00.053 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:1477]: MII mode configuration for pfe0/EMAC0 not found. Using SGMII.
Jan 01 00:00:00.053 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:1477]: MII mode configuration for pfe1/EMAC1 not found. Using SGMII.
Jan 01 00:00:00.053 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:1477]: MII mode configuration for pfe2/EMAC2 not found. Using RGMII.
Jan 01 00:00:00.053 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:1495]: Issuing PFE peripheral reset...
Jan 01 00:00:00.274 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:1496]: PFE reset OK.
Jan 01 00:00:00.274 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:3519]: PFE CBUS p0x46000000 mapped @ v0x1abef95000
Jan 01 00:00:00.274 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:3524]: HW version 0x101
Jan 01 00:00:00.274 io_pkt_v6_hc.8 slog 0 INF[src/pfe_hw_feature.c:95]: Silicon S32G3
Jan 01 00:00:00.274 io_pkt_v6_hc.8 slog 0 WRN[hw/s32g/pfe_platform_master.c:3536]: Fail-Stop mode disabled
Jan 01 00:00:00.275 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:2687]: PFE_ERRORS:Parity instance created
Jan 01 00:00:00.275 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:2702]: PFE_ERRORS:Watchdog instance created
Jan 01 00:00:00.275 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:2718]: PFE_ERRORS:Bus Error instance created
Jan 01 00:00:00.275 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:2731]: PFE_ERRORS:FW Fail Stop instance created
Jan 01 00:00:00.275 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:2744]: PFE_ERRORS:Host Fail Stop instance created
Jan 01 00:00:00.275 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:2757]: PFE_ERRORS:Fail Stop instance created
Jan 01 00:00:00.275 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:2770]: PFE_ERRORS:ECC Err instance created
Jan 01 00:00:00.275 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:1766]: BMU1 buffer base: p0xc0000000
Jan 01 00:00:00.277 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:1810]: BMU2 buffer base: p0x83000000 (0x200000 bytes)
Jan 01 00:00:00.279 io_pkt_v6_hc.8 slog 0 WRN[hw/s32g/pfe_platform_master.c:2194]: The option 'g2_ordered_class_writes' is disabled.
Jan 01 00:00:00.279 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_bmu_csr.c:96]: BMU_EMPTY_INT (BMU @ p0x88000). Pool ready.
Jan 01 00:00:00.279 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_bmu_csr.c:96]: BMU_EMPTY_INT (BMU @ p0x8c000). Pool ready.
Jan 01 00:00:00.281 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:2239]: Firmware .elf detected
Jan 01 00:00:00.281 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:2248]: Uploading CLASS firmware
Jan 01 00:00:00.281 io_pkt_v6_hc.8 slog 0 INF[src/pfe_pe.c:609]: Selected FW loading OPs to load 8 PEs in parallel
Jan 01 00:00:00.285 io_pkt_v6_hc.8 slog 0 INF[src/pfe_pe.c:1945]: pfe_ct.h file version"92367c0e25f21f49217a9b08168ad2c8"
Jan 01 00:00:00.288 io_pkt_v6_hc.8 slog 0 INF[src/pfe_pe.c:2422]: [FW VERSION] 1.6.0, Build: Mar 15 2023, 12:37:54 (), ID: 0x31454650
Jan 01 00:00:00.406 io_pkt_v6_hc.8 slog 0 WRN[hw/s32g/pfe_platform_master.c:2312]: VLAN ID incorrect or not set. Using default VLAN ID = 0x01.
Jan 01 00:00:00.406 io_pkt_v6_hc.8 slog 0 WRN[hw/s32g/pfe_platform_master.c:2318]: VLAN stats size incorrect or not set. Using default VLAN stats size = 20.
Jan 01 00:00:00.406 io_pkt_v6_hc.8 slog 0 INF[src/pfe_l2br.c:1181]: Software vlan hash table @ p0x20001208
Jan 01 00:00:00.406 io_pkt_v6_hc.8 slog 0 INF[src/pfe_l2br.c:1286]: Fall-back bridge domain @ 0x20000a44 (class)
Jan 01 00:00:00.406 io_pkt_v6_hc.8 slog 0 INF[src/pfe_l2br.c:1287]: Default bridge domain @ 0x20000a3c (class)
Jan 01 00:00:00.406 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:2412]: Routing table created, Hash Table @ p0x80014000, Pool @ p0x8001c000 (65536 bytes)
Jan 01 00:00:00.407 io_pkt_v6_hc.8 slog 0 INF[src/pfe_hif_chnl.c:1997]: Initializing RX buffer pool. Depth: 256; Buffer Size: 2048; Cache Line Size: 64
Jan 01 00:00:00.408 io_pkt_v6_hc.8 slog 0 INF[src/pfe_hif_chnl.c:1997]: Initializing RX buffer pool. Depth: 256; Buffer Size: 2048; Cache Line Size: 64
Jan 01 00:00:00.409 io_pkt_v6_hc.8 slog 0 INF[src/pfe_hif_chnl.c:1997]: Initializing RX buffer pool. Depth: 256; Buffer Size: 2048; Cache Line Size: 64
Jan 01 00:00:00.508 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:3705]: Feature err051211_workaround: DISABLED
Jan 01 00:00:00.509 iopkt.8 main_buffer 0 pfe0
Jan 01 00:00:00.509 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2145]: pfe0: Using static PHY mode, RESET=0
Jan 01 00:00:00.510 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:1795]: Adding 00:0a:0b:0c:0d:66 to pfe0
Jan 01 00:00:00.512 iopkt.8 main_buffer 0 pfe1
Jan 01 00:00:00.512 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2298]: Speed/duplex configuration for pfe0 not found. Using 1 Gbps/full-duplex.
Jan 01 00:00:00.512 io_pkt_v6_hc.8 slog 0 INF[src/pfe_hif_drv_sc.c:336]: Attempt to register HIF client: 0
Jan 01 00:00:00.512 io_pkt_v6_hc.8 slog 0 INF[src/pfe_hif_drv_sc.c:1189]: HIF driver started
Jan 01 00:00:00.512 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2363]: New PFE device: 0, ID: 0
Jan 01 00:00:00.512 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2145]: pfe1: Using static PHY mode, RESET=0
Jan 01 00:00:00.512 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:1795]: Adding 00:1a:1b:1c:1d:66 to pfe1
Jan 01 00:00:00.514 iopkt.8 main_buffer 0 pfe2
Jan 01 00:00:00.514 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2298]: Speed/duplex configuration for pfe1 not found. Using 1 Gbps/full-duplex.
Jan 01 00:00:00.514 io_pkt_v6_hc.8 slog 0 INF[src/pfe_hif_drv_sc.c:336]: Attempt to register HIF client: 1
Jan 01 00:00:00.514 io_pkt_v6_hc.8 slog 0 INF[src/pfe_hif_drv_sc.c:1189]: HIF driver started
Jan 01 00:00:00.514 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2363]: New PFE device: 1, ID: 2
Jan 01 00:00:00.514 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2145]: pfe2: Using static PHY mode, RESET=0
Jan 01 00:00:00.514 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:1795]: Adding 00:2a:2b:2c:2d:66 to pfe2
Jan 01 00:00:00.516 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2298]: Speed/duplex configuration for pfe2 not found. Using 1 Gbps/full-duplex.
Jan 01 00:00:00.516 io_pkt_v6_hc.8 slog 0 INF[src/pfe_hif_drv_sc.c:336]: Attempt to register HIF client: 2
Jan 01 00:00:00.516 io_pkt_v6_hc.8 slog 0 INF[src/pfe_hif_drv_sc.c:1189]: HIF driver started
Jan 01 00:00:00.516 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2363]: New PFE device: 2, ID: 4
Jan 01 00:00:00.531 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2702]: Adding 00:0a:0b:0c:0d:66 to pfe0
Jan 01 00:00:00.531 io_pkt_v6_hc.8 slog 0 WRN[src/pfe_drv.c:2707]: Unable to assign MAC address 00:0a:0b:0c:0d:66 to the pfe0
Jan 01 00:00:00.531 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2663]: pfe0: Disabling promiscuous mode
Jan 01 00:00:00.531 io_pkt_v6_hc.8 slog 0 WRN[src/pfe_drv.c:2829]: EMAC speed change for SGMII is currently not supported.
Jan 01 00:00:00.532 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2443]: Adding 33:33:ff:0c:0d:66 to emac0
Jan 01 00:00:00.534 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2663]: pfe0: Disabling promiscuous mode
Jan 01 00:00:00.534 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2443]: Adding 33:33:00:00:00:01 to emac0
Jan 01 00:00:00.536 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2443]: Adding 33:33:ff:0c:0d:66 to emac0
Jan 01 00:00:00.536 io_pkt_v6_hc.8 slog 0 WRN[src/pfe_drv.c:2450]: unable to add 33:33:ff:0c:0d:66 into emac0: 17
Jan 01 00:00:00.536 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2663]: pfe0: Disabling promiscuous mode
Jan 01 00:00:00.536 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2443]: Adding 33:33:00:00:00:01 to emac0
Jan 01 00:00:00.536 io_pkt_v6_hc.8 slog 0 WRN[src/pfe_drv.c:2450]: unable to add 33:33:00:00:00:01 into emac0: 17
Jan 01 00:00:00.536 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2443]: Adding 33:33:ff:0c:0d:66 to emac0
Jan 01 00:00:00.536 io_pkt_v6_hc.8 slog 0 WRN[src/pfe_drv.c:2450]: unable to add 33:33:ff:0c:0d:66 into emac0: 17
Jan 01 00:00:00.536 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2663]: pfe0: Disabling promiscuous mode
Jan 01 00:00:00.536 io_pkt_v6_hc.8 slog 0 WRN[src/pfe_drv.c:2829]: EMAC speed change for SGMII is currently not supported.
Jan 01 00:00:00.536 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2443]: Adding 01:00:5e:00:00:01 to emac0
Jan 01 00:00:00.538 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2443]: Adding 33:33:00:00:00:01 to emac0
Jan 01 00:00:00.538 io_pkt_v6_hc.8 slog 0 WRN[src/pfe_drv.c:2450]: unable to add 33:33:00:00:00:01 into emac0: 17
Jan 01 00:00:00.538 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2443]: Adding 33:33:ff:0c:0d:66 to emac0
Jan 01 00:00:00.538 io_pkt_v6_hc.8 slog 0 WRN[src/pfe_drv.c:2450]: unable to add 33:33:ff:0c:0d:66 into emac0: 17
Jan 01 00:00:00.538 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2663]: pfe0: Disabling promiscuous mode

 

 

# slog2info  | grep io_pkt_v6_hc

Jan 01 00:00:00.052 io_pkt_v6_hc.8 slog* 0 INF[src/pfe_drv.c:1377]: VERSION INFO
Jan 01 00:00:00.052 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:1384]: --- Safe IRQ enabled. No InterrupAttach() or InterruptAttach_r() allowed.
Jan 01 00:00:00.052 io_pkt_v6_hc.8 slog 0 INF[src/pfe_fw.c:83]: 49480 bytes read
Jan 01 00:00:00.052 io_pkt_v6_hc.8 slog 0 INF[src/pfe_fw.c:89]: Loaded firmware file: /proc/boot/s32g_pfe_class.fw
Jan 01 00:00:00.053 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:1477]: MII mode configuration for pfe0/EMAC0 not found. Using SGMII.
Jan 01 00:00:00.053 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:1477]: MII mode configuration for pfe1/EMAC1 not found. Using SGMII.
Jan 01 00:00:00.053 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:1477]: MII mode configuration for pfe2/EMAC2 not found. Using RGMII.
Jan 01 00:00:00.053 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:1495]: Issuing PFE peripheral reset...
Jan 01 00:00:00.274 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:1496]: PFE reset OK.
Jan 01 00:00:00.274 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:3519]: PFE CBUS p0x46000000 mapped @ v0x1abef95000
Jan 01 00:00:00.274 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:3524]: HW version 0x101
Jan 01 00:00:00.274 io_pkt_v6_hc.8 slog 0 INF[src/pfe_hw_feature.c:95]: Silicon S32G3
Jan 01 00:00:00.274 io_pkt_v6_hc.8 slog 0 WRN[hw/s32g/pfe_platform_master.c:3536]: Fail-Stop mode disabled
Jan 01 00:00:00.275 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:2687]: PFE_ERRORS:Parity instance created
Jan 01 00:00:00.275 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:2702]: PFE_ERRORS:Watchdog instance created
Jan 01 00:00:00.275 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:2718]: PFE_ERRORS:Bus Error instance created
Jan 01 00:00:00.275 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:2731]: PFE_ERRORS:FW Fail Stop instance created
Jan 01 00:00:00.275 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:2744]: PFE_ERRORS:Host Fail Stop instance created
Jan 01 00:00:00.275 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:2757]: PFE_ERRORS:Fail Stop instance created
Jan 01 00:00:00.275 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:2770]: PFE_ERRORS:ECC Err instance created
Jan 01 00:00:00.275 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:1766]: BMU1 buffer base: p0xc0000000
Jan 01 00:00:00.277 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:1810]: BMU2 buffer base: p0x83000000 (0x200000 bytes)
Jan 01 00:00:00.279 io_pkt_v6_hc.8 slog 0 WRN[hw/s32g/pfe_platform_master.c:2194]: The option 'g2_ordered_class_writes' is disabled.
Jan 01 00:00:00.279 io_pkt_v6_hc.8 slog 0 INF[src/oal_irq_qnx.c:117]: PFE BMU IRQ Worker started (IRQ ID: 226)
Jan 01 00:00:00.279 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_bmu_csr.c:96]: BMU_EMPTY_INT (BMU @ p0x88000). Pool ready.
Jan 01 00:00:00.279 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_bmu_csr.c:96]: BMU_EMPTY_INT (BMU @ p0x8c000). Pool ready.
Jan 01 00:00:00.281 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:2239]: Firmware .elf detected
Jan 01 00:00:00.281 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:2248]: Uploading CLASS firmware
Jan 01 00:00:00.281 io_pkt_v6_hc.8 slog 0 INF[src/pfe_pe.c:609]: Selected FW loading OPs to load 8 PEs in parallel
Jan 01 00:00:00.285 io_pkt_v6_hc.8 slog 0 INF[src/pfe_pe.c:1945]: pfe_ct.h file version"92367c0e25f21f49217a9b08168ad2c8"
Jan 01 00:00:00.288 io_pkt_v6_hc.8 slog 0 INF[src/pfe_pe.c:2422]: [FW VERSION] 1.6.0, Build: Mar 15 2023, 12:37:54 (), ID: 0x31454650
Jan 01 00:00:00.406 io_pkt_v6_hc.8 slog 0 WRN[hw/s32g/pfe_platform_master.c:2312]: VLAN ID incorrect or not set. Using default VLAN ID = 0x01.
Jan 01 00:00:00.406 io_pkt_v6_hc.8 slog 0 WRN[hw/s32g/pfe_platform_master.c:2318]: VLAN stats size incorrect or not set. Using default VLAN stats size = 20.
Jan 01 00:00:00.406 io_pkt_v6_hc.8 slog 0 INF[src/pfe_l2br.c:1181]: Software vlan hash table @ p0x20001208
Jan 01 00:00:00.406 io_pkt_v6_hc.8 slog 0 INF[src/pfe_l2br.c:1286]: Fall-back bridge domain @ 0x20000a44 (class)
Jan 01 00:00:00.406 io_pkt_v6_hc.8 slog 0 INF[src/pfe_l2br.c:1287]: Default bridge domain @ 0x20000a3c (class)
Jan 01 00:00:00.406 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:2412]: Routing table created, Hash Table @ p0x80014000, Pool @ p0x8001c000 (65536 bytes)
Jan 01 00:00:00.407 io_pkt_v6_hc.8 slog 0 INF[src/pfe_hif_chnl.c:1997]: Initializing RX buffer pool. Depth: 256; Buffer Size: 2048; Cache Line Size: 64
Jan 01 00:00:00.408 io_pkt_v6_hc.8 slog 0 INF[src/pfe_hif_chnl.c:1997]: Initializing RX buffer pool. Depth: 256; Buffer Size: 2048; Cache Line Size: 64
Jan 01 00:00:00.409 io_pkt_v6_hc.8 slog 0 INF[src/pfe_hif_chnl.c:1997]: Initializing RX buffer pool. Depth: 256; Buffer Size: 2048; Cache Line Size: 64
Jan 01 00:00:00.508 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:3705]: Feature err051211_workaround: DISABLED
Jan 01 00:00:00.509 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2145]: pfe0: Using static PHY mode, RESET=0
Jan 01 00:00:00.509 io_pkt_v6_hc.8 slog 0 INF[src/oal_irq_qnx.c:117]: PFE HIF0 IRQ Worker started (IRQ ID: 222)
Jan 01 00:00:00.510 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:1795]: Adding 00:0a:0b:0c:0d:66 to pfe0
Jan 01 00:00:00.512 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2298]: Speed/duplex configuration for pfe0 not found. Using 1 Gbps/full-duplex.
Jan 01 00:00:00.512 io_pkt_v6_hc.8 slog 0 INF[src/pfe_hif_drv_sc.c:336]: Attempt to register HIF client: 0
Jan 01 00:00:00.512 io_pkt_v6_hc.8 slog 0 INF[src/pfe_hif_drv_sc.c:1189]: HIF driver started
Jan 01 00:00:00.512 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2363]: New PFE device: 0, ID: 0
Jan 01 00:00:00.512 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2145]: pfe1: Using static PHY mode, RESET=0
Jan 01 00:00:00.512 io_pkt_v6_hc.8 slog 0 INF[src/oal_irq_qnx.c:117]: PFE HIF1 IRQ Worker started (IRQ ID: 223)
Jan 01 00:00:00.512 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:1795]: Adding 00:1a:1b:1c:1d:66 to pfe1
Jan 01 00:00:00.514 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2298]: Speed/duplex configuration for pfe1 not found. Using 1 Gbps/full-duplex.
Jan 01 00:00:00.514 io_pkt_v6_hc.8 slog 0 INF[src/pfe_hif_drv_sc.c:336]: Attempt to register HIF client: 1
Jan 01 00:00:00.514 io_pkt_v6_hc.8 slog 0 INF[src/pfe_hif_drv_sc.c:1189]: HIF driver started
Jan 01 00:00:00.514 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2363]: New PFE device: 1, ID: 2
Jan 01 00:00:00.514 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2145]: pfe2: Using static PHY mode, RESET=0
Jan 01 00:00:00.514 io_pkt_v6_hc.8 slog 0 INF[src/oal_irq_qnx.c:117]: PFE HIF2 IRQ Worker started (IRQ ID: 224)
Jan 01 00:00:00.514 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:1795]: Adding 00:2a:2b:2c:2d:66 to pfe2
Jan 01 00:00:00.516 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2298]: Speed/duplex configuration for pfe2 not found. Using 1 Gbps/full-duplex.
Jan 01 00:00:00.516 io_pkt_v6_hc.8 slog 0 INF[src/pfe_hif_drv_sc.c:336]: Attempt to register HIF client: 2
Jan 01 00:00:00.516 io_pkt_v6_hc.8 slog 0 INF[src/pfe_hif_drv_sc.c:1189]: HIF driver started
Jan 01 00:00:00.516 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2363]: New PFE device: 2, ID: 4
Jan 01 00:00:00.531 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2702]: Adding 00:0a:0b:0c:0d:66 to pfe0
Jan 01 00:00:00.531 io_pkt_v6_hc.8 slog 0 WRN[src/pfe_drv.c:2707]: Unable to assign MAC address 00:0a:0b:0c:0d:66 to the pfe0
Jan 01 00:00:00.531 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2663]: pfe0: Disabling promiscuous mode
Jan 01 00:00:00.531 io_pkt_v6_hc.8 slog 0 WRN[src/pfe_drv.c:2829]: EMAC speed change for SGMII is currently not supported.
Jan 01 00:00:00.532 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2443]: Adding 33:33:ff:0c:0d:66 to emac0
Jan 01 00:00:00.534 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2663]: pfe0: Disabling promiscuous mode
Jan 01 00:00:00.534 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2443]: Adding 33:33:00:00:00:01 to emac0
Jan 01 00:00:00.536 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2443]: Adding 33:33:ff:0c:0d:66 to emac0
Jan 01 00:00:00.536 io_pkt_v6_hc.8 slog 0 WRN[src/pfe_drv.c:2450]: unable to add 33:33:ff:0c:0d:66 into emac0: 17
Jan 01 00:00:00.536 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2663]: pfe0: Disabling promiscuous mode
Jan 01 00:00:00.536 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2443]: Adding 33:33:00:00:00:01 to emac0
Jan 01 00:00:00.536 io_pkt_v6_hc.8 slog 0 WRN[src/pfe_drv.c:2450]: unable to add 33:33:00:00:00:01 into emac0: 17
Jan 01 00:00:00.536 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2443]: Adding 33:33:ff:0c:0d:66 to emac0
Jan 01 00:00:00.536 io_pkt_v6_hc.8 slog 0 WRN[src/pfe_drv.c:2450]: unable to add 33:33:ff:0c:0d:66 into emac0: 17
Jan 01 00:00:00.536 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2663]: pfe0: Disabling promiscuous mode
Jan 01 00:00:00.536 io_pkt_v6_hc.8 slog 0 WRN[src/pfe_drv.c:2829]: EMAC speed change for SGMII is currently not supported.
Jan 01 00:00:00.536 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2443]: Adding 01:00:5e:00:00:01 to emac0
Jan 01 00:00:00.538 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2443]: Adding 33:33:00:00:00:01 to emac0
Jan 01 00:00:00.538 io_pkt_v6_hc.8 slog 0 WRN[src/pfe_drv.c:2450]: unable to add 33:33:00:00:00:01 into emac0: 17
Jan 01 00:00:00.538 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2443]: Adding 33:33:ff:0c:0d:66 to emac0
Jan 01 00:00:00.538 io_pkt_v6_hc.8 slog 0 WRN[src/pfe_drv.c:2450]: unable to add 33:33:ff:0c:0d:66 into emac0: 17
Jan 01 00:00:00.538 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2663]: pfe0: Disabling promiscuous mode

Process 172057 (slog2info) exited status=0.
Jan 01 00:01:01.630 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2443]: Adding 33:33:00:00:00:01 to emac0
Jan 01 00:01:01.630 io_pkt_v6_hc.8 slog 0 WRN[src/pfe_drv.c:2450]: unable to add 33:33:00:00:00:01 into emac0: 17
Jan 01 00:01:01.630 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2443]: Adding 33:33:ff:0c:0d:66 to emac0
Jan 01 00:01:01.630 io_pkt_v6_hc.8 slog 0 WRN[src/pfe_drv.c:2450]: unable to add 33:33:ff:0c:0d:66 into emac0: 17
Jan 01 00:01:01.630 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2495]: Removing 01:00:5e:00:00:01 from emac0
Jan 01 00:01:01.632 io_pkt_v6_hc.8 slog 0 INF[src/pfe_phy_if.c:2716]: Address 01:00:5e:00:00:01 removed from emac0
Jan 01 00:01:01.632 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2663]: pfe0: Disabling promiscuous mode

0 Kudos
Reply

493 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @Seneca 

Thanks for your reply.

In order for using the PFE drivers for QNX correctly,  you may have to use the versions described below to request integration related support from us.

Would you mind confirming if the QNX SDP 7.1 JBN37 is used or JBN51 is used in your test?(maybe with the name: BSP_nxp-s32g-evb_br-710_be-710_SVN984052_JBN51)

 

chenyin_h_0-1782295257793.png

Additionally, from the integration manual within the 1.4 package, the following u-boot tag is used/tested instead of bsp37.0-2020.04

chenyin_h_1-1782295597816.png

I suggest testing with this combinations firstly for initial analysis.

 

BR

Chenyin

 

0 Kudos
Reply

490 Views
Seneca
Contributor I

Greetings,

I already use the uboot U-Boot 2020.04+g156b168010 from my 37 bsp setup. Can I reuse that and only switch the IFS file on the sdcard? 

Regards

Edit: Oh, and the BSP 37 was recommended to my by your support a few months ago when I tried to get gmac0 running. Might 34 break this?

0 Kudos
Reply

487 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @Seneca 

Thanks for your reply.

From my opinion, I suggest firstly try testing it with QNX SDP 7.1 JBN37 strictly following the PFE_S32G_A53_QNX_IntegrationManual, if no issues with PFE, then checking the GMAC issues if does exist.

 

BR

Chenyin

0 Kudos
Reply

484 Views
Seneca
Contributor I

Is JBN37 the same as BSP37?

BSP37 is what I am using at the moment.BSP_nxp-s32g-rdb3_br-710_be-710_SVN996606_JBN10.zip

I tried to follow the integration manual section 2.6.2 as follows:

Set the uboot variables:

setenv boot_qnx_atf 'mmc dev 0; fatload mmc 0:1 0x83e00000 s32g399a-rdb3.dtb; run atf_fdt_0to3; run atf_fdt_4to7; fatload mmc 0:1 0x80080000 ifs-s32g399a-rdb.ui; pfeng enable; s32ccgmac disable; s32ccgmac enable; bootm 0x80080000 - 0x83E00000'
setenv atf_fdt_0to3 'fdt addr 0x83e00000; fdt resize; fdt set /cpus/cpu@1 cpu-release-addr <0x0 0xa0000010>; fdt set /cpus/cpu@100 cpu-release-addr <0x0 0xa0000010>; fdt set /cpus/cpu@101 cpu-release-addr <0x0 0xa0000010>;'
setenv atf_fdt_4to7 'fdt set /cpus/cpu@2 cpu-release-addr <0x0 0xa0000010>; fdt set /cpus/cpu@3 cpu-release-addr <0x0 0xa0000010>; fdt set /cpus/cpu@102 cpu-release-addr <0x0 0xa0000010>; fdt set /cpus/cpu@103 cpu-release-addr <0x0 0xa0000010>;'
setenv release_cpus 'run cpu_trap; mp 1 release 0xa0000000; mp 2 release 0xa0000000; mp 3 release 0xa0000000; mp 4 release 0xa0000000; mp 5 release 0xa0000000; mp 6 release 0xa0000000; mp 7 release 0xa0000000;'
setenv cpu_trap 'dcache off; mw.l 0xa0000000 0xd503205f; mw.l 0xa0000004 0x58000060; mw.l 0xa0000008 0xb4ffffc0; mw.l 0xa000000C 0xd61f0000; mw.q 0xa0000010 0x00000000; dcache on;'
setenv bootcmd 'run boot_qnx_atf'
setenv hwconfig "pcie0:mode=rc,clock=ext;pcie1:mode=sgmii,clock=ext,fmhz=125,xpcs_mode=2G5"
setenv pfeng_mode 'enable,sgmii,sgmii,rgmii'
setenv s32cc_gmac_mode disable
saveenv
boot

 

When building the ifs image in the .build file, I replaced the networking section with this:

########################################################
## Networking
########################################################
display_msg Starting Networking driver (/dev/socket)...
io-pkt-v6-hc -p tcpip -d pfe-2 pfe0_mac=000a0b0c0d66,pfe1_mac=001a1b1c1d66,
pfe2_mac=002a2b2c2d66,class_fw=/proc/boot/s32g_pfe_class.fw
waitfor /dev/socket 10
# Get IP form DHCP for pfe0 device - optional step
dhclient -m -lf /dev/shmem/dhclient.leases -pf /dev/shmem/dhclient.pid -nw pfe0
cp /proc/boot/libfci_cli /tmp # Optional component

 

And added this in the network driver section:

./../../pfebsp37/PFE-DRV_S32G_A53_QNX_1.4.0/sw/devnp-pfe-2/build/aarch64le-release/devnp-pfe-2.so # PFE driver
# Important - use [+raw] to treat fw as a raw data file
[+raw]./../../pfebsp37/PFE-FE_S32G_1.6.0/s32g_pfe_class.fw
[+raw]./../../pfebsp37/PFE-FE_S32G_1.6.0/s32g_pfe_util.fw
[perms=a+x]libfci_cli # Optional if libfci_cli is needed

In the BSP, I added in src/hardware/startup/boards/s32g/s32g399a-rdb/s32g_init_raminfo.c in s32g_init_raminfo function:

 

kprintf("Reserving RAM region for PFE driver on EVB/RDB\n");
as_add_containing(0x80000000,0x80000000 + 0x70000000 - 1,AS_ATTR_RAM,
"pfe_ddr","ram");

 

Did I miss anything?

 

0 Kudos
Reply

426 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @Seneca 

Thanks for your reply..

BSP 37 is the version number for Linux BSP provisioned by NXP(TFA, U-boot, Linux, etc.), while the JBN37 mentioned is part of the name of certain version QNX BSP release(BSP_nxp-s32g-evb_br-710_be-710_SVN950423_JBN37) provisioned by Blackberry, they are different.

According to the release notes, the QNX PFE Driver 1.4 was developed and tested with the following QNX release:  QNX® SDP 7.1 BuildID 472 (BSP_nxp-s32g-evb_br-710_be-710_SVN950423_JBN37), so I suggest firstly checking with your testing setup if the correct QNX version is used.

However, as shared from your previous reply, BSP_nxp-s32g-rdb3_br-710_be-710_SVN996606_JBN10 was used, which does not match the requirement.

 

BR

Chenyin
 

0 Kudos
Reply

396 Views
Seneca
Contributor I

Greetings,

you recommend a BSP_nxp-s32g-evb* release which looks like for the evb board will this even work with an rdb3 board like mine? Is there a driver compatible with rdb3?

Edit: The only driver version I can find at the moment that lists rdb3 at the moment is 1.9.0 which lists a BSP_nxp-s32g-rdb3_be-800_SVN1011366_JBN153.zip but only for QNX SDP 8.0 not for 7.1.

Are you aware of a package that works with rdb3 and QNX SDP 7.1?

Regards

0 Kudos
Reply

390 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @Seneca 

Thanks for your reply.

If not focused on certain version PFE QNX drivers, I suggest trying PFE QNX driver 1.8 with FW 1.11

1. It is compatible with  QNX® SDP 7.1 BSP for NXP - BuildID 51 (BSP_nxp-s32g-evb_br-710_be-710_SVN984052_JBN51) 

2. It was developed and tested with S32G-VNP-RDB3(although named with ...-evb....)  

Which fulfill your requirements.

 

BR

Chenyin

0 Kudos
Reply

354 Views
Seneca
Contributor I

Ok, so I downloaded the 

BSP_nxp-s32g-evb_br-710_be-710_SVN984052_JBN51

package you mentioned, modified the .build file and add the 

kprintf("Reserving RAM region for PFE driver on EVB/RDB\n");
as_add_containing(0x80000000,0x80000000 + 0x4000000 - 1,AS_ATTR_RAM, "pfe_ddr","ram");

to

src/hardware/startup/boards/s32g/s32g399a-rdb/s32g_init_raminfo.c and replace my ifs file with the resulting ifs-s32g399a-rdb.ui.

Unfortunately, it doesn't seem to execute the pfe_ddr allocation from above. 

Is there anything I need to modify for the uboot parameters or else for this new image to work?

Regards

 

0 Kudos
Reply

63 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @Seneca 

Thanks for your reply.

I suggest referencing the integration manual strictly, refer to the part you mentioned, the following need to be modified before building the QNX BSP.

chenyin_h_0-1782443542271.png

 

BR

Chenyin

0 Kudos
Reply

383 Views
Seneca
Contributor I

I shall try that, tx. 

Can you name me the exact package name in the QNX Software Center? All packages with EVB I see are marked with S32G274A and I don't know if these work with a S32G3 board.

Btw: Some manuals put the *.fw files on the root of the sd card so that uboot can load them with pfeng* commands but it is not part of the integration manuals I have read so far. Is this really necessary or is loading the firmware via io-pkt* enough?

0 Kudos
Reply

374 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @Seneca 

Thanks for your reply.

Sorry that since QNX is 3rd product, we may not be aware of the BSP details/changes released, my feedback is based on available NXP documents.

1. I have just checked the QNX PFE driver 1.7 and 1.8, and found that the integration manual is actually based on QNX PFE driver 1.7, so this version is also correct for your test.

2. From the corresponding document, for QNX PFE driver 1.7, it is compatible with FW 1.10

chenyin_h_0-1782375688288.png

While the name of the QNX BSP is:

chenyin_h_1-1782375744720.png

3. From my previous experience, since there would be some differences across different version QNX PFE drivers, I suggest firstly following the integration manual that is found from certain QNX PFE driver used. 

For other details of QNX BSP itself, I suggest directly contacting QNX support portal

Sorry for your inconvenience

 

BR

Chenyin

 

0 Kudos
Reply