S32G399A-RDB3 QNX PFE Driver Problems

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32G399A-RDB3 QNX PFE Driver Problems

7,014 Views
Seneca
Contributor I

Greetings,

we try to get PFE running on a S32G399A-RDB3 board with QNX. As far as I can tell, this is a valid combination:

BSP 37.0
PFE-FW_S32G_1.7.0
PFE-DRV-S32G_A53_QNX_1.4.0

It ends with a no carrier error on all network interfaces. Plugging the cable into different ethernet ports changes nothing. 

It used to work with gmac0.

Any ideas?

io pkt call:

io-pkt-v6-hc -p tcpip -d pfe-2 pfe0_mac=000a0b0c0d66,pfe1_mac=001a1b1c1d66,pfe2_mac=002a2b2c2d66,class_fw=/proc/boot/s32g_pfe_class.fw,no_reset,mode0=sgmii,phy0=0,mode1=sgmii,phy1=1

Uboot parameters:

Uboot is the same as from the Linux sdcard image with modified parmeters for qnx boot. 

setenv hwconfig "pcie0:mode=rc,clock=ext;pcie1:mode=sgmii,clock=ext,fmhz=125,xpcs_mode=2G5"
setenv pfeng_mode 'enable,sgmii,sgmii,rgmii'
setenv s32cc_gmac_mode disable
setenv pfeng enable; s32ccgmac disable; s32ccgmac enable;
setenv boot_qnx_atf 'mmc dev 0; fatload mmc 0:1 0x83e00000 s32g399a-rdb3.dtb; pfeng enable; s32ccgmac disable; s32ccgmac enable; fatload mmc 0:1 0x80080000 ifs-s32g399a-rdb.ui; bootm 0x80080000 - 0x83E00000'
setenv bootcmd 'run boot_qnx_atf'
saveenv

 

Log:

U-Boot 2020.04+g156b168010 (Jun 09 2023 - 10:14:25 +0000)
 
CPU:   NXP S32G399A rev. 1.1
Model: NXP S32G399A-RDB3
DRAM:  3.5 GiB
MMC:   FSL_SDHC: 0
Loading Environment from MMC... OK
Configuring PCIe0 as RootComplex
PCIe0: Failed to get link up
PCI: Failed autoconfig bar 1c
In:    serial@401c8000
Out:   serial@401c8000
Err:   serial@401c8000
Board revision: RDB3 Revision F
Net:   EQOS phy: rgmii @ 1
 
Warning: eth_eqos (eth0) using random MAC address - 26:e4:e6:43:15:ad
eth0: eth_eqosFailed to get speed of XPCS for emac1_xpcs PFE: emac0: sgmii emac1: sgmii emac2: rgmii
, eth1: eth_pfeng
Hit any key to stop autoboot:  3  2  1  0 
switch to partitions #0, OK
mmc0 is current device
50640 bytes read in 17 ms (2.8 MiB/s)
11948752 bytes read in 540 ms (21.1 MiB/s)
## Booting kernel from Legacy Image at 80080000 ...
   Image Name:   
   Image Type:   AArch64 Linux Kernel Image (uncompressed)
   Data Size:    11948688 Bytes = 11.4 MiB
   Load Address: 80080000
   Entry Point:  80080000
   Verifying Checksum ... OK
## Flattened Device Tree blob at 83e00000
   Booting using the fdt blob at 0x83e00000
   Loading Kernel Image
   Using Device Tree in place at 0000000083e00000, end 0000000083e0f5cf
   fixup: pfe0 set to 00:01:be:be:ef:11
   fixup: pfe1 set to 00:01:be:be:ef:22
   fixup: pfe1: update phy addr to 0x8
   fixup: pfe2 set to 00:01:be:be:ef:33
 
Starting kernel ...
 
Reserving RAM region for PFE driver on EVB/RDB
Done.
ClockCycles samples:
 0 43600679
 1 43600679
 2 43600678
 3 43600679
 4 43600678
 5 43600678
 6 43600678
 7 43600679
All ClockCycles offsets within tolerance
Welcome to QNX Neutrino 7.1.0 on the NXP S32G399A RDB Board!!
Starting watchdog...
Starting serial driver ...
Starting Networking driver (/dev/socket)...
 
Process 4107 (ifconfig) exited status=0.
 
Process 10 (sh) exited status=0.
 
Process 9 (dhclient) exited status=0.
cp: Can't open source file.  (/proc/boot/libfci_cli)
 
Process 20489 (cp) exited status=1.
Starting SPI driver (/dev/spi0,1,2,3,4,5)...
Starting I2C 0/1/2/3/4 driver (/dev/i2c0,1,2,3,4)...
Starting USDHC0 memory card driver...
[00]     SIM="SDMMC" HBA="imx"
[00,0,0] type=00 ver=05 resp=00                       SDMMC:
 
Process 24596 (chkqnx6fs) exited status=0.
 
Process 28692 (mount) exited status=0.
Starting QSPI Flash driver...
Starting USB host driver (/dev/usb/*)
Detected QSPI Flash: Macronix MX25UW512, JEDEC 0xC2 - 0x813A, Size: 0x4000000
Launching devb-umass for /dev/usb/* ...
# 
Process 36891 (sleep) exited status=0.
sh: /var/cetitec2/startup.sh: No such file or directory
 
Process 45081 (sh) terminated signo=0 code=0 by process 0 value=0.
slog2info
 
Jan 01 00:00:00.023                       random.4                  low*     0  qcrypto: loading configuration file '/etc/qcrypto.conf' [qcrypto_common.c(190)]
Jan 01 00:00:00.024                    random.4..0                 slog*   700  Random is using the Fortuna PRNG
Jan 01 00:00:00.031                       random.4                  low      0  qcrypto: 'openssl' plugin loaded [qcrypto_plugins.c(354)]
Jan 01 00:00:00.031                    random.4..0                 slog    700  Selecting timer as an entropy source
Jan 01 00:00:00.032                    random.4..0                 slog    700  Registered path names
Jan 01 00:00:00.032                    random.4..0                 slog    700  random: starting resmgr
Jan 01 00:00:00.032                    random.4..0                 slog    700  random: Daemonizing the process
Jan 01 00:00:00.042             devc_serlinflexd.7                 slog*     0  serlinflexd_interrupt_attach: Attaching to interrupt 114
Jan 01 00:00:00.047                        iopkt.8          main_buffer*     0  tcpip starting
Jan 01 00:00:00.047                        iopkt.8          main_buffer      0  smmu support is disabled
Jan 01 00:00:00.049                        iopkt.8          main_buffer      0  initializing IPsec...
Jan 01 00:00:00.049                        iopkt.8          main_buffer      0   done
 
Jan 01 00:00:00.049                        iopkt.8          main_buffer      0  IPsec: Initialized Security Association Processing.
 
Jan 01 00:00:00.051                        iopkt.8          main_buffer      0  devnp-pfe-2.so pfe0_mac=000a0b0c0d66,pfe1_mac=001a1b1c1d66,pfe2_mac=002a2b2c2d66,class_fw=/proc/boot/s32g_pfe_class.fw,pfe0_mode=sgmii,pfe0_phy=0,pfe1_mode=sgmii,pfe1_phy=1
Jan 01 00:00:00.052                 io_pkt_v6_hc.8                 slog*     0  INF[src/pfe_drv.c:1377]: VERSION INFO
Driver version: 1.4.0
Driver commit hash: 2f3265a49ac18f94ba5e48254c8f870fe7bfc511
PFE_CFG_MULTI_INSTANCE_SUPPORT: 0
PFE_CFG_LOCAL_IF: 6
PFE_CFG_MASTER_IF: 6
PFE_CFG_SC_HIF: 1
PFE_CFG_HIF_RING_LENGTH: 256
PFE_CFG_PFE0_PROMISC: 1
PFE_CFG_PFE1_PROMISC: 1
PFE_CFG_PFE2_PROMISC: 1
 
 
Jan 01 00:00:00.052                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:1384]: --- Safe IRQ enabled. No InterrupAttach() or InterruptAttach_r() allowed.
 
Jan 01 00:00:00.052                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_fw.c:83]: 42792 bytes read
 
Jan 01 00:00:00.053                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_fw.c:89]: Loaded firmware file: /proc/boot/s32g_pfe_class.fw
 
Jan 01 00:00:00.053                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:1477]: MII mode configuration for pfe0/EMAC0 not found. Using SGMII.
 
Jan 01 00:00:00.053                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:1477]: MII mode configuration for pfe1/EMAC1 not found. Using SGMII.
 
Jan 01 00:00:00.053                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:1477]: MII mode configuration for pfe2/EMAC2 not found. Using RGMII.
 
Jan 01 00:00:00.053                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:1495]: Issuing PFE peripheral reset...
 
Jan 01 00:00:00.274                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:1496]: PFE reset OK.
 
Jan 01 00:00:00.274                 io_pkt_v6_hc.8                 slog      0  INF[hw/s32g/pfe_platform_master.c:3519]: PFE CBUS p0x46000000 mapped @ v0x38f2e23000
 
Jan 01 00:00:00.274                 io_pkt_v6_hc.8                 slog      0  INF[hw/s32g/pfe_platform_master.c:3524]: HW version 0x101
 
Jan 01 00:00:00.274                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_hw_feature.c:95]: Silicon S32G3
 
Jan 01 00:00:00.274                 io_pkt_v6_hc.8                 slog      0  WRN[hw/s32g/pfe_platform_master.c:3536]: Fail-Stop mode disabled
 
Jan 01 00:00:00.275                 io_pkt_v6_hc.8                 slog      0  INF[hw/s32g/pfe_platform_master.c:2687]: PFE_ERRORS:Parity instance created
 
Jan 01 00:00:00.275                 io_pkt_v6_hc.8                 slog      0  INF[hw/s32g/pfe_platform_master.c:2702]: PFE_ERRORS:Watchdog instance created
 
Jan 01 00:00:00.275                 io_pkt_v6_hc.8                 slog      0  INF[hw/s32g/pfe_platform_master.c:2718]: PFE_ERRORS:Bus Error instance created
 
Jan 01 00:00:00.275                 io_pkt_v6_hc.8                 slog      0  INF[hw/s32g/pfe_platform_master.c:2731]: PFE_ERRORS:FW Fail Stop instance created
 
Jan 01 00:00:00.275                 io_pkt_v6_hc.8                 slog      0  INF[hw/s32g/pfe_platform_master.c:2744]: PFE_ERRORS:Host Fail Stop instance created
 
Jan 01 00:00:00.275                 io_pkt_v6_hc.8                 slog      0  INF[hw/s32g/pfe_platform_master.c:2757]: PFE_ERRORS:Fail Stop instance created
 
Jan 01 00:00:00.275                 io_pkt_v6_hc.8                 slog      0  INF[hw/s32g/pfe_platform_master.c:2770]: PFE_ERRORS:ECC Err instance created
 
Jan 01 00:00:00.275                 io_pkt_v6_hc.8                 slog      0  INF[hw/s32g/pfe_platform_master.c:1766]: BMU1 buffer base: p0xc0000000
 
Jan 01 00:00:00.277                 io_pkt_v6_hc.8                 slog      0  INF[hw/s32g/pfe_platform_master.c:1810]: BMU2 buffer base: p0x83000000 (0x200000 bytes)
 
Jan 01 00:00:00.279                 io_pkt_v6_hc.8                 slog      0  INF[src/oal_irq_qnx.c:117]: PFE BMU IRQ Worker started (IRQ ID: 226)
 
Jan 01 00:00:00.279                 io_pkt_v6_hc.8                 slog      0  WRN[hw/s32g/pfe_platform_master.c:2194]: The option 'g2_ordered_class_writes' is disabled.
 
Jan 01 00:00:00.279                 io_pkt_v6_hc.8                 slog      0  INF[hw/s32g/pfe_bmu_csr.c:96]: BMU_EMPTY_INT (BMU @ p0x88000). Pool ready.
 
Jan 01 00:00:00.279                 io_pkt_v6_hc.8                 slog      0  INF[hw/s32g/pfe_bmu_csr.c:96]: BMU_EMPTY_INT (BMU @ p0x8c000). Pool ready.
 
Jan 01 00:00:00.281                 io_pkt_v6_hc.8                 slog      0  INF[hw/s32g/pfe_platform_master.c:2239]: Firmware .elf detected
 
Jan 01 00:00:00.281                 io_pkt_v6_hc.8                 slog      0  INF[hw/s32g/pfe_platform_master.c:2248]: Uploading CLASS firmware
 
Jan 01 00:00:00.281                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_pe.c:609]: Selected FW loading OPs to load 8 PEs in parallel
 
Jan 01 00:00:00.285                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_pe.c:1945]: pfe_ct.h file version"92367c0e25f21f49217a9b08168ad2c8"
 
Jan 01 00:00:00.288                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_pe.c:2422]: [FW VERSION] 1.7.0, Build: Jun  2 2023, 13:48:57 (nogitaaa), ID: 0x31454650
 
Jan 01 00:00:00.406                 io_pkt_v6_hc.8                 slog      0  WRN[hw/s32g/pfe_platform_master.c:2312]: VLAN ID incorrect or not set. Using default VLAN ID = 0x01.
 
Jan 01 00:00:00.406                 io_pkt_v6_hc.8                 slog      0  WRN[hw/s32g/pfe_platform_master.c:2318]: VLAN stats size incorrect or not set. Using default VLAN stats size = 20.
 
Jan 01 00:00:00.406                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_l2br.c:1181]: Software vlan hash table @ p0x20001228
 
 
Jan 01 00:00:00.406                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_l2br.c:1286]: Fall-back bridge domain @ 0x20000a7c (class)
 
Jan 01 00:00:00.406                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_l2br.c:1287]: Default bridge domain @ 0x20000a74 (class)
 
Jan 01 00:00:00.406                 io_pkt_v6_hc.8                 slog      0  INF[hw/s32g/pfe_platform_master.c:2412]: Routing table created, Hash Table @ p0x80014000, Pool @ p0x8001c000 (65536 bytes)
 
Jan 01 00:00:00.407                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_hif_chnl.c:1997]: Initializing RX buffer pool. Depth: 256; Buffer Size: 2048; Cache Line Size: 64
 
Jan 01 00:00:00.408                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_hif_chnl.c:1997]: Initializing RX buffer pool. Depth: 256; Buffer Size: 2048; Cache Line Size: 64
 
Jan 01 00:00:00.409                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_hif_chnl.c:1997]: Initializing RX buffer pool. Depth: 256; Buffer Size: 2048; Cache Line Size: 64
 
Jan 01 00:00:00.508                 io_pkt_v6_hc.8                 slog      0  INF[hw/s32g/pfe_platform_master.c:3705]: Feature err051211_workaround: DISABLED
 
Jan 01 00:00:00.509                        iopkt.8          main_buffer      0  pfe0
 
Jan 01 00:00:00.509                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2152]: pfe0: Using PHY mode: MDIO=0, ADDR=0, CLAUSE=0, RESET=0
 
Jan 01 00:00:00.509                 io_pkt_v6_hc.8                 slog      0  INF[src/oal_irq_qnx.c:117]: PFE HIF0 IRQ Worker started (IRQ ID: 222)
 
Jan 01 00:00:00.509                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:1795]: Adding 00:0a:0b:0c:0d:66 to pfe0
 
Jan 01 00:00:00.511                        iopkt.8          main_buffer      0  pfe1
 
Jan 01 00:00:00.511                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2298]: Speed/duplex configuration for pfe0 not found. Using 1 Gbps/full-duplex.
 
Jan 01 00:00:00.511                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_hif_drv_sc.c:336]: Attempt to register HIF client: 0
 
Jan 01 00:00:00.511                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_hif_drv_sc.c:1189]: HIF driver started
 
Jan 01 00:00:00.511                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2363]: New PFE device: 0, ID: 0
 
Jan 01 00:00:00.511                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2152]: pfe1: Using PHY mode: MDIO=1, ADDR=0, CLAUSE=0, RESET=0
 
Jan 01 00:00:00.511                 io_pkt_v6_hc.8                 slog      0  INF[src/oal_irq_qnx.c:117]: PFE HIF1 IRQ Worker started (IRQ ID: 223)
 
Jan 01 00:00:00.511                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:1795]: Adding 00:1a:1b:1c:1d:66 to pfe1
 
Jan 01 00:00:00.513                        iopkt.8          main_buffer      0  pfe2
 
Jan 01 00:00:00.513                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2298]: Speed/duplex configuration for pfe1 not found. Using 1 Gbps/full-duplex.
 
Jan 01 00:00:00.513                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_hif_drv_sc.c:336]: Attempt to register HIF client: 1
 
Jan 01 00:00:00.513                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_hif_drv_sc.c:1189]: HIF driver started
 
Jan 01 00:00:00.513                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2363]: New PFE device: 1, ID: 2
 
Jan 01 00:00:00.513                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2145]: pfe2: Using static PHY mode, RESET=0
 
Jan 01 00:00:00.513                 io_pkt_v6_hc.8                 slog      0  INF[src/oal_irq_qnx.c:117]: PFE HIF2 IRQ Worker started (IRQ ID: 224)
 
Jan 01 00:00:00.513                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:1795]: Adding 00:2a:2b:2c:2d:66 to pfe2
 
Jan 01 00:00:00.515                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2298]: Speed/duplex configuration for pfe2 not found. Using 1 Gbps/full-duplex.
 
Jan 01 00:00:00.515                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_hif_drv_sc.c:336]: Attempt to register HIF client: 2
 
Jan 01 00:00:00.515                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_hif_drv_sc.c:1189]: HIF driver started
 
Jan 01 00:00:00.515                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2363]: New PFE device: 2, ID: 4
 
Jan 01 00:00:00.530                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2702]: Adding 00:0a:0b:0c:0d:66 to pfe0
 
Jan 01 00:00:00.530                 io_pkt_v6_hc.8                 slog      0  WRN[src/pfe_drv.c:2707]: Unable to assign MAC address 00:0a:0b:0c:0d:66 to the pfe0
 
Jan 01 00:00:00.530                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2663]: pfe0: Disabling promiscuous mode
 
Jan 01 00:00:00.538                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_mdio.c:427]: pfe0: PHY @ bus 0 addr 0 not found. Switching to static mode.
 
Jan 01 00:00:00.538                 io_pkt_v6_hc.8                 slog      0  WRN[src/pfe_drv.c:2829]: EMAC speed change for SGMII is currently not supported.
 
Jan 01 00:00:00.538                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2443]: Adding 33:33:ff:0c:0d:66 to emac0
 
Jan 01 00:00:00.540                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2663]: pfe0: Disabling promiscuous mode
 
Jan 01 00:00:00.540                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2443]: Adding 33:33:00:00:00:01 to emac0
 
Jan 01 00:00:00.542                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2443]: Adding 33:33:ff:0c:0d:66 to emac0
 
Jan 01 00:00:00.542                 io_pkt_v6_hc.8                 slog      0  WRN[src/pfe_drv.c:2450]: unable to add 33:33:ff:0c:0d:66 into emac0: 17
 
Jan 01 00:00:00.542                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2663]: pfe0: Disabling promiscuous mode
 
Jan 01 00:00:00.542                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2443]: Adding 33:33:00:00:00:01 to emac0
 
Jan 01 00:00:00.542                 io_pkt_v6_hc.8                 slog      0  WRN[src/pfe_drv.c:2450]: unable to add 33:33:00:00:00:01 into emac0: 17
 
Jan 01 00:00:00.542                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2443]: Adding 33:33:ff:0c:0d:66 to emac0
 
Jan 01 00:00:00.542                 io_pkt_v6_hc.8                 slog      0  WRN[src/pfe_drv.c:2450]: unable to add 33:33:ff:0c:0d:66 into emac0: 17
 
Jan 01 00:00:00.542                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2663]: pfe0: Disabling promiscuous mode
 
Jan 01 00:00:00.542                 io_pkt_v6_hc.8                 slog      0  WRN[src/pfe_drv.c:2829]: EMAC speed change for SGMII is currently not supported.
 
Jan 01 00:00:00.542                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2443]: Adding 01:00:5e:00:00:01 to emac0
 
Jan 01 00:00:00.544                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2443]: Adding 33:33:00:00:00:01 to emac0
 
Jan 01 00:00:00.544                 io_pkt_v6_hc.8                 slog      0  WRN[src/pfe_drv.c:2450]: unable to add 33:33:00:00:00:01 into emac0: 17
 
Jan 01 00:00:00.544                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2443]: Adding 33:33:ff:0c:0d:66 to emac0
 
Jan 01 00:00:00.544                 io_pkt_v6_hc.8                 slog      0  WRN[src/pfe_drv.c:2450]: unable to add 33:33:ff:0c:0d:66 into emac0: 17
 
Jan 01 00:00:00.544                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2663]: pfe0: Disabling promiscuous mode
 
Jan 01 00:00:00.554               spi_master.24585               normal*     0  Starting spi-master resource manager
Jan 01 00:00:00.558               spi_master.24587               normal*     0  Starting spi-master resource manager
Jan 01 00:00:00.561               spi_master.24588               normal*     0  Starting spi-master resource manager
Jan 01 00:00:00.565               spi_master.24589               normal*     0  Starting spi-master resource manager
Jan 01 00:00:00.582          devb_sdmmc_mx8x.24595                 slog*  1800  devb-sdmmc-mx8x 1.00A (Jun 23 2026 09:45:48)
Jan 01 00:00:00.583          devb_sdmmc_mx8x.24595                 slog      0  libcam.so (Jun 22 2020 21:33:15) bver 7010003
Jan 01 00:00:00.594          devb_sdmmc_mx8x.24595                 slog   1800  sdio_cd:  insertion path 0, cd state 0x1
Jan 01 00:00:00.644          devb_sdmmc_mx8x.24595                 slog   1800  SD CID:
Jan 01 00:00:00.644          devb_sdmmc_mx8x.24595                 slog   1800    MID 0x27, OID 0x5048, PNM SD32G
Jan 01 00:00:00.644          devb_sdmmc_mx8x.24595                 slog   1800    PRV 0x62, PSN 0x6c62d132, MDT 4-2023
Jan 01 00:00:00.644          devb_sdmmc_mx8x.24595                 slog   1800  SD CSD:
Jan 01 00:00:00.644          devb_sdmmc_mx8x.24595                 slog   1800    CSD_STRUCTURE 1, SPEC_VERS 0, CCC 0x5b5
Jan 01 00:00:00.644          devb_sdmmc_mx8x.24595                 slog   1800    TAAC 14, NSAC 0, TRAN_SPEED 50
Jan 01 00:00:00.644          devb_sdmmc_mx8x.24595                 slog   1800    C_SIZE 59023, C_SIZE_MULT 0
Jan 01 00:00:00.644          devb_sdmmc_mx8x.24595                 slog   1800    READ_BL_LEN 9, WRITE_BL_LEN 9
Jan 01 00:00:00.644          devb_sdmmc_mx8x.24595                 slog   1800    ERASE GRP_SIZE 0, GRP_MULT 0, SIZE 127
Jan 01 00:00:00.644          devb_sdmmc_mx8x.24595                 slog   1800    blksz 512, sectors 60440576, dtr 25000000
Jan 01 00:00:00.644          devb_sdmmc_mx8x.24595                 slog   1800  SD SW CAPS:
Jan 01 00:00:00.644          devb_sdmmc_mx8x.24595                 slog   1800    bus mode 0x3, cmd sys 0x1
Jan 01 00:00:00.644          devb_sdmmc_mx8x.24595                 slog   1800    drv type 0x1, curr limit 0x1
Jan 01 00:00:00.644          devb_sdmmc_mx8x.24595                 slog   1800    dtr 50000000
Jan 01 00:00:00.644          devb_sdmmc_mx8x.24595                 slog   1800  CFG:  Timing HS, DTR 50000000, Bus Width 4 bit
 
Jan 01 00:00:00.645          devb_sdmmc_mx8x.24595                 slog    100  cam-disk.so (Jun 22 2020 21:33:17)
Jan 01 00:00:00.647          devb_sdmmc_mx8x.24595                 slog      0  scsi_interpret_sense (sdmmc ptl-0:0:0):  cam_status=c4, scsi_status=2, flag=00000040, vuflag=0008, cmd=1a, error=70, sense=5, asc=24, ascq=0
Jan 01 00:00:00.647          devb_sdmmc_mx8x.24595                 slog      0  scsi_interpret_sense (sdmmc ptl-0:0:0):  cam_status=c4, scsi_status=2, flag=00000040, vuflag=0008, cmd=5a, error=70, sense=5, asc=24, ascq=0
Jan 01 00:00:00.647          devb_sdmmc_mx8x.24595                 slog      0  scsi_interpret_sense (sdmmc ptl-0:0:0):  cam_status=c4, scsi_status=2, flag=00000040, vuflag=0008, cmd=5a, error=70, sense=5, asc=24, ascq=0
Jan 01 00:00:01.827          devb_sdmmc_mx8x.24595                 slog   1000  fs-qnx6: Allocation strategy 0
Jan 01 00:00:01.827          devb_sdmmc_mx8x.24595                 slog   1000  fs-qnx6: Use btree directory 0
Jan 01 00:00:01.828          devb_sdmmc_mx8x.24595                 slog   1000  fs-qnx6: fs-qnx6: trim (0,1048576,2) was not requested, and is NOT supported
Jan 01 00:00:01.833               io_usb_otg.36885                 slog*     0  main(453)[tid:1]: io-usb-otg (Jun 13 2020 20:10:17) args: -d hcd-ehci-mx28 ioport=0x44064100,irq=243,ulpi,no_stream,verbose=5 
Jan 01 00:00:01.835           devf_qspi_s32g.36884                 slog*     0  (devf  t1::f3s_qspi_ident:73) Page size: 256
Jan 01 00:00:01.835           devf_qspi_s32g.36884                 slog      0  (devf  t1::f3s_qspi_ident:74) Total chip size: 0x4000000, Unit size: 0x10000
Jan 01 00:00:01.839               io_usb_otg.36885                 slog      0  ehci_init: Initialiaing with sever version: 2 
Jan 01 00:00:01.839               io_usb_otg.36885                 slog      0  ehci_controller_init(4303): devu-hcd-ehci-mx28.so (Apr 19 2024 13:44:54):  args ulpi,no_stream,verbose=5
Jan 01 00:00:01.840               io_usb_otg.36885                 slog      8  usb_enum_port(94)[tid:1]: busno 0, parent -1, port 0, High speed
Jan 01 00:00:01.840               io_usb_otg.36885                 slog     11  usb_client_descriptor_get(198)[tid:1]: (type 1, index 0, length
Jan 01 00:00:01.840               io_usb_otg.36885                 slog     12  usb_device_set_address(245)[tid:1]: b:0 devno 0
Jan 01 00:00:01.840               io_usb_otg.36885                 slog     11  usb_client_descriptor_get(198)[tid:1]: (type 1, index 0, length 18)
Jan 01 00:00:01.841               io_usb_otg.36885                 slog     11  usb_client_descriptor_get(198)[tid:1]: (type 2, index 0, length 9)
Jan 01 00:00:01.841               io_usb_otg.36885                 slog     11  usb_client_descriptor_get(198)[tid:1]: (type 2, index 0, length 25)
Jan 01 00:00:01.841               io_usb_otg.36885                 slog      8  usb_enum_port(141)[tid:1]: vid 0x0000, did 0x0000 enumerated(busno 0, devno 0:0)
Jan 01 00:00:01.841               io_usb_otg.36885                 slog     11  hub_state_inserted(569)[tid:1]: bdentry 0, dentry 0 0
Jan 01 00:00:01.841               io_usb_otg.36885                 slog     13  hub_configuration_enable(263)[tid:1]: 1
Jan 01 00:00:01.943               io_usb_otg.36885                 slog      0  usbh_timeout_init(203)[tid:1]: Complete
Jan 01 00:00:01.954               io_usb_otg.36885                 slog      0  read_vid_pid: ULPI VID 0x0424 PID 0x0009
Jan 01 00:00:01.954               io_usb_otg.36885                 slog      0  s32g_phy_set_vbus: set_vbus off
Jan 01 00:00:01.968               io_usb_otg.36885                 slog      0  s32g_phy_set_vbus: set_vbus on
Jan 01 00:00:01.979               io_usb_otg.36885                 slog      0  ehci_get_port_status(3568 0x44064100): port=0, tpstatus 10100 e_pstatus 8c001000
Jan 01 00:00:01.979               io_usb_otg.36885                 slog      8  usb_enum_port_extract(172)[tid:7]: (busno 0, pdevno 0, portno 1)
Jan 01 00:00:01.979               io_usb_otg.36885                 slog      8  usb_enum_port_extract(192)[tid:7]: status (2)
Jan 01 00:00:01.983               devb_umass.36886                 slog*   900  devb-umass 1.00A (Jun 22 2020 21:33:41)
Jan 01 00:00:01.984               devb_umass.36886                 slog      0  libcam.so (Jun 22 2020 21:33:15) bver 7010003
Jan 01 00:00:01.985               io_usb_otg.36885                 slog      0  usbdi_client_connect(58)[tid:5]: pid 36886 proc=proc/boot/devb-umass usbdi_client 32eebb9a80
Jan 01 00:00:01.986               io_usb_otg.36885                 slog      0  usbdi_resmgr_connect(310)[tid:5]: usbdi_resmgr_connect: pid 36886 usbdi_client 32eebb9a80 
Jan 01 00:00:01.986               devb_umass.36886                 slog      0  usbdi debug path /pps/usb/debug/ doesn't exist
 
Process 49177 (slog2info) exited status=0.
# ifconfig
 
lo0: flags=8049<UP,LOOPBACK,RUNNING,MULTICAST> mtu 33136
inet 127.0.0.1 netmask 0xff000000
inet6 ::1 prefixlen 128
inet6 fe80::1%lo0 prefixlen 64 scopeid 0x1
pfe0: flags=8843<UP,BROADCAST,RUNNING,SIMPLEX,MULTICAST> mtu 1500
capabilities=1f<IP4CSUM,TCP4CSUM,UDP4CSUM,TCP6CSUM,UDP6CSUM>
enabled=0
address: 00:0a:0b:0c:0d:66
media: Ethernet none (1000baseT full-duplex)
status: active
inet 0.0.0.0 netmask 0xff000000 broadcast 255.255.255.255
inet6 fe80::20a:bff:fe0c:d66%pfe0 prefixlen 64 scopeid 0x11
pfe1: flags=8802<BROADCAST,SIMPLEX,MULTICAST> mtu 1500
capabilities=1f<IP4CSUM,TCP4CSUM,UDP4CSUM,TCP6CSUM,UDP6CSUM>
enabled=0
address: 00:1a:1b:1c:1d:66
media: Ethernet none (1000baseT full-duplex)
status: no carrier
pfe2: flags=8802<BROADCAST,SIMPLEX,MULTICAST> mtu 1500
capabilities=1f<IP4CSUM,TCP4CSUM,UDP4CSUM,TCP6CSUM,UDP6CSUM>
enabled=0
address: 00:2a:2b:2c:2d:66
media: Ethernet none (1000baseT full-duplex)
status: no carrier
 
Process 57369 (ifconfig) exited status=0.
# 
0 Kudos
Reply
54 Replies

1,150 Views
Seneca
Contributor I

Another thing. Will this uboot line recommended in the integration manual:

hwconfig "serdes0:mode=pcie,clock=ext;pcie0:mode=rc;serdes1:mode=xpcs0&xpcs1,clock=ext,fmhz=125;xpcs1_0:speed=2G5;xpcs1_1:speed=1G"

Really enable gmac0, pfe0 and pfe2 as individual interfaces or only two of them?

0 Kudos
Reply

1,149 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @Seneca 

Thanks for your reply.

1. For the hwconfig you mentioned, when using them on RDB3, the 3 MACs could all be used.

2. For the error log you shared, sorry that we do not commonly support QNX commands directly, form my personal experience, it may caused by the command used itself, I suggest  re-checking syntax of commands based on the QNX document.

3. Under QNX, there are some limitation for the PFE driver, auto-negotiation is not supported, so you may make sure that the two sides are running with the same speed.

chenyin_h_0-1784104171784.png

 

BR

Chenyin

0 Kudos
Reply

1,136 Views
Seneca
Contributor I

Greetings,

I recorded the network adapter state of a LInux Laptop that successfully connects to the TC387 media converter (which should be in 100T1 master mode). Can you tell me if pfe2 can drive this mode?

 

  *-network:1
       description: Ethernet interface
       physical id: e
       bus info: usb@2:4
       logical name: enx00e04c680383
       serial: 00:e0:4c:68:03:83
       size: 100Mbit/s
       capacity: 1Gbit/s
       capabilities: ethernet physical tp mii 10bt 10bt-fd 100bt 100bt-fd 1000bt 1000bt-fd autonegotiation
       configuration: autonegotiation=on broadcast=yes driver=r8152 driverversion=v1.12.13 duplex=full firmware=rtl8153b-2 v2 04/27/23 ip=192.168.10.102 link=yes multicast=yes port=MII speed=100Mbit/s
       
       
       NIC statistics:
     tx_packets: 60
     rx_packets: 3
     tx_errors: 0
     rx_errors: 0
     rx_missed: 0
     align_errors: 0
     tx_single_collisions: 0
     tx_multi_collisions: 0
     rx_unicast: 3
     rx_broadcast: 0
     rx_multicast: 0
     tx_aborted: 0
     tx_underrun: 0
     
     
     enx00e04c680383: flags=4163<UP,BROADCAST,RUNNING,MULTICAST>  mtu 1500
        inet 192.168.10.102  netmask 255.255.255.0  broadcast 192.168.10.255
        inet6 fe80::9165:ed06:804a:54c0  prefixlen 64  scopeid 0x20<link>
        ether 00:e0:4c:68:03:83  txqueuelen 1000  (Ethernet)
        RX packets 0  bytes 0 (0.0 B)
        RX errors 0  dropped 0  overruns 0  frame 0
        TX packets 0  bytes 0 (0.0 B)
        TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0
        
        
        Settings for enx00e04c680383:
Supported ports: [ TP MII ]
Supported link modes:   10baseT/Half 10baseT/Full
                        100baseT/Half 100baseT/Full
                        1000baseT/Half 1000baseT/Full
Supported pause frame use: No
Supports auto-negotiation: Yes
Supported FEC modes: Not reported
Advertised link modes:  10baseT/Half 10baseT/Full
                        100baseT/Half 100baseT/Full
                        1000baseT/Full
Advertised pause frame use: No
Advertised auto-negotiation: Yes
Advertised FEC modes: Not reported
Link partner advertised link modes:  10baseT/Half 10baseT/Full
                                     100baseT/Half 100baseT/Full
Link partner advertised pause frame use: No
Link partner advertised auto-negotiation: Yes
Link partner advertised FEC modes: Not reported
Speed: 100Mb/s
Duplex: Full
Auto-negotiation: on
Port: MII
PHYAD: 32
Transceiver: internal
Supports Wake-on: pumbg
Wake-on: g
        Current message level: 0x00007fff (32767)
                               drv probe link timer ifdown ifup rx_err tx_err tx_queued intr tx_done rx_status pktdata hw wol
Link detected: yes

 

0 Kudos
Reply

1,132 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @Seneca 

Thanks for your post.

1. I can confirm that the PFE2 port on RDB3 could work correctly with connection to 100T1 network via a 100base-TX<->100base-T1 converter under Linux BSP provisioned by NXP.

2. You may try the following command for a test: io-pkt-v6-hc -p tcpip -d pfe2_link=100-1-2 

But I am not very sure for these settings on QNX since it is beyond our S32G community supporting scope,  sorry for your inconvenience.


BR

Chenyin

 

0 Kudos
Reply

1,142 Views
Seneca
Contributor I

Greetings,

I tried setting the correct speed on QNX with something like

ifconfig pfe2 media 100baseTX mediaopt full-duplex

but it wasn't enough. Do I have to do something else, maybe even in uboot parameters?

Regards

0 Kudos
Reply

1,151 Views
Seneca
Contributor I

Greetings,

after more research it seem that pfe_mac2 in particular has problems with our 100T1 ethernet adapters. Connecting a Linux Laptop with USB ethernet works fine though.

Do you know if pfe_mac2 can connect to this adapter type correctly and if I have to do something special to make it work?

Regards

0 Kudos
Reply

1,153 Views
Seneca
Contributor I

Ok, so I should be able to use, from the three stacked ports, left port as pfe0 and top center as pfe2 I presume. Bottom center for gmac0.

Now, I try to start the interfaces in bridge mode using the following io pkt syntax (note the bridge parameter behind tcp ip):

io-pkt-v6-hc -p tcpip bridge pkt_typed_mem=pfe_ddr -d dwceqos-s32g mac=`genmac-random -m`,ptp_off,verbose=5 -d /proc/boot/devnp-pfe-2.so pfe0_mac=000a0b0c0d66,pfe1_mac=001a1b1c1d66,pfe2_mac=002a2b2c2d66,class_fw=/proc/boot/s32g_pfe_class.fw,util_fw=/proc/boot/s32g_pfe_util.fw
ifconfig dwc0 192.168.10.100 up
ifconfig pfe0 0.0.0.0 up
ifconfig pfe2 0.0.0.0 up
ifconfig bridge0 create
ifconfig bridge0 add dwc0 add pfe0 add pfe2 up

This will result in lots of memory errors in slog2info

Jan 01 00:04:37.485 io_pkt_v6_hc.159753 slog 0 ERR[src/pfe_drv.c:2996]: (DRIVER) event 1 - Driver runtime error: Mbuf addr out of 32bit. Start @ p0x8df239b58 end @ p0x8df239b82

Jan 01 00:04:38.485 io_pkt_v6_hc.159753 slog 0 ERR[src/pfe_drv.c:2996]: (DRIVER) event 1 - Driver runtime error: Mbuf addr out of 32bit. Start @ p0x8df239558 end @ p0x8df239582

Jan 01 00:04:38.485 io_pkt_v6_hc.159753 slog 0 ERR[src/pfe_drv.c:2996]: (DRIVER) event 1 - Driver runtime error: Mbuf addr out of 32bit. Start @ p0x8df239558 end @ p0x8df239582

Jan 01 00:04:39.451 io_pkt_v6_hc.159753 slog 0 ERR[src/pfe_drv.c:2996]: (DRIVER) event 1 - Driver runtime error: Mbuf addr out of 32bit. Start @ p0x8df239b58 end @ p0x8df239b82

Jan 01 00:04:39.451 io_pkt_v6_hc.159753 slog 0 ERR[src/pfe_drv.c:2996]: (DRIVER) event 1 - Driver runtime error: Mbuf addr out of 32bit. Start @ p0x8df239b58 end @ p0x8df239b82

Is bridge parameter correct in io-pkt-v6-hc call? 

Also, I use this allocation from the driver integration manual for both gmac0 and pfe as can be seen in the io-pkt-v6-hc call. Is that a problem?

kprintf("Reserving RAM region for PFE driver on EVB/RDB\n");
as_add_containing(0x80000000,0x80000000 + 0x4000000 - 1,AS_ATTR_RAM, "pfe_ddr","ram");

0 Kudos
Reply

1,209 Views
Seneca
Contributor I

Greetings,

when I connect the TC387 to my Linux desktop there are lots of arp/icmp messages produced immediately. The same when I connect my S32G pfe2 port to the Linux desktop. But when I connect the TC387 to the S32G pfe2 port I get not arp or icmp messages at all.

For which error messages should I look?

Regards

0 Kudos
Reply

1,344 Views
Seneca
Contributor I

Greetings,

can you tell me if 192.168.0.200 listens to broadcast calls or something like that?

Regards

0 Kudos
Reply

1,300 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @Seneca 

Thanks for your reply.

This IP could receive the broadcast packets from linked devices.

 

BR

Chenyin

0 Kudos
Reply

1,353 Views
Seneca
Contributor I

Greetings,

init_serdes();

has been commented out from the s32g399a-rdb main.c.

Regards

0 Kudos
Reply

1,441 Views
Seneca
Contributor I

Greetings,

I intend to try the following combination:

BSP 33

PFE Driver 1.2.0

PFE FW 1.3.0

Is this officially supported?

Regards

0 Kudos
Reply

1,361 Views
chenyin_h
NXP Employee
NXP Employee

Hello. @Seneca 

Thanks for your reply.

1. For the combination, I suggest referencing the documents included in the QNX PFE drivers directly, which included the recommended/tested combination.

Other combination may or may not work, you may test it accordingly if indeed needed.

2. From the available information, for QNX PFE drive 1.2, the supported PFE FW is 1.2 with BSP30 used for test

 

BR

Chenyin

0 Kudos
Reply