S32G399A-RDB3 QNX PFE Driver Problems

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32G399A-RDB3 QNX PFE Driver Problems

6,033 Views
Seneca
Contributor I

Greetings,

we try to get PFE running on a S32G399A-RDB3 board with QNX. As far as I can tell, this is a valid combination:

BSP 37.0
PFE-FW_S32G_1.7.0
PFE-DRV-S32G_A53_QNX_1.4.0

It ends with a no carrier error on all network interfaces. Plugging the cable into different ethernet ports changes nothing. 

It used to work with gmac0.

Any ideas?

io pkt call:

io-pkt-v6-hc -p tcpip -d pfe-2 pfe0_mac=000a0b0c0d66,pfe1_mac=001a1b1c1d66,pfe2_mac=002a2b2c2d66,class_fw=/proc/boot/s32g_pfe_class.fw,no_reset,mode0=sgmii,phy0=0,mode1=sgmii,phy1=1

Uboot parameters:

Uboot is the same as from the Linux sdcard image with modified parmeters for qnx boot. 

setenv hwconfig "pcie0:mode=rc,clock=ext;pcie1:mode=sgmii,clock=ext,fmhz=125,xpcs_mode=2G5"
setenv pfeng_mode 'enable,sgmii,sgmii,rgmii'
setenv s32cc_gmac_mode disable
setenv pfeng enable; s32ccgmac disable; s32ccgmac enable;
setenv boot_qnx_atf 'mmc dev 0; fatload mmc 0:1 0x83e00000 s32g399a-rdb3.dtb; pfeng enable; s32ccgmac disable; s32ccgmac enable; fatload mmc 0:1 0x80080000 ifs-s32g399a-rdb.ui; bootm 0x80080000 - 0x83E00000'
setenv bootcmd 'run boot_qnx_atf'
saveenv

 

Log:

U-Boot 2020.04+g156b168010 (Jun 09 2023 - 10:14:25 +0000)
 
CPU:   NXP S32G399A rev. 1.1
Model: NXP S32G399A-RDB3
DRAM:  3.5 GiB
MMC:   FSL_SDHC: 0
Loading Environment from MMC... OK
Configuring PCIe0 as RootComplex
PCIe0: Failed to get link up
PCI: Failed autoconfig bar 1c
In:    serial@401c8000
Out:   serial@401c8000
Err:   serial@401c8000
Board revision: RDB3 Revision F
Net:   EQOS phy: rgmii @ 1
 
Warning: eth_eqos (eth0) using random MAC address - 26:e4:e6:43:15:ad
eth0: eth_eqosFailed to get speed of XPCS for emac1_xpcs PFE: emac0: sgmii emac1: sgmii emac2: rgmii
, eth1: eth_pfeng
Hit any key to stop autoboot:  3  2  1  0 
switch to partitions #0, OK
mmc0 is current device
50640 bytes read in 17 ms (2.8 MiB/s)
11948752 bytes read in 540 ms (21.1 MiB/s)
## Booting kernel from Legacy Image at 80080000 ...
   Image Name:   
   Image Type:   AArch64 Linux Kernel Image (uncompressed)
   Data Size:    11948688 Bytes = 11.4 MiB
   Load Address: 80080000
   Entry Point:  80080000
   Verifying Checksum ... OK
## Flattened Device Tree blob at 83e00000
   Booting using the fdt blob at 0x83e00000
   Loading Kernel Image
   Using Device Tree in place at 0000000083e00000, end 0000000083e0f5cf
   fixup: pfe0 set to 00:01:be:be:ef:11
   fixup: pfe1 set to 00:01:be:be:ef:22
   fixup: pfe1: update phy addr to 0x8
   fixup: pfe2 set to 00:01:be:be:ef:33
 
Starting kernel ...
 
Reserving RAM region for PFE driver on EVB/RDB
Done.
ClockCycles samples:
 0 43600679
 1 43600679
 2 43600678
 3 43600679
 4 43600678
 5 43600678
 6 43600678
 7 43600679
All ClockCycles offsets within tolerance
Welcome to QNX Neutrino 7.1.0 on the NXP S32G399A RDB Board!!
Starting watchdog...
Starting serial driver ...
Starting Networking driver (/dev/socket)...
 
Process 4107 (ifconfig) exited status=0.
 
Process 10 (sh) exited status=0.
 
Process 9 (dhclient) exited status=0.
cp: Can't open source file.  (/proc/boot/libfci_cli)
 
Process 20489 (cp) exited status=1.
Starting SPI driver (/dev/spi0,1,2,3,4,5)...
Starting I2C 0/1/2/3/4 driver (/dev/i2c0,1,2,3,4)...
Starting USDHC0 memory card driver...
[00]     SIM="SDMMC" HBA="imx"
[00,0,0] type=00 ver=05 resp=00                       SDMMC:
 
Process 24596 (chkqnx6fs) exited status=0.
 
Process 28692 (mount) exited status=0.
Starting QSPI Flash driver...
Starting USB host driver (/dev/usb/*)
Detected QSPI Flash: Macronix MX25UW512, JEDEC 0xC2 - 0x813A, Size: 0x4000000
Launching devb-umass for /dev/usb/* ...
# 
Process 36891 (sleep) exited status=0.
sh: /var/cetitec2/startup.sh: No such file or directory
 
Process 45081 (sh) terminated signo=0 code=0 by process 0 value=0.
slog2info
 
Jan 01 00:00:00.023                       random.4                  low*     0  qcrypto: loading configuration file '/etc/qcrypto.conf' [qcrypto_common.c(190)]
Jan 01 00:00:00.024                    random.4..0                 slog*   700  Random is using the Fortuna PRNG
Jan 01 00:00:00.031                       random.4                  low      0  qcrypto: 'openssl' plugin loaded [qcrypto_plugins.c(354)]
Jan 01 00:00:00.031                    random.4..0                 slog    700  Selecting timer as an entropy source
Jan 01 00:00:00.032                    random.4..0                 slog    700  Registered path names
Jan 01 00:00:00.032                    random.4..0                 slog    700  random: starting resmgr
Jan 01 00:00:00.032                    random.4..0                 slog    700  random: Daemonizing the process
Jan 01 00:00:00.042             devc_serlinflexd.7                 slog*     0  serlinflexd_interrupt_attach: Attaching to interrupt 114
Jan 01 00:00:00.047                        iopkt.8          main_buffer*     0  tcpip starting
Jan 01 00:00:00.047                        iopkt.8          main_buffer      0  smmu support is disabled
Jan 01 00:00:00.049                        iopkt.8          main_buffer      0  initializing IPsec...
Jan 01 00:00:00.049                        iopkt.8          main_buffer      0   done
 
Jan 01 00:00:00.049                        iopkt.8          main_buffer      0  IPsec: Initialized Security Association Processing.
 
Jan 01 00:00:00.051                        iopkt.8          main_buffer      0  devnp-pfe-2.so pfe0_mac=000a0b0c0d66,pfe1_mac=001a1b1c1d66,pfe2_mac=002a2b2c2d66,class_fw=/proc/boot/s32g_pfe_class.fw,pfe0_mode=sgmii,pfe0_phy=0,pfe1_mode=sgmii,pfe1_phy=1
Jan 01 00:00:00.052                 io_pkt_v6_hc.8                 slog*     0  INF[src/pfe_drv.c:1377]: VERSION INFO
Driver version: 1.4.0
Driver commit hash: 2f3265a49ac18f94ba5e48254c8f870fe7bfc511
PFE_CFG_MULTI_INSTANCE_SUPPORT: 0
PFE_CFG_LOCAL_IF: 6
PFE_CFG_MASTER_IF: 6
PFE_CFG_SC_HIF: 1
PFE_CFG_HIF_RING_LENGTH: 256
PFE_CFG_PFE0_PROMISC: 1
PFE_CFG_PFE1_PROMISC: 1
PFE_CFG_PFE2_PROMISC: 1
 
 
Jan 01 00:00:00.052                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:1384]: --- Safe IRQ enabled. No InterrupAttach() or InterruptAttach_r() allowed.
 
Jan 01 00:00:00.052                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_fw.c:83]: 42792 bytes read
 
Jan 01 00:00:00.053                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_fw.c:89]: Loaded firmware file: /proc/boot/s32g_pfe_class.fw
 
Jan 01 00:00:00.053                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:1477]: MII mode configuration for pfe0/EMAC0 not found. Using SGMII.
 
Jan 01 00:00:00.053                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:1477]: MII mode configuration for pfe1/EMAC1 not found. Using SGMII.
 
Jan 01 00:00:00.053                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:1477]: MII mode configuration for pfe2/EMAC2 not found. Using RGMII.
 
Jan 01 00:00:00.053                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:1495]: Issuing PFE peripheral reset...
 
Jan 01 00:00:00.274                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:1496]: PFE reset OK.
 
Jan 01 00:00:00.274                 io_pkt_v6_hc.8                 slog      0  INF[hw/s32g/pfe_platform_master.c:3519]: PFE CBUS p0x46000000 mapped @ v0x38f2e23000
 
Jan 01 00:00:00.274                 io_pkt_v6_hc.8                 slog      0  INF[hw/s32g/pfe_platform_master.c:3524]: HW version 0x101
 
Jan 01 00:00:00.274                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_hw_feature.c:95]: Silicon S32G3
 
Jan 01 00:00:00.274                 io_pkt_v6_hc.8                 slog      0  WRN[hw/s32g/pfe_platform_master.c:3536]: Fail-Stop mode disabled
 
Jan 01 00:00:00.275                 io_pkt_v6_hc.8                 slog      0  INF[hw/s32g/pfe_platform_master.c:2687]: PFE_ERRORS:Parity instance created
 
Jan 01 00:00:00.275                 io_pkt_v6_hc.8                 slog      0  INF[hw/s32g/pfe_platform_master.c:2702]: PFE_ERRORS:Watchdog instance created
 
Jan 01 00:00:00.275                 io_pkt_v6_hc.8                 slog      0  INF[hw/s32g/pfe_platform_master.c:2718]: PFE_ERRORS:Bus Error instance created
 
Jan 01 00:00:00.275                 io_pkt_v6_hc.8                 slog      0  INF[hw/s32g/pfe_platform_master.c:2731]: PFE_ERRORS:FW Fail Stop instance created
 
Jan 01 00:00:00.275                 io_pkt_v6_hc.8                 slog      0  INF[hw/s32g/pfe_platform_master.c:2744]: PFE_ERRORS:Host Fail Stop instance created
 
Jan 01 00:00:00.275                 io_pkt_v6_hc.8                 slog      0  INF[hw/s32g/pfe_platform_master.c:2757]: PFE_ERRORS:Fail Stop instance created
 
Jan 01 00:00:00.275                 io_pkt_v6_hc.8                 slog      0  INF[hw/s32g/pfe_platform_master.c:2770]: PFE_ERRORS:ECC Err instance created
 
Jan 01 00:00:00.275                 io_pkt_v6_hc.8                 slog      0  INF[hw/s32g/pfe_platform_master.c:1766]: BMU1 buffer base: p0xc0000000
 
Jan 01 00:00:00.277                 io_pkt_v6_hc.8                 slog      0  INF[hw/s32g/pfe_platform_master.c:1810]: BMU2 buffer base: p0x83000000 (0x200000 bytes)
 
Jan 01 00:00:00.279                 io_pkt_v6_hc.8                 slog      0  INF[src/oal_irq_qnx.c:117]: PFE BMU IRQ Worker started (IRQ ID: 226)
 
Jan 01 00:00:00.279                 io_pkt_v6_hc.8                 slog      0  WRN[hw/s32g/pfe_platform_master.c:2194]: The option 'g2_ordered_class_writes' is disabled.
 
Jan 01 00:00:00.279                 io_pkt_v6_hc.8                 slog      0  INF[hw/s32g/pfe_bmu_csr.c:96]: BMU_EMPTY_INT (BMU @ p0x88000). Pool ready.
 
Jan 01 00:00:00.279                 io_pkt_v6_hc.8                 slog      0  INF[hw/s32g/pfe_bmu_csr.c:96]: BMU_EMPTY_INT (BMU @ p0x8c000). Pool ready.
 
Jan 01 00:00:00.281                 io_pkt_v6_hc.8                 slog      0  INF[hw/s32g/pfe_platform_master.c:2239]: Firmware .elf detected
 
Jan 01 00:00:00.281                 io_pkt_v6_hc.8                 slog      0  INF[hw/s32g/pfe_platform_master.c:2248]: Uploading CLASS firmware
 
Jan 01 00:00:00.281                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_pe.c:609]: Selected FW loading OPs to load 8 PEs in parallel
 
Jan 01 00:00:00.285                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_pe.c:1945]: pfe_ct.h file version"92367c0e25f21f49217a9b08168ad2c8"
 
Jan 01 00:00:00.288                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_pe.c:2422]: [FW VERSION] 1.7.0, Build: Jun  2 2023, 13:48:57 (nogitaaa), ID: 0x31454650
 
Jan 01 00:00:00.406                 io_pkt_v6_hc.8                 slog      0  WRN[hw/s32g/pfe_platform_master.c:2312]: VLAN ID incorrect or not set. Using default VLAN ID = 0x01.
 
Jan 01 00:00:00.406                 io_pkt_v6_hc.8                 slog      0  WRN[hw/s32g/pfe_platform_master.c:2318]: VLAN stats size incorrect or not set. Using default VLAN stats size = 20.
 
Jan 01 00:00:00.406                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_l2br.c:1181]: Software vlan hash table @ p0x20001228
 
 
Jan 01 00:00:00.406                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_l2br.c:1286]: Fall-back bridge domain @ 0x20000a7c (class)
 
Jan 01 00:00:00.406                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_l2br.c:1287]: Default bridge domain @ 0x20000a74 (class)
 
Jan 01 00:00:00.406                 io_pkt_v6_hc.8                 slog      0  INF[hw/s32g/pfe_platform_master.c:2412]: Routing table created, Hash Table @ p0x80014000, Pool @ p0x8001c000 (65536 bytes)
 
Jan 01 00:00:00.407                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_hif_chnl.c:1997]: Initializing RX buffer pool. Depth: 256; Buffer Size: 2048; Cache Line Size: 64
 
Jan 01 00:00:00.408                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_hif_chnl.c:1997]: Initializing RX buffer pool. Depth: 256; Buffer Size: 2048; Cache Line Size: 64
 
Jan 01 00:00:00.409                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_hif_chnl.c:1997]: Initializing RX buffer pool. Depth: 256; Buffer Size: 2048; Cache Line Size: 64
 
Jan 01 00:00:00.508                 io_pkt_v6_hc.8                 slog      0  INF[hw/s32g/pfe_platform_master.c:3705]: Feature err051211_workaround: DISABLED
 
Jan 01 00:00:00.509                        iopkt.8          main_buffer      0  pfe0
 
Jan 01 00:00:00.509                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2152]: pfe0: Using PHY mode: MDIO=0, ADDR=0, CLAUSE=0, RESET=0
 
Jan 01 00:00:00.509                 io_pkt_v6_hc.8                 slog      0  INF[src/oal_irq_qnx.c:117]: PFE HIF0 IRQ Worker started (IRQ ID: 222)
 
Jan 01 00:00:00.509                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:1795]: Adding 00:0a:0b:0c:0d:66 to pfe0
 
Jan 01 00:00:00.511                        iopkt.8          main_buffer      0  pfe1
 
Jan 01 00:00:00.511                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2298]: Speed/duplex configuration for pfe0 not found. Using 1 Gbps/full-duplex.
 
Jan 01 00:00:00.511                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_hif_drv_sc.c:336]: Attempt to register HIF client: 0
 
Jan 01 00:00:00.511                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_hif_drv_sc.c:1189]: HIF driver started
 
Jan 01 00:00:00.511                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2363]: New PFE device: 0, ID: 0
 
Jan 01 00:00:00.511                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2152]: pfe1: Using PHY mode: MDIO=1, ADDR=0, CLAUSE=0, RESET=0
 
Jan 01 00:00:00.511                 io_pkt_v6_hc.8                 slog      0  INF[src/oal_irq_qnx.c:117]: PFE HIF1 IRQ Worker started (IRQ ID: 223)
 
Jan 01 00:00:00.511                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:1795]: Adding 00:1a:1b:1c:1d:66 to pfe1
 
Jan 01 00:00:00.513                        iopkt.8          main_buffer      0  pfe2
 
Jan 01 00:00:00.513                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2298]: Speed/duplex configuration for pfe1 not found. Using 1 Gbps/full-duplex.
 
Jan 01 00:00:00.513                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_hif_drv_sc.c:336]: Attempt to register HIF client: 1
 
Jan 01 00:00:00.513                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_hif_drv_sc.c:1189]: HIF driver started
 
Jan 01 00:00:00.513                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2363]: New PFE device: 1, ID: 2
 
Jan 01 00:00:00.513                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2145]: pfe2: Using static PHY mode, RESET=0
 
Jan 01 00:00:00.513                 io_pkt_v6_hc.8                 slog      0  INF[src/oal_irq_qnx.c:117]: PFE HIF2 IRQ Worker started (IRQ ID: 224)
 
Jan 01 00:00:00.513                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:1795]: Adding 00:2a:2b:2c:2d:66 to pfe2
 
Jan 01 00:00:00.515                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2298]: Speed/duplex configuration for pfe2 not found. Using 1 Gbps/full-duplex.
 
Jan 01 00:00:00.515                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_hif_drv_sc.c:336]: Attempt to register HIF client: 2
 
Jan 01 00:00:00.515                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_hif_drv_sc.c:1189]: HIF driver started
 
Jan 01 00:00:00.515                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2363]: New PFE device: 2, ID: 4
 
Jan 01 00:00:00.530                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2702]: Adding 00:0a:0b:0c:0d:66 to pfe0
 
Jan 01 00:00:00.530                 io_pkt_v6_hc.8                 slog      0  WRN[src/pfe_drv.c:2707]: Unable to assign MAC address 00:0a:0b:0c:0d:66 to the pfe0
 
Jan 01 00:00:00.530                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2663]: pfe0: Disabling promiscuous mode
 
Jan 01 00:00:00.538                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_mdio.c:427]: pfe0: PHY @ bus 0 addr 0 not found. Switching to static mode.
 
Jan 01 00:00:00.538                 io_pkt_v6_hc.8                 slog      0  WRN[src/pfe_drv.c:2829]: EMAC speed change for SGMII is currently not supported.
 
Jan 01 00:00:00.538                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2443]: Adding 33:33:ff:0c:0d:66 to emac0
 
Jan 01 00:00:00.540                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2663]: pfe0: Disabling promiscuous mode
 
Jan 01 00:00:00.540                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2443]: Adding 33:33:00:00:00:01 to emac0
 
Jan 01 00:00:00.542                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2443]: Adding 33:33:ff:0c:0d:66 to emac0
 
Jan 01 00:00:00.542                 io_pkt_v6_hc.8                 slog      0  WRN[src/pfe_drv.c:2450]: unable to add 33:33:ff:0c:0d:66 into emac0: 17
 
Jan 01 00:00:00.542                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2663]: pfe0: Disabling promiscuous mode
 
Jan 01 00:00:00.542                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2443]: Adding 33:33:00:00:00:01 to emac0
 
Jan 01 00:00:00.542                 io_pkt_v6_hc.8                 slog      0  WRN[src/pfe_drv.c:2450]: unable to add 33:33:00:00:00:01 into emac0: 17
 
Jan 01 00:00:00.542                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2443]: Adding 33:33:ff:0c:0d:66 to emac0
 
Jan 01 00:00:00.542                 io_pkt_v6_hc.8                 slog      0  WRN[src/pfe_drv.c:2450]: unable to add 33:33:ff:0c:0d:66 into emac0: 17
 
Jan 01 00:00:00.542                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2663]: pfe0: Disabling promiscuous mode
 
Jan 01 00:00:00.542                 io_pkt_v6_hc.8                 slog      0  WRN[src/pfe_drv.c:2829]: EMAC speed change for SGMII is currently not supported.
 
Jan 01 00:00:00.542                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2443]: Adding 01:00:5e:00:00:01 to emac0
 
Jan 01 00:00:00.544                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2443]: Adding 33:33:00:00:00:01 to emac0
 
Jan 01 00:00:00.544                 io_pkt_v6_hc.8                 slog      0  WRN[src/pfe_drv.c:2450]: unable to add 33:33:00:00:00:01 into emac0: 17
 
Jan 01 00:00:00.544                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2443]: Adding 33:33:ff:0c:0d:66 to emac0
 
Jan 01 00:00:00.544                 io_pkt_v6_hc.8                 slog      0  WRN[src/pfe_drv.c:2450]: unable to add 33:33:ff:0c:0d:66 into emac0: 17
 
Jan 01 00:00:00.544                 io_pkt_v6_hc.8                 slog      0  INF[src/pfe_drv.c:2663]: pfe0: Disabling promiscuous mode
 
Jan 01 00:00:00.554               spi_master.24585               normal*     0  Starting spi-master resource manager
Jan 01 00:00:00.558               spi_master.24587               normal*     0  Starting spi-master resource manager
Jan 01 00:00:00.561               spi_master.24588               normal*     0  Starting spi-master resource manager
Jan 01 00:00:00.565               spi_master.24589               normal*     0  Starting spi-master resource manager
Jan 01 00:00:00.582          devb_sdmmc_mx8x.24595                 slog*  1800  devb-sdmmc-mx8x 1.00A (Jun 23 2026 09:45:48)
Jan 01 00:00:00.583          devb_sdmmc_mx8x.24595                 slog      0  libcam.so (Jun 22 2020 21:33:15) bver 7010003
Jan 01 00:00:00.594          devb_sdmmc_mx8x.24595                 slog   1800  sdio_cd:  insertion path 0, cd state 0x1
Jan 01 00:00:00.644          devb_sdmmc_mx8x.24595                 slog   1800  SD CID:
Jan 01 00:00:00.644          devb_sdmmc_mx8x.24595                 slog   1800    MID 0x27, OID 0x5048, PNM SD32G
Jan 01 00:00:00.644          devb_sdmmc_mx8x.24595                 slog   1800    PRV 0x62, PSN 0x6c62d132, MDT 4-2023
Jan 01 00:00:00.644          devb_sdmmc_mx8x.24595                 slog   1800  SD CSD:
Jan 01 00:00:00.644          devb_sdmmc_mx8x.24595                 slog   1800    CSD_STRUCTURE 1, SPEC_VERS 0, CCC 0x5b5
Jan 01 00:00:00.644          devb_sdmmc_mx8x.24595                 slog   1800    TAAC 14, NSAC 0, TRAN_SPEED 50
Jan 01 00:00:00.644          devb_sdmmc_mx8x.24595                 slog   1800    C_SIZE 59023, C_SIZE_MULT 0
Jan 01 00:00:00.644          devb_sdmmc_mx8x.24595                 slog   1800    READ_BL_LEN 9, WRITE_BL_LEN 9
Jan 01 00:00:00.644          devb_sdmmc_mx8x.24595                 slog   1800    ERASE GRP_SIZE 0, GRP_MULT 0, SIZE 127
Jan 01 00:00:00.644          devb_sdmmc_mx8x.24595                 slog   1800    blksz 512, sectors 60440576, dtr 25000000
Jan 01 00:00:00.644          devb_sdmmc_mx8x.24595                 slog   1800  SD SW CAPS:
Jan 01 00:00:00.644          devb_sdmmc_mx8x.24595                 slog   1800    bus mode 0x3, cmd sys 0x1
Jan 01 00:00:00.644          devb_sdmmc_mx8x.24595                 slog   1800    drv type 0x1, curr limit 0x1
Jan 01 00:00:00.644          devb_sdmmc_mx8x.24595                 slog   1800    dtr 50000000
Jan 01 00:00:00.644          devb_sdmmc_mx8x.24595                 slog   1800  CFG:  Timing HS, DTR 50000000, Bus Width 4 bit
 
Jan 01 00:00:00.645          devb_sdmmc_mx8x.24595                 slog    100  cam-disk.so (Jun 22 2020 21:33:17)
Jan 01 00:00:00.647          devb_sdmmc_mx8x.24595                 slog      0  scsi_interpret_sense (sdmmc ptl-0:0:0):  cam_status=c4, scsi_status=2, flag=00000040, vuflag=0008, cmd=1a, error=70, sense=5, asc=24, ascq=0
Jan 01 00:00:00.647          devb_sdmmc_mx8x.24595                 slog      0  scsi_interpret_sense (sdmmc ptl-0:0:0):  cam_status=c4, scsi_status=2, flag=00000040, vuflag=0008, cmd=5a, error=70, sense=5, asc=24, ascq=0
Jan 01 00:00:00.647          devb_sdmmc_mx8x.24595                 slog      0  scsi_interpret_sense (sdmmc ptl-0:0:0):  cam_status=c4, scsi_status=2, flag=00000040, vuflag=0008, cmd=5a, error=70, sense=5, asc=24, ascq=0
Jan 01 00:00:01.827          devb_sdmmc_mx8x.24595                 slog   1000  fs-qnx6: Allocation strategy 0
Jan 01 00:00:01.827          devb_sdmmc_mx8x.24595                 slog   1000  fs-qnx6: Use btree directory 0
Jan 01 00:00:01.828          devb_sdmmc_mx8x.24595                 slog   1000  fs-qnx6: fs-qnx6: trim (0,1048576,2) was not requested, and is NOT supported
Jan 01 00:00:01.833               io_usb_otg.36885                 slog*     0  main(453)[tid:1]: io-usb-otg (Jun 13 2020 20:10:17) args: -d hcd-ehci-mx28 ioport=0x44064100,irq=243,ulpi,no_stream,verbose=5 
Jan 01 00:00:01.835           devf_qspi_s32g.36884                 slog*     0  (devf  t1::f3s_qspi_ident:73) Page size: 256
Jan 01 00:00:01.835           devf_qspi_s32g.36884                 slog      0  (devf  t1::f3s_qspi_ident:74) Total chip size: 0x4000000, Unit size: 0x10000
Jan 01 00:00:01.839               io_usb_otg.36885                 slog      0  ehci_init: Initialiaing with sever version: 2 
Jan 01 00:00:01.839               io_usb_otg.36885                 slog      0  ehci_controller_init(4303): devu-hcd-ehci-mx28.so (Apr 19 2024 13:44:54):  args ulpi,no_stream,verbose=5
Jan 01 00:00:01.840               io_usb_otg.36885                 slog      8  usb_enum_port(94)[tid:1]: busno 0, parent -1, port 0, High speed
Jan 01 00:00:01.840               io_usb_otg.36885                 slog     11  usb_client_descriptor_get(198)[tid:1]: (type 1, index 0, length
Jan 01 00:00:01.840               io_usb_otg.36885                 slog     12  usb_device_set_address(245)[tid:1]: b:0 devno 0
Jan 01 00:00:01.840               io_usb_otg.36885                 slog     11  usb_client_descriptor_get(198)[tid:1]: (type 1, index 0, length 18)
Jan 01 00:00:01.841               io_usb_otg.36885                 slog     11  usb_client_descriptor_get(198)[tid:1]: (type 2, index 0, length 9)
Jan 01 00:00:01.841               io_usb_otg.36885                 slog     11  usb_client_descriptor_get(198)[tid:1]: (type 2, index 0, length 25)
Jan 01 00:00:01.841               io_usb_otg.36885                 slog      8  usb_enum_port(141)[tid:1]: vid 0x0000, did 0x0000 enumerated(busno 0, devno 0:0)
Jan 01 00:00:01.841               io_usb_otg.36885                 slog     11  hub_state_inserted(569)[tid:1]: bdentry 0, dentry 0 0
Jan 01 00:00:01.841               io_usb_otg.36885                 slog     13  hub_configuration_enable(263)[tid:1]: 1
Jan 01 00:00:01.943               io_usb_otg.36885                 slog      0  usbh_timeout_init(203)[tid:1]: Complete
Jan 01 00:00:01.954               io_usb_otg.36885                 slog      0  read_vid_pid: ULPI VID 0x0424 PID 0x0009
Jan 01 00:00:01.954               io_usb_otg.36885                 slog      0  s32g_phy_set_vbus: set_vbus off
Jan 01 00:00:01.968               io_usb_otg.36885                 slog      0  s32g_phy_set_vbus: set_vbus on
Jan 01 00:00:01.979               io_usb_otg.36885                 slog      0  ehci_get_port_status(3568 0x44064100): port=0, tpstatus 10100 e_pstatus 8c001000
Jan 01 00:00:01.979               io_usb_otg.36885                 slog      8  usb_enum_port_extract(172)[tid:7]: (busno 0, pdevno 0, portno 1)
Jan 01 00:00:01.979               io_usb_otg.36885                 slog      8  usb_enum_port_extract(192)[tid:7]: status (2)
Jan 01 00:00:01.983               devb_umass.36886                 slog*   900  devb-umass 1.00A (Jun 22 2020 21:33:41)
Jan 01 00:00:01.984               devb_umass.36886                 slog      0  libcam.so (Jun 22 2020 21:33:15) bver 7010003
Jan 01 00:00:01.985               io_usb_otg.36885                 slog      0  usbdi_client_connect(58)[tid:5]: pid 36886 proc=proc/boot/devb-umass usbdi_client 32eebb9a80
Jan 01 00:00:01.986               io_usb_otg.36885                 slog      0  usbdi_resmgr_connect(310)[tid:5]: usbdi_resmgr_connect: pid 36886 usbdi_client 32eebb9a80 
Jan 01 00:00:01.986               devb_umass.36886                 slog      0  usbdi debug path /pps/usb/debug/ doesn't exist
 
Process 49177 (slog2info) exited status=0.
# ifconfig
 
lo0: flags=8049<UP,LOOPBACK,RUNNING,MULTICAST> mtu 33136
inet 127.0.0.1 netmask 0xff000000
inet6 ::1 prefixlen 128
inet6 fe80::1%lo0 prefixlen 64 scopeid 0x1
pfe0: flags=8843<UP,BROADCAST,RUNNING,SIMPLEX,MULTICAST> mtu 1500
capabilities=1f<IP4CSUM,TCP4CSUM,UDP4CSUM,TCP6CSUM,UDP6CSUM>
enabled=0
address: 00:0a:0b:0c:0d:66
media: Ethernet none (1000baseT full-duplex)
status: active
inet 0.0.0.0 netmask 0xff000000 broadcast 255.255.255.255
inet6 fe80::20a:bff:fe0c:d66%pfe0 prefixlen 64 scopeid 0x11
pfe1: flags=8802<BROADCAST,SIMPLEX,MULTICAST> mtu 1500
capabilities=1f<IP4CSUM,TCP4CSUM,UDP4CSUM,TCP6CSUM,UDP6CSUM>
enabled=0
address: 00:1a:1b:1c:1d:66
media: Ethernet none (1000baseT full-duplex)
status: no carrier
pfe2: flags=8802<BROADCAST,SIMPLEX,MULTICAST> mtu 1500
capabilities=1f<IP4CSUM,TCP4CSUM,UDP4CSUM,TCP6CSUM,UDP6CSUM>
enabled=0
address: 00:2a:2b:2c:2d:66
media: Ethernet none (1000baseT full-duplex)
status: no carrier
 
Process 57369 (ifconfig) exited status=0.
# 
0 Kudos
Reply
54 Replies

1,482 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @Seneca 

Thanks for your reply.

Would you mind providing the full booting log including all u-boot env information for further checking?

 

BR

Chenyin 

0 Kudos
Reply

1,481 Views
Seneca
Contributor I

Note: io pkt is not started at the moment. Starting it will not remove the no carrier problem though.

 

U-Boot 2022.04 (Jul 01 2026 - 16:53:39 +0200)

SoC: NXP S32G399A rev. 1.1
CPU: ARM Cortex-A53 r0p4 @ max 1300 MHz
Model: NXP S32G399A-RDB3
DRAM: 3.5 GiB
Core: 306 devices, 25 uclasses, devicetree: board
MMC: FSL_SDHC: 0
Loading Environment from MMC... OK
In: serial@401c8000
Out: serial@401c8000
Err: serial@401c8000
Board revision: RDB3 Revision F
PCIe: BusDevFun VendorId DeviceId Device Class Sub-Class
__________________________________________________________________________
pcie@40400000 RootComplex
| `-- 01:00.00 0x1957 0x4300 Bridge device 0x04
Net: eth0: ethernet@4033c000
Found PFE version 0x0101 (S32G3)
, eth1: pfe0, eth2: pfe1, eth3: pfe2
Hit any key to stop autoboot: 2  1  0
=> printenv
atf_fdt_0to3=fdt addr 0x83e00000; fdt resize; fdt set /cpus/cpu@1 cpu-release-addr <0x0 0xa0000010>; fdt set /cpus/cpu@100 cpu-release-addr <0x0 0xa0000010>; fdt set /cpus/cpu@101 cpu-release-addr <0x0 0xa0000010>;
atf_fdt_4to7=fdt set /cpus/cpu@2 cpu-release-addr <0x0 0xa0000010>; fdt set /cpus/cpu@3 cpu-release-addr <0x0 0xa0000010>; fdt set /cpus/cpu@102 cpu-release-addr <0x0 0xa0000010>; fdt set /cpus/cpu@103 cpu-release-addr <0x0 0xa0000010>;
baudrate=115200
board_rev=F
boot_mtd=booti
boot_qnx_atf=mmc dev 0; fatload mmc 0:1 0x83e00000 s32g399a-rdb3.dtb; run atf_fdt_0to3; run atf_fdt_4to7; fatload mmc 0:1 0x80080000 ifs-s32g399a-rdb.ui; bootm 0x80080000 - 0x83E00000
bootargs=root=/dev/ram rw earlycon loglevel=7
bootcmd=run boot_qnx_atf
bootdelay=2
console=ttyLF0
cpu_trap=dcache off; mw.l 0xa0000000 0xd503205f; mw.l 0xa0000004 0x58000060; mw.l 0xa0000008 0xb4ffffc0; mw.l 0xa000000C 0xd61f0000; mw.q 0xa0000010 0x00000000; dcache on;
eth1addr=00:04:9f:be:ef:00
eth2addr=00:04:9f:be:ef:01
eth3addr=00:04:9f:be:ef:02
ethaddr=0e:46:58:92:0b:68
fdt_addr=0x83000000
fdt_enable_hs400es=fdt addr ${fdt_addr}; fdt rm /soc/mmc no-1-8-v; fdt resize;
fdt_file=s32g399a-rdb3.dtb
fdt_high=0xffffffffffffffff
fdt_override=;
fdtcontroladdr=ffa96000
flashboot=echo Booting from flash...; run flashbootargs;mtd read Kernel ${loadaddr};mtd read DTB ${fdt_addr};mtd read Rootfs ${ramdisk_addr};${boot_mtd} ${loadaddr} ${ramdisk_addr} ${fdt_addr};
flashbootargs=setenv bootargs console=${console},${baudrate} root=/dev/ram rw earlycon ;setenv flashsize 0x04000000;
hwconfig=serdes0:mode=pcie,clock=ext;pcie0:mode=rc;serdes1:mode=xpcs0&xpcs1,clock=ext,fmhz=125;xpcs1_0:speed=2G5;xpcs1_1:speed=1G
image=Image
initrd_high=0xffffffffffffffff
ipaddr=10.0.0.100
loadaddr=0x80000000
loadfdt=fatload mmc ${mmcdev}:${mmcpart} ${fdt_addr} ${fdt_file}; run fdt_override;
loadimage=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${image}
loadtftpfdt=tftp ${fdt_addr} ${fdt_file};
loadtftpimage=tftp ${loadaddr} ${image};
mmcargs=setenv bootargs console=${console},${baudrate} root=${mmcroot} earlycon
mmcboot=echo Booting from mmc ...; run mmcargs; if run loadfdt; then run fdt_fixups; ${boot_mtd} ${loadaddr} - ${fdt_addr}; else echo WARN: Cannot load the DT; fi;
mmcdev=0
mmcpart=1
mmcroot=/dev/mmcblk0p2 rootwait rw
netargs=setenv bootargs console=${console},${baudrate} root=/dev/nfs ip=dhcp nfsroot=${serverip}:${nfsroot},v3,tcp earlycon
netboot=echo Booting from net ...; run netargs; if test ${ip_dyn} = yes; then setenv get_cmd dhcp; else setenv get_cmd tftp; fi; ${get_cmd} ${image}; if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if ${get_cmd} ${fdt_addr} ${fdt_file}; then ${boot_mtd} ${loadaddr} - ${fdt_addr}; else if test ${boot_fdt} = try; then ${boot_mtd}; else echo WARN: Cannot load the DT; fi; fi; else ${boot_mtd}; fi;
netmask=255.255.255.0
nfsboot=echo Booting from net using tftp and nfs...; run nfsbootargs;run loadtftpimage; run loadtftpfdt;${boot_mtd} ${loadaddr} - ${fdt_addr};
nfsbootargs=setenv bootargs console=${console},${baudrate} root=/dev/nfs rw ip=${ipaddr}:${serverip}::${netmask}::eth0:off nfsroot=${serverip}:/tftpboot/rfs,nolock,v3,tcp earlycon
pfe1_phy_addr=8
pfeng_mode=enable,sgmii,sgmii,rgmii
ramdisk_addr=0x90000000
release_cpus=run cpu_trap; mp 1 release 0xa0000000; mp 2 release 0xa0000000; mp 3 release 0xa0000000; mp 4 release 0xa0000000; mp 5 release 0xa0000000; mp 6 release 0xa0000000; mp 7 release 0xa0000000;
script=boot.scr
serverip=10.0.0.1
skip_scmi_reset_agent=1
stderr=serial@401c8000
stdin=serial@401c8000
stdout=serial@401c8000

Environment size: 3581/8188 bytes
=> boot
switch to partitions #0, OK
mmc0 is current device
59970 bytes read in 7 ms (8.2 MiB/s)
9362112 bytes read in 394 ms (22.7 MiB/s)
## Booting kernel from Legacy Image at 80080000 ...
Image Name:
Image Type: AArch64 Linux Kernel Image (uncompressed)
Data Size: 9362048 Bytes = 8.9 MiB
Load Address: 80080000
Entry Point: 80080000
Verifying Checksum ... OK
## Flattened Device Tree blob at 83e00000
Booting using the fdt blob at 0x83e00000
Loading Kernel Image
Using Device Tree in place at 0000000083e00000, end 0000000083e11fff
fixup: pfe1: update phy addr to 0x8

Starting kernel ...

board_cleanup_before_linux: QNX PFE code.
ethernet@4033c000 Waiting for PHY auto negotiation to complete......... TIMEOUT !
phy_startup() failed: -110FAILED: -110
Found PFE version 0x0101 (S32G3)

Found PFE version 0x0101 (S32G3)
pfe2 Waiting for PHY auto negotiation to complete......... TIMEOUT !
pfeng_netif pfe1: Failed to establish XPCS link on PFE1
## Setting pfe_ts clock ...
## Setting ftm0_sys clock ...
## Setting ftm0_ext clock ...
## Setting ftm1_sys clock ...
## Setting ftm1_ext clock ...
Reserving RAM region for PFE driver on EVB/RDB
ClockCycles samples:
0 166386615
1 166386614
2 166386615
3 166386615
4 166386615
5 166386615
6 166386616
7 166386615
All ClockCycles offsets within tolerance
Welcome to QNX Neutrino 7.1.0 on the NXP S32G399A RDB Board!!
Starting watchdog...
Starting serial driver ...
Starting Networking driver (/dev/socket)...
Utarting SPI driver (/dev/spi0,1,2,3,4,5)...
Starting I2C 0/1/2/3/4 driver (/dev/i2c0,1,2,3,4)...
Starting USDHC0 memory card driver...
[00] Starting QSPI Flash driver...
SIM="SDMMC" HBA="imx"
[00,0,0] type=00 ver=05 resp=00 SDMMC:
Starting USB host driver (/dev/usb/*)
Detected QSPI Flash: Macronix MX25UW512, JEDEC 0xC2 - 0x813A, Size: 0x4000000
Launching devb-umass for /dev/usb/* ...
U# slogi 2info

Jan 01 00:00:00.022 random.4 low* 0 qcrypto: loading configuration file '/etc/qcrypto.conf' [qcrypto_common.c(190)]
Jan 01 00:00:00.023 random.4..0 slog* 700 Random is using the Fortuna PRNG
Jan 01 00:00:00.031 random.4 low 0 qcrypto: 'openssl' plugin loaded [qcrypto_plugins.c(354)]
Jan 01 00:00:00.031 random.4..0 slog 700 Selecting timer as an entropy source
Jan 01 00:00:00.031 random.4..0 slog 700 Registered path names
Jan 01 00:00:00.031 random.4..0 slog 700 random: starting resmgr
Jan 01 00:00:00.031 random.4..0 slog 700 random: Daemonizing the process
Jan 01 00:00:00.041 devc_serlinflexd.7 slog* 0 serlinflexd_interrupt_attach: Attaching to interrupt 114
Jan 01 00:00:10.146 spi_master.8 normal* 0 Starting spi-master resource manager
Jan 01 00:00:10.149 spi_master.9 normal* 0 Starting spi-master resource manager
Jan 01 00:00:10.152 spi_master.10 normal* 0 Starting spi-master resource manager
Jan 01 00:00:10.155 spi_master.11 normal* 0 Starting spi-master resource manager
Jan 01 00:00:10.158 spi_master.12 normal* 0 Starting spi-master resource manager
Jan 01 00:00:10.161 spi_master.13 normal* 0 Starting spi-master resource manager
Jan 01 00:00:10.177 devb_sdmmc_mx8x.19 slog* 1800 devb-sdmmc-mx8x 1.00A (Jul 1 2026 14:10:37)
Jan 01 00:00:10.178 devb_sdmmc_mx8x.19 slog 0 libcam.so (Jun 22 2020 21:33:15) bver 7010003
Jan 01 00:00:10.189 devb_sdmmc_mx8x.19 slog 1800 sdio_cd: insertion path 0, cd state 0x1
Jan 01 00:00:10.239 devb_sdmmc_mx8x.19 slog 1800 SD CID:
Jan 01 00:00:10.239 devb_sdmmc_mx8x.19 slog 1800 MID 0x27, OID 0x5048, PNM SD32G
Jan 01 00:00:10.239 devb_sdmmc_mx8x.19 slog 1800 PRV 0x62, PSN 0x6c62d196, MDT 4-2023
Jan 01 00:00:10.239 devb_sdmmc_mx8x.19 slog 1800 SD CSD:
Jan 01 00:00:10.239 devb_sdmmc_mx8x.19 slog 1800 CSD_STRUCTURE 1, SPEC_VERS 0, CCC 0x5b5
Jan 01 00:00:10.239 devb_sdmmc_mx8x.19 slog 1800 TAAC 14, NSAC 0, TRAN_SPEED 50
Jan 01 00:00:10.239 devb_sdmmc_mx8x.19 slog 1800 C_SIZE 59023, C_SIZE_MULT 0
Jan 01 00:00:10.239 devb_sdmmc_mx8x.19 slog 1800 READ_BL_LEN 9, WRITE_BL_LEN 9
Jan 01 00:00:10.239 devb_sdmmc_mx8x.19 slog 1800 ERASE GRP_SIZE 0, GRP_MULT 0, SIZE 127
Jan 01 00:00:10.239 devb_sdmmc_mx8x.19 slog 1800 blksz 512, sectors 60440576, dtr 25000000
Jan 01 00:00:10.239 devb_sdmmc_mx8x.19 slog 1800 SD SW CAPS:
Jan 01 00:00:10.239 devb_sdmmc_mx8x.19 slog 1800 bus mode 0x3, cmd sys 0x1
Jan 01 00:00:10.239 devb_sdmmc_mx8x.19 slog 1800 drv type 0x1, curr limit 0x1
Jan 01 00:00:10.239 devb_sdmmc_mx8x.19 slog 1800 dtr 50000000
Jan 01 00:00:10.239 devb_sdmmc_mx8x.19 slog 1800 CFG: Timing HS, DTR 50000000, Bus Width 4 bit

Jan 01 00:00:10.240 devb_sdmmc_mx8x.19 slog 100 cam-disk.so (Jun 22 2020 21:33:17)
Jan 01 00:00:10.242 devb_sdmmc_mx8x.19 slog 0 scsi_interpret_sense (sdmmc ptl-0:0:0): cam_status=c4, scsi_status=2, flag=00000040, vuflag=0008, cmd=1a, error=70, sense=5, asc=24, ascq=0
Jan 01 00:00:10.242 devb_sdmmc_mx8x.19 slog 0 scsi_interpret_sense (sdmmc ptl-0:0:0): cam_status=c4, scsi_status=2, flag=00000040, vuflag=0008, cmd=5a, error=70, sense=5, asc=24, ascq=0
Jan 01 00:00:10.242 devb_sdmmc_mx8x.19 slog 0 scsi_interpret_sense (sdmmc ptl-0:0:0): cam_status=c4, scsi_status=2, flag=00000040, vuflag=0008, cmd=5a, error=70, sense=5, asc=24, ascq=0
Jan 01 00:00:10.248 io_usb_otg.21 slog* 0 main(453)[tid:1]: io-usb-otg (Jun 13 2020 20:10:17) args: -d hcd-ehci-mx28 ioport=0x44064100,irq=243,ulpi,no_stream,verbose=5
Jan 01 00:00:10.250 devf_qspi_s32g.20 slog* 0 (devf t1::f3s_qspi_ident:73) Page size: 256
Jan 01 00:00:10.250 devf_qspi_s32g.20 slog 0 (devf t1::f3s_qspi_ident:74) Total chip size: 0x4000000, Unit size: 0x10000
Jan 01 00:00:10.254 io_usb_otg.21 slog 0 ehci_init: Initialiaing with sever version: 2
Jan 01 00:00:10.254 io_usb_otg.21 slog 0 ehci_controller_init(4292): devu-hcd-ehci-mx28.so (Aug 15 2023 16:44:48): args ulpi,no_stream,verbose=5
Jan 01 00:00:10.254 io_usb_otg.21 slog 8 usb_enum_port(94)[tid:1]: busno 0, parent -1, port 0, High speed
Jan 01 00:00:10.255 io_usb_otg.21 slog 11 usb_client_descriptor_get(198)[tid:1]: (type 1, index 0, length
Jan 01 00:00:10.255 io_usb_otg.21 slog 12 usb_device_set_address(245)[tid:1]: b:0 devno 0
Jan 01 00:00:10.255 io_usb_otg.21 slog 11 usb_client_descriptor_get(198)[tid:1]: (type 1, index 0, length 18)
Jan 01 00:00:10.255 io_usb_otg.21 slog 11 usb_client_descriptor_get(198)[tid:1]: (type 2, index 0, length 9)
Jan 01 00:00:10.255 io_usb_otg.21 slog 11 usb_client_descriptor_get(198)[tid:1]: (type 2, index 0, length 25)
Jan 01 00:00:10.256 io_usb_otg.21 slog 8 usb_enum_port(141)[tid:1]: vid 0x0000, did 0x0000 enumerated(busno 0, devno 0:0)
Jan 01 00:00:10.256 io_usb_otg.21 slog 11 hub_state_inserted(569)[tid:1]: bdentry 0, dentry 0 0
Jan 01 00:00:10.256 io_usb_otg.21 slog 13 hub_configuration_enable(263)[tid:1]: 1
Jan 01 00:00:10.358 io_usb_otg.21 slog 0 usbh_timeout_init(203)[tid:1]: Complete
Jan 01 00:00:10.369 io_usb_otg.21 slog 0 read_vid_pid: ULPI VID 0x0424 PID 0x0009
Jan 01 00:00:10.369 io_usb_otg.21 slog 0 s32g_phy_set_vbus: set_vbus off
Jan 01 00:00:10.383 io_usb_otg.21 slog 0 s32g_phy_set_vbus: set_vbus on
Jan 01 00:00:10.394 io_usb_otg.21 slog 0 ehci_get_port_status(3557 0x44064100): port=0, tpstatus 10100 e_pstatus 8c001000
Jan 01 00:00:10.394 io_usb_otg.21 slog 8 usb_enum_port_extract(172)[tid:7]: (busno 0, pdevno 0, portno 1)
Jan 01 00:00:10.394 io_usb_otg.21 slog 8 usb_enum_port_extract(192)[tid:7]: status (2)
Jan 01 00:00:10.398 devb_umass.22 slog* 900 devb-umass 1.00A (Jun 22 2020 21:33:41)
Jan 01 00:00:10.399 devb_umass.22 slog 0 libcam.so (Jun 22 2020 21:33:15) bver 7010003
Jan 01 00:00:10.400 io_usb_otg.21 slog 0 usbdi_client_connect(58)[tid:5]: pid 22 proc=proc/boot/devb-umass usbdi_client 51ba29fa80
Jan 01 00:00:10.400 io_usb_otg.21 slog 0 usbdi_resmgr_connect(310)[tid:5]: usbdi_resmgr_connect: pid 22 usbdi_client 51ba29fa80
Jan 01 00:00:10.400 devb_umass.22 slog 0 usbdi debug path /pps/usb/debug/ doesn't exist
Jan 01 00:00:14.507 qconn.24 slog* 0 Couldn't initialize listen service: tcp (Address family not supported by protocol family)

0 Kudos
Reply

1,477 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @Seneca 

Thanks for sharing the log.

There seems serdes issues existed during the booting phase, may I know if you had done the following modification? (to comment out the init_serdes() function)

chenyin_h_0-1782977121730.png

 

BR

Chenyin

0 Kudos
Reply

1,465 Views
Seneca
Contributor I

Note: I not both pfe0 and pfe2 work at the same time. And when I ping them from an external machine it assigns pfe0 a funny mac address:

arp -a | grep 192
? (192.168.0.200) at 22:33:44:55:66:77 [ether] on enx00e04c680383
? (192.168.0.202) at <incomplete> on enx00e04c680383

 

This is from qnx slog2info:

Jan 01 00:00:58.251 iopkt.4121 main_buffer 0 duplicate IP address 192.168.0.200 sent from link address 22:33:44:55:66:77

0 Kudos
Reply

1,465 Views
Seneca
Contributor I

Ok some more news:

When I start the network client manually

io-pkt-v6-hc -p tcpip pkt_typed_mem=pfe_ddr -d /proc/boot/devnp-pfe-2.so pfe0_mac=000a0b0c0d66,pfe1_mac=001a1b1c1d66,pfe2_mac=002a2b2c2d66,class_fw=/proc/boot/s32g_pfe_class.fw,util_fw=/proc/boot/s32g_pfe_util.fw

and set a static ip for pfe0

ifconfig pfe0 192.168.0.200 netmask 255.255.255.0

ifconfig pfe0 down

ifconfig pfe0 up

I actually get a ping to an external address.

Nevertheless, in ifconfig pfe0 still shows ethernet none. It seems to me there are problems negotiating interface speed

 

# slog2info | grep pfe0

Jan 01 00:00:25.515 iopkt.4121 main_buffer 0 /proc/boot/devnp-pfe-2.so pfe0_mac=000a0b0c0d66,pfe1_mac=001a1b1c1d66,pfe2_mac=002a2b2c2d66,class_fw=/proc/boot/s32g_pfe_class.fw,util_fw=/proc/boot/s32g_pfe_util.fw
Jan 01 00:00:25.517 io_pkt_v6_hc.4121 slog 0 INF[src/pfe_drv.c:1460]: MII mode configuration for pfe0/EMAC0 not found. Using SGMII.
Jan 01 00:00:25.647 iopkt.4121 main_buffer 0 pfe0

Process 98332 (slog2info) exited status=0.
Jan 01 00:00:25.647 io_pkt_v6_hc.4121 slog 0 INF[src/pfe_drv.c:2124]: pfe0: Using static PHY mode, RESET=0
Jan 01 00:00:25.647 io_pkt_v6_hc.4121 slog 0 INF[src/pfe_drv.c:2286]: Speed/duplex configuration for pfe0 not found. Using 1 Gbps/full-duplex.
Jan 01 00:00:58.251 io_pkt_v6_hc.4121 slog 0 INF[src/pfe_drv.c:2606]: pfe0: Disabling promiscuous mode
Jan 01 00:00:58.251 io_pkt_v6_hc.4121 slog 0 INF[src/pfe_drv.c:2606]: pfe0: Disabling promiscuous mode
Jan 01 00:00:58.251 io_pkt_v6_hc.4121 slog 0 INF[src/pfe_drv.c:2606]: pfe0: Disabling promiscuous mode
Jan 01 00:00:58.251 io_pkt_v6_hc.4121 slog 0 INF[src/pfe_drv.c:2606]: pfe0: Disabling promiscuous mode
Jan 01 00:01:05.966 io_pkt_v6_hc.4121 slog 0 INF[src/pfe_drv.c:2606]: pfe0: Disabling promiscuous mode

 

For Pfe2 it might already fail in uboot in the board_cleanup_before_linux

pfe2 Waiting for PHY auto negotiation to complete......... TIMEOUT !

Edit: I can also obtain a ping from pfe2 but it also seems to have problems negotiating the correct speed. I wonder if the above timeout is correct.

0 Kudos
Reply

1,461 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @Seneca 

Thanks for your updates.

Glad that the PFE would ping correctly with the external machine.

There are limitation for the PFE driver in QNX:

chenyin_h_0-1783044213433.png

So that it is suggested using the fixed link, while speed changes triggered by AN are not supported.

 

BR

Chenyin

0 Kudos
Reply

1,456 Views
Seneca
Contributor I

Ok then hopefully these questions will bring me close to the finish line:

- How should I set the MAC addresses of pfe0 and pfe2? I understand an attempt is made to set it via io pkt

io-pkt-v6-hc -p tcpip pkt_typed_mem=pfe_ddr -d /proc/boot/devnp-pfe-2.so pfe0_mac=000a0b0c0d66,pfe1_mac=001a1b1c1d66,pfe2_mac=002a2b2c2d66,class_fw=/proc/boot/s32g_pfe_class.fw,util_fw=/proc/boot/s32g_pfe_util.fw

But when I ping pfe0 from an external machine that machines arp table presents a bogus address

? (192.168.0.200) at 22:33:44:55:66:77 [ether] on enx00e04c680383

On the external machine, tcpdump reveals there doesn't seem to be an arp response from pfe0 which has 192.168.0.200:

08:53:11.208021 IP6 user-Precision-7510 > ff02::16: HBH ICMP6, multicast listener report v2, 2 group record(s), length 48
08:53:11.394038 IP6 user-Precision-7510 > ff02::16: HBH ICMP6, multicast listener report v2, 2 group record(s), length 48
08:53:25.750284 ARP, Request who-has 192.168.0.200 tell 192.168.0.200, length 46
08:53:26.641915 IP6 :: > ff02::1:ff0c:d66: HBH ICMP6, multicast listener reportmax resp delay: 0 addr: ff02::1:ff0c:d66, length 24
08:53:26.692011 IP6 :: > ff02::1:ff0c:d66: ICMP6, neighbor solicitation, who has fe80::20a:bff:fe0c:d66, length 24
08:53:32.742005 IP6 fe80::20a:bff:fe0c:d66 > ff02::1:ff0c:d66: HBH ICMP6, multicast listener reportmax resp delay: 0 addr: ff02::1:ff0c:d66, length 24

When I cast another ping from the external machine I finally get a response:

08:59:22.118282 ARP, Request who-has 192.168.0.200 tell user-Precision-7510, length 28
08:59:22.118553 ARP, Reply 192.168.0.200 is-at 22:33:44:55:66:77 (oui Unknown), length 46
08:59:22.118569 IP user-Precision-7510 > 192.168.0.200: ICMP echo request, id 1, seq 1, length 64
08:59:22.118554 ARP, Reply 192.168.0.200 is-at 00:0a:0b:0c:0d:66 (oui Unknown), length 46

00:0a:0b:0c:0d:66 is what should be the correct mac address.

Nevertheless the arp table of the external machine still shows the bogus address

arp -a

? (192.168.0.200) at 22:33:44:55:66:77 [ether] on enx00e04c680383

 

My first guess would be to set them manually in uboot but I see no section in the integration manual that recommends that.

 

- What are the commands to use "fixed link"?

 

Regards

0 Kudos
Reply

1,453 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @Seneca 

Thanks for your reply.

1. For setting the MAC address, you may try using the  "io-pkt-v6-hc -p tcpip -d <driver> \ pfe1_mac=000a0b0c0d0e,pfe2_mac=001a1b1c1d1e" for example.

2. Since you are using RDB3, while with default settings you tried, the PFE0 connected to the sja1110 switch, usually the 192.168.0.200 is set internally within the SJA1110 SDK, so I suggest not using this IP for testing with PFE0, you may try setting other IP address like 192.168.1.X for PFE0

3. In u-boot, you may try setting the mac address with the "setenv ethaddr/eth1addr/eth2addr xxxx" for each MAC.

 

BR

Chenyin

0 Kudos
Reply

1,450 Views
Seneca
Contributor I

Ok, just for understanding this right:

There is another component that just happens to use 192.168.0.200?

And if I use 192.168.1.200 for pfe0 I will be fine?

Regards

0 Kudos
Reply

1,446 Views
Seneca
Contributor I

I see.

The ethaddr, eth1addr, eth2addr, eth3addr are set in my uboot but they are not enough to prevent the funny MAC for pfe0.

Are there other parameters?

0 Kudos
Reply

1,448 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @Seneca 

Thanks for the reply.

1. Yes, it is usually by default used by the switch connected.

2. I think the new IP addr you mentioned is fine for the test.

 

BR

Chenyin

0 Kudos
Reply

1,391 Views
Seneca
Contributor I

Greetings chenyin,

I intend to create a bridge interface using the ethernet ports gmac0, pfe0, pfe2.

https://www.qnx.com/developers/docs/7.0.0/index.html#com.qnx.doc.neutrino.utilities/topic/b/brconfig...

The connected clients are intended to be in the subnet 192.168.0.X netmask 255.255.255.0 

Will this conflict with 192.168.0.200 or anything else?

Regards

0 Kudos
Reply

1,381 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @Seneca 

Thanks for your reply.

From my understanding, there would not be confliction while not using 192.168.0.200.

However, if possible, you may use other subnet instead to avoid possible issues.

 

BR

Chenyin

0 Kudos
Reply

1,377 Views
Seneca
Contributor I

Would you mind making sure internally? Is there anything 192.168.0.200 does that requires it to have sole control of the subnet?

0 Kudos
Reply

1,373 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @Seneca 

Thanks for your reply.

If you do want to use the 192.168,.0.x subnet, when not assigning 192.168.0.200 to both PFE0 and the external devices that are connected to the switch, It would be correct for the network connection when you try pinging from outside to PFE0 or vice versa.

 

BR

Chenyin

 

0 Kudos
Reply

1,299 Views
Seneca
Contributor I

Greetings chenyin,

a new problem has arisen:

The arp handshake fails when I connect a TC387 / FreeRTOS target to pfe_mac2. It works with a regular Linux machine.

Any ideas?

0 Kudos
Reply

1,287 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @Seneca 

Thanks for your reply.

Since the same setup works with a Linux machine, the problem is more likely to be on the TC387 side (Ethernet driver, TCP/IP stack configuration, or related implementation) rather than on the MAC side. Further packet-level analysis would be needed to confirm the exact cause

 

BR

Chenyin

0 Kudos
Reply

1,285 Views
Seneca
Contributor I

Greetings,

the problem only occurs with the pfe2 port. Connecting the TC387 to pfe0 or gmac0 will not give that problem. 

0 Kudos
Reply

1,283 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @Seneca 

Thanks for your reply.

Since the PFE2 could work correctly with a Linux machine, there may not much issue existed on the S32G side, in order for solving your issue, you may try checking the link status, every frames sent between the two sides and then analyze on them, sorry that I do not know much about the software stack on your Infineon board.

 

BR

Chenyin

0 Kudos
Reply

1,179 Views
Seneca
Contributor I

Greetings chenyin,

could you please tell me again which ports on the target was exactly pfe0 and pfe2 on s32g399Ardb3?

I assumed pfe0 is the left one of the three stacked ports and pfe2 top-center, is this correct?

Are there any known problems mixing pfe and gmac?

Regards

0 Kudos
Reply

1,145 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @Seneca 

Thanks for your reply. I suggest referencing the following picture.

chenyin_h_0-1784081687384.png

PFE0 is connected with the SJA1110, cables connected to P1/2/3 could be linked with PFE0

GMAC could be used with PFE together.

 

BR

Chenyin

0 Kudos
Reply