S32G3 network interface

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32G3 network interface

Jump to solution
2,864 Views
JasonTseng
Contributor I

S32G3 block diagram shows 

Networking: 

4x FlexCAN
3x LINFlexD

1x 2-channel FlexRay

1x GMAC                   <--- this one
1x USBOTG
2x SerDes with PCIe 3.0 and 2 lanes each

 

Ethernet networks:

PFE, IEEE 1588v2 + AVB and three 2.5 Gbit MAC 

 

So my question is what is the difference and/or relationship between 

GMAC and 2.5Gbit Mac?

 

Thanks

 

 

0 Kudos
Reply
1 Solution
2,837 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @JasonTseng

Thanks for the questions.

There are two kinds of ethernet interface on S32G3, one is called GMAC, the other one is called PFE, the 2.5G there means that the PFE could support on three ports at 2.5G network.

 

Best Regards

Chenyin

View solution in original post

0 Kudos
Reply
4 Replies
2,829 Views
chenyin_h
NXP Employee
NXP Employee

Thanks for using NXP products, it is my pleasure to help.

 

Best Regards

Chenyin

0 Kudos
Reply
2,830 Views
JasonTseng
Contributor I

OK, understood, thank you.

0 Kudos
Reply
2,838 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @JasonTseng

Thanks for the questions.

There are two kinds of ethernet interface on S32G3, one is called GMAC, the other one is called PFE, the 2.5G there means that the PFE could support on three ports at 2.5G network.

 

Best Regards

Chenyin

0 Kudos
Reply
2,841 Views
JasonTseng
Contributor I

ps: I am referring PBS32G3V2.pdf p. 2 block diagram 

0 Kudos
Reply