S32G3 memory support list

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32G3 memory support list

Jump to solution
3,582 Views
Chenxu1
Contributor II

Hi, NXP colleagues
I see DDR ,NOR Flash and EMMC are supported by S32G3 in datasheet, but can you provide a list of DDR and other memories that have been tested for compatibility?

If any LPDDR4 protocol compliant DRAM in the market can be interfaced with  S32G3 with max density of 4GB ,have you not done fitness testing?

Expecting a reply.

Thank you .

0 Kudos
Reply
1 Solution
3,563 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @Chenxu1 

Thanks for the questions.

Sorry that seems there is not such list, NXP recommends any LPDDR4 DRAM of 4GB max density which is complaint with LPDDR4 protocol and follow JEDEC specs.

 

Best Regards

Chenyin

 

View solution in original post

5 Replies
3,444 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @Chenxu1 

Thanks for your kindly suggestions.

 

BR

Chenyin

0 Kudos
Reply
3,493 Views
chenyin_h
NXP Employee
NXP Employee

Hi, @Chenxu1 

Thanks for the reply.

Yes, from the information I could understand, there are not such lists for EMMC/Nors.

I apologize for the inconvenience.

 

BR

Chenyin

 

0 Kudos
Reply
3,456 Views
Chenxu1
Contributor II

Hi , 

Please make suggestions to your internal company, because the memory fitting test  of DDR and EMMC is very important to us.

Thanks.

0 Kudos
Reply
3,564 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @Chenxu1 

Thanks for the questions.

Sorry that seems there is not such list, NXP recommends any LPDDR4 DRAM of 4GB max density which is complaint with LPDDR4 protocol and follow JEDEC specs.

 

Best Regards

Chenyin

 

3,525 Views
Chenxu1
Contributor II

----This is not very conventional, although the LPDDR4 protocol is standard, but each DDR manufacturer also does some differences, which is the reason why many SOCs provide list, in theory, but not suitable for direct use.
----Is this true of other EMMCs and NOR?

0 Kudos
Reply