S32G2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32G2

1,124件の閲覧回数
Damodara_S
Contributor I

Hi @chenyin_h,

Does S32G274A supports IEEE 802.1 AS standard?

Can all SPI interfaces works in both Master and slave modes?

is there any limit on supported DDR memory size?

Regards,

Damodara.s

0 件の賞賛
返信
1 返信

1,107件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Thanks for the questions.

  1. Yes, it could support 802.1-AS
  2. Yes, all 6 SPIs could support both Master/Slave mode
  3. The device could support with max density of 4GB DDR.

Hope it helps

 

Best Regards

Chenyin

0 件の賞賛
返信