S32G3: debugging Linux with s32 debug probe

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32G3: debugging Linux with s32 debug probe

2,762 Views
s153022
Contributor III

Dear NXP Support Team,

We have recently purchased the S32G-VNP-RDB3 Board and have successfully compiled the NXP Auto Yocto Linux BSP v38.0. We can run Linux and boot to the Linux prompt without issues. Additionally, we have purchased the S32 Debug Probe.

Our current objective is to debug the Linux kernel, ATF (Arm Trusted Firmware), and U-Boot using the debugger. We seek guidance on how to connect the debugger to these components, set breakpoints within the kernel, ATF, and U-Boot code, and navigate through the debugging process.

Could you kindly direct us to a comprehensive guide or provide instructions that cover the connection of the debugger, setting of breakpoints, and stepping through the debugger?

Thank you for your assistance.

Best regards,

0 Kudos
Reply
2 Replies

1,447 Views
rizwan_at_disruptdotcom
Contributor III

@chenyin_h  I do not find any information regarding "attaching to a running target" in any of the available documentation for S32 debug probe, or any instructions on debugging a running linux image. Can you please check internally and provide a debug example for this use case.
Also on the S32 DS, the debug configuration has no option for setting "attach only". The debugger always gives a reset to the hardware and even if the target is stopped at u-boot for DDR initialization, the debugger would give it  reset and then timeout on the connection.

0 Kudos
Reply

2,744 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @contributor3

Thanks for the question.

For using the debugger, the corresponding official documents could be downloaded from the following link: (including the user guide, quick start guide and fact sheet), which could be the basics for using the debugger.

https://www.nxp.com/design/design-center/software/automotive-software-and-tools/s32-debug-probe:S32-...

 

Besides, there are also some other useful posts from the community, which could help for the details.

https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-JTAG-Flash-Programming-with-S32-...

https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Start-S32-Debugger-from-S32-Desi...

Hope it helps.

 

Best Regards

Chenyin

 

0 Kudos
Reply