Hi,
I’m using Design Studio 3.5 to build the RGB_LED_M7 project and have followed the software enablement guide to update the linker script. I used the IVT tools to generate a blob image, and the SD card image worked well. However, when I tried generating the QSPI image, it didn’t work—the LEDs didn’t blink at all.
I made sure to change the interface selection to QSPI and selected the MX25UM51245G in S32Flashtool. I’ve attached both screenshots for reference.
Since I was able to use S32Flashtool to flash fip.s32-qspi successfully, and the board booted, I suspect there might be an issue with the IVT configuration of the LED project. Could you help me troubleshoot this?
Thanks in advance for your support.
XD
XD_0-1726779679883.png
XD_1-1726779787833.png