S32G3-NAD or Modem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32G3-NAD or Modem

1,033件の閲覧回数
MohamedAbdelslam
Contributor III

Hi,
Does The NXP S32G399A-RDB3 development board include a built-in cellular modem or Network Access Device (NAD)?
If not, does it provide expansion options to add one?

タグ(1)
0 件の賞賛
返信
1 返信

1,014件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @MohamedAbdelslam

Thanks for the post.

The RDB3 provides the following network connectors, but not including built-in modems.

chenyin_h_0-1747823221373.png

There are M.2, PCIe, USB, etc. exist on the RDB3, from my experience, devices like WIFI module, LTE/5G module could be connected to the board.

 

BR

Chenyin

 

0 件の賞賛
返信