S32G3-NAD or Modem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32G3-NAD or Modem

1,044 Views
MohamedAbdelslam
Contributor III

Hi,
Does The NXP S32G399A-RDB3 development board include a built-in cellular modem or Network Access Device (NAD)?
If not, does it provide expansion options to add one?

Tags (1)
0 Kudos
Reply
1 Reply

1,025 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @MohamedAbdelslam

Thanks for the post.

The RDB3 provides the following network connectors, but not including built-in modems.

chenyin_h_0-1747823221373.png

There are M.2, PCIe, USB, etc. exist on the RDB3, from my experience, devices like WIFI module, LTE/5G module could be connected to the board.

 

BR

Chenyin

 

0 Kudos
Reply