S32G3 – How to flash application with S32 Flash Tool without erasing BSP Linux

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32G3 – How to flash application with S32 Flash Tool without erasing BSP Linux

Jump to solution
1,306 Views
MrAlexIV
Contributor III

Hi,

I am trying to flash a .bin file generated with S32 Design Studio onto my board.

On the SD card I’ve already flashed the Linux BSP, and I’d like to keep it, since I want to use it to visualize the logs of my program (e.g., through UART or a console).

However, when I use the Flash Tool and choose Destination = Flash, it seems to overwrite the entire SD, including the BSP.

My question is:

What is the correct way to flash my .bin application without erasing the existing BSP on the SD card?

Is there a specific option or memory region I should select, or should I flash the application to a different location (e.g., RAM or external QSPI/NOR) to preserve Linux?

Thanks in advance!

0 Kudos
Reply
1 Solution
1,276 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @MrAlexIV 

Thanks for your reply.

Not sure how you starting the M core application via Linux.

A possible way is firstly flashed the full BSP to the SD card, then boot the board directly; Secondly, stopped in u-boot, and then use network connection to transfer your M core image to the DDR(or flash the M core application to the QSPI/eMMC in advance before boot, and in uboot, load it from QSPI to the DDR); After it, use the uboot to run the M7 application, next, to boot with your Linux. 

 

BR

Chenyin

View solution in original post

0 Kudos
Reply
11 Replies
1,218 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @MrAlexIV 

Thanks for your reply.

Gmac is the eth0 in the uboot, commonly it could be directly used by default? if you have issues, would you mind providing us your setup?and the logs during your operation?

Which BSP you are working with? which kind of S32G board?

 

BR

Chenyin 

0 Kudos
Reply
1,101 Views
MrAlexIV
Contributor III

When I try to up the eth0, i receive this:

root@s32g399aevb3:~# ifconfig
lo: flags=73<UP,LOOPBACK,RUNNING> mtu 65536
inet 127.0.0.1 netmask 255.0.0.0
inet6 ::1 prefixlen 128 scopeid 0x10<host>
loop txqueuelen 1000 (Local Loopback)
RX packets 82 bytes 6220 (6.0 KiB)
RX errors 0 dropped 0 overruns 0 frame 0
TX packets 82 bytes 6220 (6.0 KiB)
TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0

pfe2: flags=4163<UP,BROADCAST,RUNNING,MULTICAST> mtu 1500
inet 192.168.128.249 netmask 255.255.255.0 broadcast 192.168.128.255
inet6 fe80::201:beff:febe:ef33 prefixlen 64 scopeid 0x20<link>
ether 00:01:be:be:ef:33 txqueuelen 1000 (Ethernet)
RX packets 0 bytes 0 (0.0 B)
RX errors 0 dropped 0 overruns 0 frame 0
TX packets 17 bytes 1386 (1.3 KiB)
TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0
device memory 0x46000000-46ffffff

root@s32g399aevb3:~# sudo ifconfig eth0 up
SIOCSIFFLAGS: No such device


root@s32g399aevb3:~# sudo ip link set eth0 up
RTNETLINK answers: No such device

0 Kudos
Reply
1,087 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @MrAlexIV 

Thanks for your reply.

I understand that the previous issue is transfer failure when transferring your image from PC to the board via tftp under u-boot. As a result, I suggest using the gmac0 to transfer the image instead.

But from the log you shared, it is in the Linux, I am not sure about your current status.

In order for better providing you accurate and direct support, would you mind firstly clarifying the following?

1. The BSP version you used is?

2. From the log, seems the S32G3EVB3 is used, right? if possible, would you mind share me a pic of your board used?

3. May I know if you still focus on the issue raised last Thursday, for dealing with the transfer issue for your M7 binary under uboot?

 

BR

Chenyin

0 Kudos
Reply
1,084 Views
MrAlexIV
Contributor III

Hi, ok here the following answers:


1) 38.0

2) Yes exactly, it is that board (can't access to a pic rn)

3) I am actually still focusing on it. However, I found a way to run the .elf on my SD, but It is for the A53 cores and not M7, and the example (like the FlexCAN one) are for M7

0 Kudos
Reply
1,080 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @MrAlexIV 

Thanks for your confirmation.

On EVB3, you may try the following:

1. Plug the network cable to the the following interface:

 

chenyin_h_3-1753181523444.png

2. Once booted, before transfer the image, set the default interface to eth0

chenyin_h_4-1753181703806.png

 

3. Try transferring the image from your PC to the EVB3 via the tftp service.

I hope it will help.

 

BR

Chenyin

0 Kudos
Reply
1,244 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @MrAlexIV 

Thanks for your reply.

I suggest using the GMAC0 to transfer the binary instead of PFEX, since PFE may need additional configuration to have it functional under u-boot.

chenyin_h_0-1752818643520.png

 

BR

Chenyin

0 Kudos
Reply
1,241 Views
MrAlexIV
Contributor III

Thank you again,
I was trying to use GMAC0 but I could not see the interface. I had a eth0, but I could not set it UP. Do I need to do something in particular?
Thanks.     

0 Kudos
Reply
1,277 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @MrAlexIV 

Thanks for your reply.

Not sure how you starting the M core application via Linux.

A possible way is firstly flashed the full BSP to the SD card, then boot the board directly; Secondly, stopped in u-boot, and then use network connection to transfer your M core image to the DDR(or flash the M core application to the QSPI/eMMC in advance before boot, and in uboot, load it from QSPI to the DDR); After it, use the uboot to run the M7 application, next, to boot with your Linux. 

 

BR

Chenyin

0 Kudos
Reply
1,262 Views
MrAlexIV
Contributor III

Hi,
thank you for your response. I am trying to get the bin in my u-boot via tftp. I am having some issues tho, in particular I receive this messgae: 

=> tftp ${loadaddr} FlexCAN_Ip_Example_S32G399A_M7_blob2.bin

Attached to pfe0

Using eth_pfeng device

TFTP from server 192.168.128.244; our IP address is 192.168.128.249

Filename 'FlexCAN_Ip_Example_S32G399A_M7_blob2.bin'.

Load address: 0x80000000

Loading: *

ARP Retry count exceeded; starting again


I started the server on my pc (192.128.168.244)

MrAlexIV_0-1752749479232.png

In u-boot I applied this configuration:
setenv ipaddr 192.168.128.249
setenv serverip 192.168.128.244
setenv netmask  255.255.255.0
setenv gatewayip 192.168.128.1
setenv ethaddr 00:04:9F:09:6D:07 (since I connected my ethernet cable to PFE_MAC2)

I can't even ping 192.168.128.244 and yes, I disabled the firewall

0 Kudos
Reply
1,287 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @MrAlexIV 

Thanks for your post.

May I know if the bin file is used for running on M core or A cores? how and where could it be executed/called from your design?

May I know if you would like to only use the flash tool to flash it to your SD card, or other method could be acceptable?

 

BR

Chenyin

0 Kudos
Reply
1,282 Views
MrAlexIV
Contributor III

Hi, 

It is a M7 cortex. Any method is appreciated actually, I just want to flash my bin in a way that I can see the logs via Linux. At the moment, if I flags the bin on the SD card, I can't access while it is running (via Putty), so I flashed the BSP Linux on the SD and now I can access even when the SD is running. Any solution is appreciated. My final goal is to read the logs of my application, through Linux 

0 Kudos
Reply