S32G2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32G2

1,281件の閲覧回数
gopalakrishna
Contributor I

In one of our application using the S32G2 NXP processor (Part Nr: S32G254AABK1VUCT) and PCIe interface is using. A 100MHz (Clock freq configurable) external clock generator is interfaced for PCIE1_CLK_P, PCIE1_CLK_N signals.

Please confirm the clock type - LVDS/ LP-HSCL?

Thank you.

Regards,

Gopala

0 件の賞賛
返信
1 返信

1,267件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @gopalakrishna

Thanks for the question.

As far as I know, the external reference clock for PCIe/sgmii is HCSL level on RDB2, you can refer to design files of the RDB2 for details.

May I know if HCSL could also be accepted or have to be LP-HCSL ?

 

Best Regards

Chenyin

0 件の賞賛
返信