S32G2-VNP-RDB2 for Core M7, Application gateway

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32G2-VNP-RDB2 for Core M7, Application gateway

ソリューションへジャンプ
2,554件の閲覧回数
Balavanth_1993
Contributor I

Hi Community,

I am working on S32G274A RDB2 board for M7 core,  for our gateway project, i needed firmwares like LLCE,PFE and HSE, and i have installed Automotive
Software Package Manager, but still i am not getting particular documents for core M7 and gateway, could anyone suggest how to get a flow on M7.

Thanks in advance,

Balavanth.

 

0 件の賞賛
返信
1 解決策
2,522件の閲覧回数
bpe
NXP Employee
NXP Employee

Automotive Software Package Manger is an online tool. You cannot download it.
After you select packages to download, it offers you two files, one is a self-
extractor to install, another is a Manual. Make sure you saved both of them.
Follow the Manual to install the package(s) you selected. More information is
available in each package's installation directory. For ARM M7 core details,
Arm Cortex-M7 Processor Technical Reference Manual, DDI 0489D Revision r1p1. 

Best Regards,
Platon

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,523件の閲覧回数
bpe
NXP Employee
NXP Employee

Automotive Software Package Manger is an online tool. You cannot download it.
After you select packages to download, it offers you two files, one is a self-
extractor to install, another is a Manual. Make sure you saved both of them.
Follow the Manual to install the package(s) you selected. More information is
available in each package's installation directory. For ARM M7 core details,
Arm Cortex-M7 Processor Technical Reference Manual, DDI 0489D Revision r1p1. 

Best Regards,
Platon

 

 

0 件の賞賛
返信