S32G2 - NOR Flash interrupt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32G2 - NOR Flash interrupt

2,605 Views
sangrael
Contributor I

Hi! I am using S32G274A chip and checking the design with S32G_0P77B: Mask Set Errata for Mask 0P77B.

It says the interrupt pin on QSPI must be low during the boot and all NXP reference design use

NOR Flash (QSPI) with an interrupt pin. I can see the NOR Flash on the design is not from a major manufacturer. Is that because S32G2 needs NOR Flash with an interrupt pin?

sangrael_0-1652064162362.png

 

The NOR Flash on my design doesn't have an interrupt pin (I think that's normal not to have an interrupt pin). Is it okay not to have an interrupt pin or I need to change NOR flash with an interrupt pin?

 

sangrael_1-1652064326694.png

 

Regards,

Sangrae

 

 

Labels (1)
0 Kudos
Reply
2 Replies

2,577 Views
marcuslim
NXP Employee
NXP Employee

Hi Sangrae,

 

The interrupt in the Flash is meant for ECC.  This depends if you need this feature.  If in use, you will need to ensure S32G interrupt pin is per the Errata mentioned. 

 

Regards,

Marcus

0 Kudos
Reply

2,593 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello sangrael,

 

It is ok, if your NOR does not need an Interrupt.

Regards

 

0 Kudos
Reply