S32G2 Linux BSP build fail

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32G2 Linux BSP build fail

跳至解决方案
881 次查看
yangjinzhuang
Contributor IV

Hello,

      I chose YOCTO to build Linux-BSP 39.0, I chose to build auto target

       my ubuntu is 22.04, 8 cores and memory more than 8M, is it OK?  (Ubuntu version must be 18.04.4 LTS?)

      My PC restarts everytime and build failed.

       What are the minimum requirements for the number of cores, memory, and operating system for the compiler PC?

0 项奖励
回复
1 解答
866 次查看
chenyin_h
NXP Employee
NXP Employee

From the BSP39.0 UM, it is mentioned that  

“All the steps described below have been run and validated on Ubuntu-20.04 LTS (native or through a virtual machine). It is then recommended to install Ubuntu-20.04 LTS before going through the following sections.”

“A Yocto build needs at least 50GB of free space and takes a lot of time (2 to 10 hours, depending on the system configuration). It is recommended to use a powerful system with many cores and a fast storage media (SSD is recommended). The recommended RAM size is 8 GB.”

So, in summary, it is suggested that:

  1. Host: Ubuntu20.04-LTS is recommended.
  2. DDR: 8GB+ is recommended.
  3. Storage: SSD is recommended, better to have large size
  4. CPU: Powerful CPU with many cores.

Hope it helps.

 

Best Regards

Chenyin

 

在原帖中查看解决方案

0 项奖励
回复
1 回复
867 次查看
chenyin_h
NXP Employee
NXP Employee

From the BSP39.0 UM, it is mentioned that  

“All the steps described below have been run and validated on Ubuntu-20.04 LTS (native or through a virtual machine). It is then recommended to install Ubuntu-20.04 LTS before going through the following sections.”

“A Yocto build needs at least 50GB of free space and takes a lot of time (2 to 10 hours, depending on the system configuration). It is recommended to use a powerful system with many cores and a fast storage media (SSD is recommended). The recommended RAM size is 8 GB.”

So, in summary, it is suggested that:

  1. Host: Ubuntu20.04-LTS is recommended.
  2. DDR: 8GB+ is recommended.
  3. Storage: SSD is recommended, better to have large size
  4. CPU: Powerful CPU with many cores.

Hope it helps.

 

Best Regards

Chenyin

 

0 项奖励
回复