S32G2 : LLCE CAN Controller MIXED interrupt setting

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32G2 : LLCE CAN Controller MIXED interrupt setting

ソリューションへジャンプ
3,373件の閲覧回数
skseofh
Contributor II

Hi~

I'm using S32G274A.

In 'LLCE firmware user guide.pdf' page 12, there is explanation on MIXED interrupt processing.(See below)

skseofh_0-1636598264538.pngskseofh_0-1636598264538.png

Based on this docs, I thought that FIFO can be configurable between INTERRUPT and POLLING.

But in S32DS 3.4 IDE peripheral component setting, there is no configuration on FIFO about INTR & POLLING.

I only can find CAN Controller level configuration.(See below)

skseofh_1-1636598574703.pngskseofh_1-1636598574703.png

 

How do I set INTR to some FIFOs and POLLING to some FIFOs on SAME CAN Controller?

0 件の賞賛
返信
1 解決策
3,329件の閲覧回数
bpe
NXP Employee
NXP Employee

In mixed mode, you need several HRH's each configured for either polling or
interrupt. See the Sections 3.6.2 and 3.6.3 of the CAN_LLCE Driver User Manual
for detailed information. Sections 4.116, 4.118 discuss related
Tresos configuration objects and their parameters.

Best Regards,
Platon

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,330件の閲覧回数
bpe
NXP Employee
NXP Employee

In mixed mode, you need several HRH's each configured for either polling or
interrupt. See the Sections 3.6.2 and 3.6.3 of the CAN_LLCE Driver User Manual
for detailed information. Sections 4.116, 4.118 discuss related
Tresos configuration objects and their parameters.

Best Regards,
Platon

 

0 件の賞賛
返信
3,298件の閲覧回数
skseofh
Contributor II

Thank you!

It really helps me to understand.

0 件の賞賛
返信