S32G2 Eth_43_PFE Problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32G2 Eth_43_PFE Problem

7,363件の閲覧回数
jack_huang1
Contributor IV

Dear,

       When the eth_43_PFE module was imported into the Davinci tool, the generated code failed to be compiled. See Figure 1 for details. 

        The error content is as follows:

/include/oal_mutex_autosar.h:660:22: error: 'SchM_Exit_Eth_43_PFE_ETH_EXCLUSIVE_AREA_173' undeclared here (not in a function); did you mean 'SchM_Exit_Eth_43_PFE_ETH_EXCLUSIVE_AREA_ID'?

But there's actually a definition for SchM_Exit_Eth_43_PFE_ETH_EXCLUSIVE_AREA_173. See Figure 2 for details

I wonder if there is something wrong with the writing. Macro functions cannot directly assign values to a variable.

RTD uses SW32G_RTD_4.4_S32CC_4.0.1

PFE uses pfe-drv_s32g_m7_mcal_1.0.0_qlp3

Please help to see how to solve it.

Thank you very much.

Best Regards.

 

タグ(1)
0 件の賞賛
返信
4 返答(返信)

7,339件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Could be a problem with the tool itself, but due to you using a non-public RTD (v4.0.1 for what we understood), we recommend either opening a ticket under the NXP online service or sending this same topic to your local NXP FAE/representative, for them to channel it adequately, since could be related to a bug since it is still under development.

Please, let us know.

0 件の賞賛
返信

7,350件の閲覧回数
viswa_kondapall
Contributor IV

Hi Jack, 

Can i share same thread with you, for the same topic. In My case EBtresos but for you its davinci tool. 1. i am unable to load EB tresos generated code s32 design studio. 

2. Unable to find the good NXP example code for PFE. could you please share info like which sample project taken as example for PFE ??

3. PFE MCAL driver 0.9.7 is asking EBtresos project generated code and unable to compile the source code.

4. PFE-Demo code is there - which we too wanted PFE as Master bit it not compiling too. Unable to progress in PFE with sample project. 

AN13423 we following but for PFE few steps they missed and directly came to CAN2CAN project leave CAN2ETH project code in hanging in AIR.

regards,

Viswa

0 件の賞賛
返信

6,553件の閲覧回数
Youngsoo_do
Contributor III

Is there any solution to this problem?

I have the same problem using PFE.

0 件の賞賛
返信

6,539件の閲覧回数
viswa_kondapall
Contributor IV

We left it. me too eagerly waiting to find the solution. PFE-->ETH_43 interface.

0 件の賞賛
返信