S32G2 BSP 44 Ubuntu Build Failure

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32G2 BSP 44 Ubuntu Build Failure

Jump to solution
460 Views
sid_rotor
Contributor I

Hello, I am trying to build an ubuntu image for xx as specified by S32G2_LinuxBSP_44.0_User_Manual_updated_D250603.pdf. However, I am running into the following errors. Inspecting the configuration files, it appears that some of the system still expects `kirkstone` even though we are now building with `scarthgap`? And the glib versions that are expected don't seem to match. I have listed the commands run and the error output when I attempt to run the build. Am I missing some configuration?

Commands:

mkdir fsl-auto-yocto-bsp
cd fsl-auto-yocto-bsp
repo init -u https://github.com/nxp-auto-linux/auto_yocto_bsp/ -b release/bsp44.0 -m default.xml
repo sync
sudo apt update
./sources/meta-alb/scripts/host-prepare.sh
source nxp-setup-alb.sh -m s32g274ardb2ubuntu
# Set NXP_FIRMWARE_LOCAL_DIR in local/local.conf
bitbake fsl-image-ubuntu-base

Output:

❯ bitbake fsl-image-ubuntu-base
Loading cache: 100% |#######################################################################################################################################################################################################| Time: 0:00:00
Loaded 1143 entries from dependency cache.
ERROR: /path/reproduce-for-forum/fsl-auto-yocto-bsp/sources/meta-alb/meta-alb-sdk/recipes-fsl/images/fsl-image-ubuntu.bb: nativeaptinstall.bbclass is incompatible to the current layer set | ETA: 0:00:44
ERROR: /path/reproduce-for-forum/fsl-auto-yocto-bsp/sources/meta-alb/meta-alb-sdk/recipes-fsl/images/fsl-image-ubuntu.bb: You must check APTGET_YOCTO_TRANSLATION and update the anonymous python() function!
ERROR: /path/reproduce-for-forum/fsl-auto-yocto-bsp/sources/meta-alb/meta-alb-sdk/recipes-fsl/images/fsl-image-ubuntu-ros.bb: nativeaptinstall.bbclass is incompatible to the current layer set | ETA: 0:00:32
ERROR: /path/reproduce-for-forum/fsl-auto-yocto-bsp/sources/meta-alb/meta-alb-sdk/recipes-fsl/images/fsl-image-ubuntu-ros.bb: You must check APTGET_YOCTO_TRANSLATION and update the anonymous python() function!
ERROR: /path/reproduce-for-forum/fsl-auto-yocto-bsp/sources/meta-alb/meta-alb-sdk/recipes-fsl/images/fsl-image-ubuntu-base.bb: nativeaptinstall.bbclass is incompatible to the current layer set | ETA: 0:00:29
ERROR: /path/reproduce-for-forum/fsl-auto-yocto-bsp/sources/meta-alb/meta-alb-sdk/recipes-fsl/images/fsl-image-ubuntu-base.bb: You must check APTGET_YOCTO_TRANSLATION and update the anonymous python() function!
ERROR: /path/reproduce-for-forum/fsl-auto-yocto-bsp/sources/meta-alb/meta-alb-sdk/recipes-extended/ubuntu/ubuntu-base_22.04.1.bb: nativeaptinstall.bbclass is incompatible to the current layer setETA: 0:00:17
ERROR: /path/reproduce-for-forum/fsl-auto-yocto-bsp/sources/meta-alb/meta-alb-sdk/recipes-extended/ubuntu/ubuntu-base_22.04.1.bb: You must check APTGET_YOCTO_TRANSLATION and update the anonymous python() function!
Parsing recipes: 100% |#####################################################################################################################################################################################################| Time: 0:00:55
Parsing of 3692 .bb files complete (766 cached, 2926 parsed). 5803 targets, 617 skipped, 2 masked, 0 errors.
NOTE: Resolving any missing task queue dependencies
WARNING: preferred version 2.35 of cross-localedef-native not available (for item cross-localedef-native)
WARNING: versions of cross-localedef-native available: 2.31+git 2.39+git
WARNING: preferred version 2.38 of binutils-cross-aarch64 not available (for item virtual/aarch64-fsl-linux-binutils)
WARNING: versions of binutils-cross-aarch64 available: 2.34 2.42
WARNING: preferred version 2.35 of cross-localedef-native not available (for item cross-localedef-native-dev)
WARNING: versions of cross-localedef-native available: 2.31+git 2.39+git
WARNING: preferred version 2.35 of cross-localedef-native not available (for item cross-localedef-native)
WARNING: versions of cross-localedef-native available: 2.31+git 2.39+git
WARNING: preferred version 2.38 of binutils-crosssdk-x86_64-fslbsp-linux not available (for item virtual/x86_64-fslbsp-linux-binutils)
WARNING: versions of binutils-crosssdk-x86_64-fslbsp-linux available: 2.42
WARNING: preferred version 2.35 of nativesdk-glibc not available (for item virtual/nativesdk-libc)
WARNING: versions of nativesdk-glibc available: 2.39+git
WARNING: preferred version 2.35 of glibc not available (for item virtual/libc)
WARNING: versions of glibc available: 2.31+git 2.39+git
WARNING: preferred version 2.38 of binutils-native not available (for item binutils-native)
WARNING: versions of binutils-native available: 2.42
WARNING: preferred version 2.35 of nativesdk-glibc not available (for item virtual/nativesdk-libintl)
WARNING: versions of nativesdk-glibc available: 2.39+git
WARNING: preferred version 2.35 of nativesdk-glibc not available (for item virtual/nativesdk-libiconv)
WARNING: versions of nativesdk-glibc available: 2.39+git
WARNING: preferred version 2.35 of glibc not available (for item glibc-thread-db)
WARNING: versions of glibc available: 2.31+git 2.39+git
WARNING: preferred version 2.35 of glibc-locale not available (for item glibc-localedata-i18n)
WARNING: versions of glibc-locale available: 2.31 2.39+git
WARNING: preferred version 2.35 of glibc not available (for item glibc-utils)
WARNING: versions of glibc available: 2.31+git 2.39+git
WARNING: preferred version 2.35 of glibc not available (for item glibc-dbg)
WARNING: versions of glibc available: 2.31+git 2.39+git
WARNING: preferred version 2.35 of glibc not available (for item glibc-dev)
WARNING: versions of glibc available: 2.31+git 2.39+git
WARNING: preferred version 2.38 of binutils-cross-canadian-aarch64 not available (for item binutils-cross-canadian-aarch64)
WARNING: versions of binutils-cross-canadian-aarch64 available: 2.34 2.42
WARNING: preferred version 2.35 of nativesdk-glibc not available (for item nativesdk-ldconfig)
WARNING: versions of nativesdk-glibc available: 2.39+git
WARNING: preferred version 2.35 of nativesdk-glibc not available (for item nativesdk-glibc)
WARNING: versions of nativesdk-glibc available: 2.39+git
WARNING: preferred version 2.35 of nativesdk-glibc not available (for item nativesdk-glibc-utils)
WARNING: versions of nativesdk-glibc available: 2.39+git
WARNING: preferred version 2.35 of nativesdk-glibc not available (for item nativesdk-glibc-dev)
WARNING: versions of nativesdk-glibc available: 2.39+git
WARNING: preferred version 2.35 of glibc not available (for item glibc)
WARNING: versions of glibc available: 2.31+git 2.39+git
WARNING: preferred version 2.35 of glibc not available (for item ldconfig)
WARNING: versions of glibc available: 2.31+git 2.39+git
WARNING: preferred version 2.35 of glibc-locale not available (for item glibc-locale)
WARNING: versions of glibc-locale available: 2.31 2.39+git
ERROR: Nothing PROVIDES 'virtual/x86_64-fslbsp-linux-gcc-crosssdk' (but /path/reproduce-for-forum/fsl-auto-yocto-bsp/sources/meta-alb/meta-alb-sdk/recipes-devtools/binutils2.34/binutils-cross-canadian_2.34.bb DEPENDS on or otherwise requires it). Close matches:
virtual/x86_64-fslbsp-linux-g++
virtual/x86_64-fslbsp-linux-gcc
virtual/x86_64-fslbsp-linux-go
NOTE: Runtime target 'binutils-cross-canadian-aarch64' is unbuildable, removing...
Missing or unbuildable dependency chain was: ['binutils-cross-canadian-aarch64', 'virtual/x86_64-fslbsp-linux-gcc-crosssdk']
NOTE: Runtime target 'packagegroup-cross-canadian-s32g274ardb2' is unbuildable, removing...
Missing or unbuildable dependency chain was: ['packagegroup-cross-canadian-s32g274ardb2', 'binutils-cross-canadian-aarch64', 'virtual/x86_64-fslbsp-linux-gcc-crosssdk']
ERROR: Required build target 'fsl-image-ubuntu-base' has no buildable providers.
Missing or unbuildable dependency chain was: ['fsl-image-ubuntu-base', 'packagegroup-cross-canadian-s32g274ardb2', 'binutils-cross-canadian-aarch64', 'virtual/x86_64-fslbsp-linux-gcc-crosssdk']

Summary: There were 46 WARNING messages.
Summary: There were 10 ERROR messages, returning a non-zero exit code.

 

0 Kudos
Reply
1 Solution
399 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @sid_rotor 

Thanks for your reply.

As far as I know, the BSP version before 44(43 or earlier) could support the ubuntu build correctly, you may try using these versions for your work.

 

BR

Chenyin

View solution in original post

0 Kudos
Reply
3 Replies
426 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @sid_rotor 

Thanks for your post.

Building Ubuntu images for running on S32G processors is not available in BSP44 release, I feel sorry that the BSP UM is not updated correctly, I suggest ignoring the related chapter in the UM.

 

BR

Chenyin

0 Kudos
Reply
406 Views
sid_rotor
Contributor I
Thanks for the quick response. Is this also the case for other BSP versions? I will try to port our patches to a different BSP, but would like to make sure they support building an Ubuntu image.

Also, where might I be able to find a changelog/release notes/porting guide to update my BSP version?
0 Kudos
Reply
400 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @sid_rotor 

Thanks for your reply.

As far as I know, the BSP version before 44(43 or earlier) could support the ubuntu build correctly, you may try using these versions for your work.

 

BR

Chenyin

0 Kudos
Reply