S32G-VNP-RDB3 can not run the lwIP&&FreeRTOS example

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32G-VNP-RDB3 can not run the lwIP&&FreeRTOS example

2,444 Views
xueqing
Contributor I

hi  nxp

0 Kudos
Reply
5 Replies

2,265 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @xueqing 

Thanks for the reply.

If you have already downloaded the "PFE-DRV_S32G_M7_MCAL_xxx", unzip it and you may find example_application directory, there are several examples in it. you may reference the readme.txt in this directory for detailed reference.

Hope it helps.

 

Best Regards

Chenyin

0 Kudos
Reply

2,337 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @xueqing

Thank you for the reply.

You may reference the following method to find PFE related code/demos:

- Sign in to your NXP account (link to NXP site: Automotive, IoT & Industrial Solutions | NXP Semiconductors)
- Click on "My NXP Account" (top-right) and click on "Software Licensing and Support" under the "Licensing" section within the window it opens.
- This will redirect you to another page. In this new page, select the option "View Accounts" under the "Software accounts" section.
- This will again redirect you to another page. On this page, you should see an " Automotive SW – S32G Standard Software" option, click on it.

 

In there, you may see “Automotive SW - S32G - PFE Driver + Standard Firmware”, click on it, all the available versions are shown for your account.

Downloaded the S32G PFE MCAL 4.4 driver, then you may reference the code and the documents(both pdf and txt files) in it for further detaileds.

Hope it helps.

 

Best Regards

Chenyin

0 Kudos
Reply

2,412 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @xueqing

Thanks for the question

  1. If you want to use the lwIP related examples,  then you may have to install the packages including Real Time Drivers, FreeRTOS, TCP/IP stack. Use online Automotive Software Package Manager and download all mentioned above packages in a bundle to ensure version compatibility. Then you may study the documentation enclosed with these packages for installation steps and corresponding usage.
  1. Besides the samples mentioned above, you may also reference the PFE driver and the gPTP stack from the S32G reference software for studying more of the network usecase on M cores.

 

Best Regards

Chenyin

0 Kudos
Reply

2,279 Views
xueqing
Contributor I

hello  nxp

thanks for your  help!i find the file follow the steps.but i don't know how to use the file.......

can you give me some document and examples ,so  i can follow the steps to finish the test?

thanks

0 Kudos
Reply

2,352 Views
xueqing
Contributor I

hello  nxp

 

can you give me an example project with code and the guide document?

so  i can follow the steps  build and run the function

 

thank you 

0 Kudos
Reply