S32G-VNP-RDB3, UART Sample Debugging failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32G-VNP-RDB3, UART Sample Debugging failed

Jump to solution
2,654 Views
ulfschlieben
Contributor II

Hi all, 

I've added with the config tools some pins to the board setup and after the the debugging fails at the first call.

Any idea what could happen there ?

 

ulfschlieben_0-1715169534864.png

 

 

0 Kudos
Reply
1 Solution
2,555 Views
ulfschlieben
Contributor II

Hi all,

I found out that the update to SW32_S32DS_3.5.11_D2403.zip was the root cause, the S32DS was not usable anymore!

Downgrade S32DS V3.5   to Version SW32_S32DS_3.5.10_D2401.zip , fixed my problem

View solution in original post

0 Kudos
Reply
4 Replies
2,556 Views
ulfschlieben
Contributor II

Hi all,

I found out that the update to SW32_S32DS_3.5.11_D2403.zip was the root cause, the S32DS was not usable anymore!

Downgrade S32DS V3.5   to Version SW32_S32DS_3.5.10_D2401.zip , fixed my problem

0 Kudos
Reply
2,579 Views
ulfschlieben
Contributor II

HEre is a test source code that fails ...

0 Kudos
Reply
2,575 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Thanks for your feedback.

Can you let us know which RTD version are you using? Also, did the example work before adding the pins to the example?

Can you debug step by step to understand in which instruction is the program being sent to a HardFault? Which modifications have you implemented?

We also understand that the default debug configurations for S32G3 under S32DS are designed for S32 Debug Probe, can you confirm that you are able to debug the example without modifications with PE Micro's debugger?

Please, let us know.

0 Kudos
Reply
2,630 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Can you let us know which RTD version are you using? Also, did the example work before adding the pins to the example?

Can you debug step by step to understand in which instruction is the program being sent to a HardFault? Which modifications have you implemented?

We also understand that the default debug configurations for S32G3 under S32DS are designed for S32 Debug Probe, can you confirm that you are able to debug the example without modifications with PE Micro's debugger?

Please, let us know.

0 Kudos
Reply