S32G-VNP-RDB USB clarification

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32G-VNP-RDB USB clarification

1,356件の閲覧回数
nxpuser1231
Contributor I

I am referring to the schematic of S32G VNP for USB functionality, 

nxpuser1231_0-1658421366284.pngnxpuser1231_0-1658421366284.png

 

Now my questions are i can see a micro USB connector. The micro supports the USB2.0 OTG, and uses micro usb connector, can i use connectors of Type A for the host and Type B for the device functionality in place of micro usb by updating the schematic, so that i can use either of them. Please help.

 

0 件の賞賛
返信
1 返信

1,342件の閲覧回数
nxpuser1231
Contributor I

Actual requirement is instead of using USB Micro A/B connector, i have to use the type C connector. How to do it? 

0 件の賞賛
返信