S32G RTC slowly

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32G RTC slowly

Jump to solution
5,789 Views
StanleyShen
Contributor IV

Hi 

After I set the system clock and synchronized it to the RTC clock,

I found that the RTC clock would become slower and slower.

Could you tell me the reason?

It seems that the hardware is rtc-pcf85063.

Env.

CPU: S32G274A

BSP: 33.0

Yocto Machine:fsl-image-base

 

root@(none):~# date -s "2023-03-08 10:52:10"
root@(none):~# hwclock -w

 

 

 

root@(none):~# date && hwclock
Wed Mar  8 10:55:12 UTC 2023
Wed Mar  8 10:55:01 2023  0.000000 seconds
root@(none):~# date && hwclock
Wed Mar  8 10:55:20 UTC 2023
Wed Mar  8 10:55:10 2023  0.000000 seconds
root@(none):~# date && hwclock
Wed Mar  8 10:56:38 UTC 2023
Wed Mar  8 10:56:23 2023  0.000000 seconds
root@(none):~# date && hwclock
Wed Mar  8 10:56:40 UTC 2023
Wed Mar  8 10:56:25 2023  0.000000 seconds
。。。
root@(none):~# date && hwclock
Wed Mar  8 11:03:11 UTC 2023
Wed Mar  8 11:02:34 2023  0.000000 seconds
root@(none):~# date && hwclock
Wed Mar  8 11:06:32 UTC 2023
Wed Mar  8 11:05:44 2023  0.000000 seconds
root@(none):~# date && hwclock
Wed Mar  8 11:06:35 UTC 2023
Wed Mar  8 11:05:48 2023  0.000000 seconds

 

 

0 Kudos
Reply
1 Solution
5,698 Views
StanleyShen
Contributor IV

Hi Patel

Thanks for you help.

Just recording  to the dmesg Info. , I found two RTC devices:

 

# dmesg |grep rtc
[    0.924372] s32gen1-rtc 40060000.rtc: registered as rtc0
[    0.929816] s32gen1-rtc 40060000.rtc: setting system clock to 1970-01-01T00:00:00 UTC (0)
[    1.150208] rtc-pcf85063 0-0051: registered as rtc1

 

 The rtc0 is  default RTC and rtc1 is external RTC, when I was synchronized time to rtc1, 

No matter how long it takes, the time of both soft and hard has always been consistent.

 

# date -s "2023-03-08 10:52:10" &  hwclock -f /dev/rtc1 -w
# date && hwclock -f /dev/rtc1
Wed Mar  8 10:52:30 UTC 2023
2023-03-08 10:52:31.201735+00:00
。。。
# date && hwclock -f /dev/rtc1
Wed Mar  8 11:00:39 UTC 2023
2023-03-08 11:00:40.426119+00:00

 

 

if considering the FIRC running at 48 MHz

By default, it seems that the frequency  is 48 MHz

(linux-bsp33.0-5.10.109-rt/linux/arch/arm64/boot/dts/freescale/s32cc.dtsi )

StanleyShen_0-1680843920641.png

 

View solution in original post

0 Kudos
Reply
5 Replies
5,699 Views
MayanksPatel
NXP Employee
NXP Employee

Hi @StanleyShen,

Hope you are doing well.

 

The RTC shouldn’t be used as a hardware clock due to the clock that is used for its counters. The FIRC clock powers it on all NXP boards. We set FIRC’s reference frequency to 51MHz due to possible drifts caused by temperature variations (see BootROM_Clocking spreadsheet, part of S32G_boot_settings.xlsx, attached to the Reference Manual).  This is the main cause of the RTC imprecision, but it is expected. The RTC drift will be less observable if considering the FIRC running at 48 MHz, at room temperature, but this might not apply to other temperature ranges.

An external RTC module must be used for better precision. PCA85073A modules have been integrated on S32G RDB boards for this purpose. Another option is to use an external clock source for the RTC counters.

 

Hope this helps.

 

Thanks,

Mayank s Patel

 

0 Kudos
Reply
5,699 Views
StanleyShen
Contributor IV

Hi Patel

Thanks for you help.

Just recording  to the dmesg Info. , I found two RTC devices:

 

# dmesg |grep rtc
[    0.924372] s32gen1-rtc 40060000.rtc: registered as rtc0
[    0.929816] s32gen1-rtc 40060000.rtc: setting system clock to 1970-01-01T00:00:00 UTC (0)
[    1.150208] rtc-pcf85063 0-0051: registered as rtc1

 

 The rtc0 is  default RTC and rtc1 is external RTC, when I was synchronized time to rtc1, 

No matter how long it takes, the time of both soft and hard has always been consistent.

 

# date -s "2023-03-08 10:52:10" &  hwclock -f /dev/rtc1 -w
# date && hwclock -f /dev/rtc1
Wed Mar  8 10:52:30 UTC 2023
2023-03-08 10:52:31.201735+00:00
。。。
# date && hwclock -f /dev/rtc1
Wed Mar  8 11:00:39 UTC 2023
2023-03-08 11:00:40.426119+00:00

 

 

if considering the FIRC running at 48 MHz

By default, it seems that the frequency  is 48 MHz

(linux-bsp33.0-5.10.109-rt/linux/arch/arm64/boot/dts/freescale/s32cc.dtsi )

StanleyShen_0-1680843920641.png

 

0 Kudos
Reply
5,685 Views
MayanksPatel
NXP Employee
NXP Employee

Hi @StanleyShen,

Thanks for the update.

 

0 Kudos
Reply
5,718 Views
MayanksPatel
NXP Employee
NXP Employee

Hi @StanleyShen ,

Thank you for reaching out to NXP.

I am working on this ticket and already started discussion with internal engineering team.

I will get back to you once anything comes.

 

Thanks,

Mayank s Patel

0 Kudos
Reply
5,766 Views
StanleyShen
Contributor IV

Hi 

Can anyone help me?

0 Kudos
Reply