S32G RDB2 multicore boot hang in bsp41

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32G RDB2 multicore boot hang in bsp41

423 Views
Allen_Cheng
Contributor I

Hi NXP team,

 

I try to setup a multicores environment with A53 and M7 following AN13750 official document.

I found a boot issue in bsp41 and I also use bsp42 to clarify.

But BSP42 can bootup to Linux kernel successfully.

BSP41 will always hang in

bootloader 0x2 Application 1 image fragment 0 loaded from QSPI.
bootloader 0x2 Application M7_0 was loaded.

I add these two versions log in attachment.

Could you please help to clarify this issue?

Thanks.

 

SW:

Integration_Reference_Examples_S32G2_2023_06

EB 27.1

RTD 4.4_4.0.0_P05_HF01

HSE_FW S32G2XX_0_1_0_16

 

 

 

 

0 Kudos
Reply
9 Replies

400 Views
Joey_z
NXP Employee
NXP Employee

hi,Allen_Cheng

Did you change the ATF Load address and Entry point in the Bootloader? As shown in the following figure, the corresponding address is different for different versions of BSP.

Joey_z_0-1733455728747.png

Also, you need to check that no SRAM image loading and running addresses of M7 and fip are conflicting

BR

Joey

 

0 Kudos
Reply

386 Views
Allen_Cheng
Contributor I
Hi Joey,

The ATF load address are the same in bsp41/bsp42.
Entry point are 0x34700000.
Thanks.

Allen
0 Kudos
Reply

274 Views
Joey_z
NXP Employee
NXP Employee

hi,Allen_Cheng

Thank you for your reply.

Your BSP41 print message attachment shows that BL2 should not be started, check to see if the fip.bin of BSP41 was loaded correctly during your compliance with AN13750.

In addition, in order to provide better support, whether you can provide your blob.bin, I will test this problem for you as soon as possible.

BR

Joey

0 Kudos
Reply

249 Views
Allen_Cheng
Contributor I

Hi Joey,

 

Attachment is my blob.bin.

Thanks.

0 Kudos
Reply

217 Views
Joey_z
NXP Employee
NXP Employee

hi,Allen_Cheng

I have received your blob.bin and have repeated your problem and will solve it as soon as possible.
In addition, I found that BSP41 can be started using your blob.bin and BSP42's fip.bin, you can try it, I suspect that this may be caused by some initialization conflict between the ATF in BSP41 and the Bootloader used, this needs further testing.

BR

Joey

0 Kudos
Reply

204 Views
Allen_Cheng
Contributor I

Hi Joey,

 

I used the blob.bin and BSP42's fip.bin with BSP41's sdcard(official image+BSP41's fip.s32).

It can bootup to linux successfully.

So the result means the first question BL2 can't start in BSP41 may have certain issue?  

 

Another confusion:

If the ATF Load address and others condition are the same in BSP41 and BSP42, the blob.bin need to rebuild again? or they can use the same blob.bin?

 

Thanks!

 

Allen

0 Kudos
Reply

115 Views
Joey_z
NXP Employee
NXP Employee

hi,

1. According to the printed information, BL2 fails to start. There is an initialization conflict between fip.bin of BSP41 and the Bootloader you made, resulting in a start failure. Did you completely follow the configuration of AN13750? If you made some modifications, could you please give me more specific information? Or could you please provide me with your modified Bootloader project?
2.The ATF Load address in BSP41 is the same as that in BSP42. It should be noted that the Size is a little different, but it does not affect the result of starting kernal. When you have other changes to the initialization requirements, you need to modify the Bootloader project and then regenerate blob.bin.

BR

Joey

0 Kudos
Reply

96 Views
Allen_Cheng
Contributor I

Hi Joey,

 

All Configuration of the AN13750 are almost the same but I only modified:

1. u-boot : enable HSE and firmware path

2. ATF not apply mmc patch

3. remove m7_1 and m7_2 in bootloader

 

Attach files are bootlader and eb project.

Thanks.

 

Allen

0 Kudos
Reply

65 Views
Joey_z
NXP Employee
NXP Employee

hi,Allen_Cheng

Sorry for the late reply.
You can try Disable Secure Boot, as shown in the image below.

Joey_z_0-1734833365615.png

In addition, if you are not using mmc patch, make sure you modify the s32_common.mk file.

Wish it can help you.

BR

Joey

0 Kudos
Reply