S32G RDB2 boot hang in bsp42 + RTD4.0.2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32G RDB2 boot hang in bsp42 + RTD4.0.2

1,393件の閲覧回数
Allen_Cheng
Contributor II

Hi NXP team,

 

I want to create a multicore boot environment following AN13750.

Before the issue occurred, BSP42+RTD4.0.0 will bootup into Linux kernel successfully.

Below is my sw version:

Linux BSP42

RTD4.0.2 HF03

bootloader project(GoldVIP-S32G2-1.12.0)

HSE S32G2XX_0_2_22_0

 

boot hang log:(first time)

bootloader 0x2 ComDal_Init() done.
bootloader 0x2 CryptoDal HSE status HSE_STATUS_RNG_INIT_OK
bootloader 0x2 CryptoDal HSE status HSE_STATUS_INIT_OK
bootloader 0x2 CryptoDal HSE status HSE_STATUS_INSTALL_OK
bootloader 0x2 CryptoDal HSE status HSE_STATUS_BOOT_OK
bootloader 0x2 CryptoDal HSE status HSE_STATUS_CUST_SUPER_USER
bootloader 0x2 CryptoDal HSE status HSE_STATUS_PRIMARY_SYS_IMAGE
bootloader 0x2 HSE FW Version: 0.1.0_2.22.0
bootloader 0x2 CryptoDal skipped the key catalogs format
bootloader 0x2 Bootloader secure boot is enabled.
bootloader 0x2 Bootloader initialization complete.
bootloader 0x2 Application 0 image fragment 0 of size 262144 was loaded from QSPI, address 0x100000.
bootloader 0x2 Application 0 image fragment 0 was loaded in 10.847 milliseconds.
bootloader 0x2 Application A53_0 was loaded.
bootloader 0x2 Application 1 image fragment 0 of size 1048576 was loaded from QSPI, address 0x200000.
bootloader 0x2 Application 1 image fragment 0 was loaded in 15.135 milliseconds.
bootloader 0x2 Application M7_0 was loaded.
NOTICE: Reset status: Power-On Reset
NOTICE: BL2: v2.10.0 (release):bsp42.0-2.10-dirty
NOTICE: BL2: Built : 13:53:34, Jan 16 2025
NOTICE: BL2: Booting BL31

After RDB2 power cycle log:

bootloader 0x2 ComDal_Init() done.

 

Could you please supply some suggestions?

Thanks.

 

Allen

0 件の賞賛
返信
3 返答(返信)

1,372件の閲覧回数
Joey_z
NXP Employee
NXP Employee

Hi,Allen_Cheng

Thank you for contacting us.

Is Application 1 Image an IPCF image? Which version of IPCF are you using?

In addition, which version of the bootloader project are you using?

BR 

Joey

0 件の賞賛
返信

1,337件の閲覧回数
Allen_Cheng
Contributor II

Hi Joey,

 

Sorry to late reply.

Is Application 1 Image an IPCF image? Which version of IPCF are you using?

Ans: based on 4.6(AN13750 example version) patch to 4.8

In addition, which version of the bootloader project are you using?

Ans: the bootloader project from GoldVIP-S32G-1.12.0

 

Thanks.

 

Allen

0 件の賞賛
返信

1,283件の閲覧回数
Joey_z
NXP Employee
NXP Employee

Hi,Allen_Cheng

Thank you for your reply.

According to the ReleaseNotes, If you are using the version 4.8 of IPCF , then the RTD version 4.0.0 is required. If you are using the version 4.9 of IPCF , then the RTD version 4.0.2 is required.

BR

Joey

0 件の賞賛
返信