S32G3 BSP41 PFE2 RGMII to RGMII without PHY on the customized board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32G3 BSP41 PFE2 RGMII to RGMII without PHY on the customized board

Jump to solution
3,085 Views
XD
Contributor II

Hi,

Our hardware design connects PFE2 RGMII directly to the switch RGMII without a PHY. The PFE2 is configured with rgmii-id, and we have verified the 125MHz TX clock output. I have come across discussions suggesting the use of a common external clock for both sides. Is clock drifting the only concern in this setup? If so, is it possible to configure PFE2 as a clock slave and use the clock output from the switch to synchronize TX and RX?

Thanks,

XD

0 Kudos
Reply
1 Solution
2,963 Views
alejandro_e
NXP TechSupport
NXP TechSupport

Hello @XD,

I can not access the technical information for the Marvell Switch, however, I see it is relatively similar to the SJA1110, for which you can check the following document: AN13335.pdf, in particular please check section 2.2 RGMII interface in page 8:

 
 

Screenshot 2025-01-31 115639.png

 

Let me know if this information solved your problem.

 

View solution in original post

0 Kudos
Reply
7 Replies
3,064 Views
alejandro_e
NXP TechSupport
NXP TechSupport

Hello @XD,

It is good to support you again. About your question, please refer the the S32G3 - Hardware Design Guidelines, in particular please check sections: 10 Communication Peripherals, 10.1.1 RGMII signal routing requirements and 13.3 High-speed routing recommendations.

There you should be able to find all the relevant information about RGMII on a HW level.

 

Let me know if you have more questions about this topic.

 

   

0 Kudos
Reply
3,037 Views
XD
Contributor II

Hi @alejandro_e ,

It's great that you're helping me again—I really appreciate it.

The guideline you provided is for an RGMII-to-PHY scenario. Do you have any guidelines for a direct RGMII-to-RGMII connection without a PHY?

Thanks,

XD

0 Kudos
Reply
3,027 Views
alejandro_e
NXP TechSupport
NXP TechSupport

Hello @XD,

To the best of my knowledge the same guidelines should apply to any device connected using RGMII, either a PHY or a switch. 

with that said, can you share the RGMII device you are connecting the S32G3 to? So I can check if there could be special considerations.

 

Thanks in advance.

0 Kudos
Reply
3,010 Views
XD
Contributor II

Hi @alejandro_e ,

We have a Marvell switch port running in RGMII mode, connected to PFE2 on our hardware.

Thanks,

XD

0 Kudos
Reply
2,964 Views
alejandro_e
NXP TechSupport
NXP TechSupport

Hello @XD,

I can not access the technical information for the Marvell Switch, however, I see it is relatively similar to the SJA1110, for which you can check the following document: AN13335.pdf, in particular please check section 2.2 RGMII interface in page 8:

 
 

Screenshot 2025-01-31 115639.png

 

Let me know if this information solved your problem.

 

0 Kudos
Reply
2,958 Views
XD
Contributor II

Hi @alejandro_e ,

Thank you again for your help. This information is very helpful.

Thanks,

XD

0 Kudos
Reply
2,794 Views
alejandro_e
NXP TechSupport
NXP TechSupport

Hello @XD,

I am glad you found the information helpful. Thanks for accepting my answer as a solution.

 

Best regards,

Alejandro 

0 Kudos
Reply