S32G QSPI issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32G QSPI issue

932 Views
Alex_mjl
Contributor II

Hi NXP,

    The chip I am currently using is S32G274ARDB2. I'm using both the A-core and M-core of this chip. I want them to have access to use QSPI Nor-flash.

    With reference to the AN13750, I have implemented starting both A and M cores at the same time. But on this basis, I wanted M-core applications to access QSPI and ran into some problems. The current phenomenon is as follows:

    Refer to AN13750, I only start M-core, and using bootloader + M-app, the QSPI driver can work normally in the M-core APP. Once the A-core is started on this basis, the QSPI Nor-flash of the M-core APP cannot be initialized normally. The M-APP QSPI Nor-flash init function crashed in the following function:

Alex_mjl_0-1731250731524.png

At the same time, I also checked the code of A-core, and when the ATF of A-core ran this function, it caused the M-core QSPI Nor-flash initialization failed.

Alex_mjl_1-1731251042109.png

 

0 Kudos
Reply
0 Replies