Hi experts,
I am working on an example of IPCF on S32G399A board IPCF_FreeRTOS_S32G399A_M7_0
I got the error shown in the attachment screenshot.
Versions:
IPCF: 4.10.0
BSP : 41
Hello @MohamedAbdelslam ,
Thank you for contacting NXP Tech Support. Kindly note that the versions of IPCF used by the M core and the A core must be consistent. Since the IPCF version you are using on the M core is 4.10.0, the A core should also employ version 4.10.0. However, the default IPCF in Linux BSP41 may not be this version. You need to manually compile IPCF 4.10.0 for Linux. The source code of IPCF for the A core is available at the following link: https://github.com/nxp-auto-linux/ipc-shm.
We hope the above information is of use to you.
Best Regards,
Celeste