S32G QSPI Micron configuration

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32G QSPI Micron configuration

1,169 次查看
Ciprian
Contributor I

Hello,

I am trying to configure a Micron MT25QU512 external flash for S32G, but I cannot find any suitable examples. Can someone help me with any Tresos example for Micron configuration?

0 项奖励
回复
1 回复

1,144 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

The only available project that is not related to the embedded Macronix NOR Flash under the different S32G reference boards is the one provided under the S32 Flash Tool installation folder. The related guide should be provided under the following path:

"C:/nxp/S32DS.3.4/S32DS/help/resources/howto/HOWTO_Use_FlashSDK_to_add_support_for_QuadSPI_flash_memory_devices_for_S32_Flash_Tool.pdf"

But again, is to create a new binary to be used under the S32 Flash Tool.

For the S32G family, there is no configuration example project for other NOR Flash vendors. The only documentation available is the AN13563 which can be found under the S32G2 product page (link: S32G2 Safe and Secure Vehicle Network Processor | NXP Semiconductors). We do apologize.

Please, let us know.

0 项奖励
回复