S32G LLCE CAN HOH filter priority

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32G LLCE CAN HOH filter priority

ソリューションへジャンプ
1,242件の閲覧回数
chansookang
Contributor III

Hello,

I've been working with the S32G CAN LLCE, and it seems that the priority of HRH filters in the CanHardwareObject configuration is not mainly determined by the index or object ID order.

In my case, I had both FULL and BASIC filter types configured, and even though the BASIC filter had a lower index, it looked like the FULL filter matched first.

When multiple HOHs are configured for the same controller, how exactly is the matching priority determined? (index, basic/full, filter code size? etc)

 

タグ(1)
0 件の賞賛
返信
1 解決策
1,209件の閲覧回数
Joey_z
NXP Employee
NXP Employee

hi,chansookang

Thank you for your information.

Refer to the RTD_CAN_LLCE_UM.pdf,All filter entries for a channel are searched in ‘order’ – the first match completes the search. Therefore, If FULL filter is tried first and it fails, search will continue and eventually match a BASIC filter.

Joey_z_1-1750734824797.png

Joey_z_0-1750734785039.png

Hope it can help you.

BR

Joey

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,210件の閲覧回数
Joey_z
NXP Employee
NXP Employee

hi,chansookang

Thank you for your information.

Refer to the RTD_CAN_LLCE_UM.pdf,All filter entries for a channel are searched in ‘order’ – the first match completes the search. Therefore, If FULL filter is tried first and it fails, search will continue and eventually match a BASIC filter.

Joey_z_1-1750734824797.png

Joey_z_0-1750734785039.png

Hope it can help you.

BR

Joey

0 件の賞賛
返信
1,228件の閲覧回数
Joey_z
NXP Employee
NXP Employee

hi,chansookang

Thank you for your reply.

Could you share more information for us?

Which version of LLCE are you using? Are you using S32G3 or S32G2?

BR

Joey

0 件の賞賛
返信
1,222件の閲覧回数
chansookang
Contributor III

Hello, 

i am using LLCE 1.0.9 and S32G2 (s32g274a rdb2)

thank you

タグ(1)
0 件の賞賛
返信