S32G EB Tresos Studio failed to activate

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32G EB Tresos Studio failed to activate

4,835 Views
heshuwen
Contributor I

image.pngplease tell me how to solve the problem?

0 Kudos
Reply
7 Replies

3,517 Views
Hang
Contributor I

Is it impact from internect issue when we work on China?
Do we need conect VPN to jump and then active code for Tresos?

0 Kudos
Reply

3,458 Views
Hang
Contributor I

OK, success.
I try to more time it's success.

I  think we need a good internet environment.

0 Kudos
Reply

4,805 Views
asap
NXP Employee
NXP Employee

heshuwen,

At your step2, once you are clicking through, you should be able to find the "activation code" to be used for your EB client license registration. here below a screenshot: 

 asap_0-1649056625519.png

 

Albert
0 Kudos
Reply

4,801 Views
heshuwen
Contributor I

What can't be activated is version 28.0.0, so I suspect it is a version problem, then I downloaded version 28.2.0, after downloading version 28.2.0, I double-clicked ''EB_Client_License_Administrator_1_4_3_Setup.exe'',but it can't run on my computer.And I have windows 10 installed on my computer.

0 Kudos
Reply

4,607 Views
zongliang
Contributor II

hi heshuwen, can you share a link as i want to download version 28.2.0

0 Kudos
Reply

4,803 Views
heshuwen
Contributor I

Hi asap,

  My mean is that I can download the EB Tresos Studio and I had get the activation code,but when I fill it in the ''activation code'' window, it still reports an error message:

  

INFO: Trusted Storage initialization done.
Activating NodeLocked License 98B6-6782-A434-4E40, Number Of Licenses: 1
Status: 4, Creating request

Status: 5, Request created

Status: 6, Context created

Status: 0, Error

ERROR: flxActAppActivationSend (50041,41143,34)
Connection to FlexNet Operations Server failed.

heshuwen_0-1649059452526.png

 

 

 

0 Kudos
Reply

4,829 Views
heshuwen
Contributor I

also I download the newest edition and click EB_Client_License_Administrator_1_4_3_Setup.exe,but it dosen't work

1.

heshuwen_0-1648891454124.png

2.

heshuwen_1-1648891485509.png

 

3.

heshuwen_2-1648891506373.png

 

0 Kudos
Reply