S32G EB Tresos Studio failed to activate

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32G EB Tresos Studio failed to activate

4,870件の閲覧回数
heshuwen
Contributor I

image.pngplease tell me how to solve the problem?

0 件の賞賛
返信
7 返答(返信)

3,552件の閲覧回数
Hang
Contributor I

Is it impact from internect issue when we work on China?
Do we need conect VPN to jump and then active code for Tresos?

0 件の賞賛
返信

3,493件の閲覧回数
Hang
Contributor I

OK, success.
I try to more time it's success.

I  think we need a good internet environment.

0 件の賞賛
返信

4,840件の閲覧回数
asap
NXP Employee
NXP Employee

heshuwen,

At your step2, once you are clicking through, you should be able to find the "activation code" to be used for your EB client license registration. here below a screenshot: 

 asap_0-1649056625519.png

 

Albert
0 件の賞賛
返信

4,836件の閲覧回数
heshuwen
Contributor I

What can't be activated is version 28.0.0, so I suspect it is a version problem, then I downloaded version 28.2.0, after downloading version 28.2.0, I double-clicked ''EB_Client_License_Administrator_1_4_3_Setup.exe'',but it can't run on my computer.And I have windows 10 installed on my computer.

0 件の賞賛
返信

4,642件の閲覧回数
zongliang
Contributor II

hi heshuwen, can you share a link as i want to download version 28.2.0

0 件の賞賛
返信

4,838件の閲覧回数
heshuwen
Contributor I

Hi asap,

  My mean is that I can download the EB Tresos Studio and I had get the activation code,but when I fill it in the ''activation code'' window, it still reports an error message:

  

INFO: Trusted Storage initialization done.
Activating NodeLocked License 98B6-6782-A434-4E40, Number Of Licenses: 1
Status: 4, Creating request

Status: 5, Request created

Status: 6, Context created

Status: 0, Error

ERROR: flxActAppActivationSend (50041,41143,34)
Connection to FlexNet Operations Server failed.

heshuwen_0-1649059452526.png

 

 

 

0 件の賞賛
返信

4,864件の閲覧回数
heshuwen
Contributor I

also I download the newest edition and click EB_Client_License_Administrator_1_4_3_Setup.exe,but it dosen't work

1.

heshuwen_0-1648891454124.png

2.

heshuwen_1-1648891485509.png

 

3.

heshuwen_2-1648891506373.png

 

0 件の賞賛
返信