S32DS on Ubuntu

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32DS on Ubuntu

1,584 次查看
Coco111
Contributor III

Hello, my friend, I want to know the answers to the following questions. Thank you very much。

 

 

Question1: Why is RTD not recognized on ubuntu S32DS?

Question2: When I want to upgrade SW32G_S32DS_3.4.3_D2112.zip, do I need to complete the upgrade for SW32G2_ S32DS_ 3.4.1_ D2104.zip first?

Question3: what' the difference between SW32G_RTD_4.4_3.0.2_HF01_DS_updatesite_D2204.zip and SW32_RTD_4.4_3.0.4_DS_updatesite_D2207.zip?

Screenshot from 2023-03-23 16-00-19.pngScreenshot from 2023-03-23 16-00-19.pngScreenshot from 2023-03-23 15-58-50.pngScreenshot from 2023-03-23 15-58-50.png

0 项奖励
回复
2 回复数

1,338 次查看
supergyr
Contributor I

I got the same problem on ubuntu that there's no RTD in S32DS Extensions and Updates after clicking "Add Update Sites" and choosing SW32G_RTD_4.4_4.0.2_D2306_DS_updatesite.zip.

0 项奖励
回复

1,517 次查看
MayanksPatel
NXP Employee
NXP Employee

Hi @Coco111,

 

Sorry for the delay.

Question1: Why is RTD not recognized on ubuntu S32DS?
Answer: Can you please re-install RTD Packages into the S32DS as it seems that the RTD Packages were not installed properly.

Question2: When I want to upgrade SW32G_S32DS_3.4.3_D2112.zip, do I need to complete the upgrade for SW32G2_ S32DS_ 3.4.1_ D2104.zip first?
Answer: You need to sequentially install development packages first you need to install SW32G2_ S32DS_ 3.4.1_ D2104.zip and then after need to install SW32G_S32DS_3.4.3_D2112.zip as SW32G_S32DS_3.4.3_D2112.zip contains new eclipse version and that might create problem while you install SW32G2_ S32DS_ 3.4.1_ D2104.zip.

Question3: what' the difference between SW32G_RTD_4.4_3.0.2_HF01_DS_updatesite_D2204.zip and SW32_RTD_4.4_3.0.4_DS_updatesite_D2207.zip?
Answer: Aside from 3.0.4 being more recent, the HF should integrate minor bug correction in relation to the non-HF version (i.e v3.0.2 vs v3.0.2HF01).
As for recommendations, It depends on which stacks/packages you are trying to implement. Some stacks/packages are only compatible with some versions,
giving trouble with other version.

Hope this helps to you.

 

Thanks,

Mayank s Patel