Rootfs Size Expansion on S32G-VNP-RDB2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Rootfs Size Expansion on S32G-VNP-RDB2

1,161件の閲覧回数
dylee
Contributor II

Hello,

I am using the S32G-VNP-RDB2 and currently working with Yocto BSP35 release version. After generating the image and loading it onto the eMMC, I noticed that the rootfs size is very small. Could you please provide guidance on how to increase the rootfs size using Yocto?

Additionally, I downloaded the e2fsprogs package through Yocto, and while the necessary tools like e2fsck and tune2fs are available, resize2fs is missing.

 

root@s32g274ardb2:/sbin# df
Filesystem 1K-blocks Used Available Use% Mounted on
/dev/root 879752 494572 320876 61% /
devtmpfs 1617268 0 1617268 0% /dev
tmpfs 1748980 0 1748980 0% /dev/shm
tmpfs 699596 8728 690868 2% /run
tmpfs 4096 0 4096 0% /sys/fs/cgroup
tmpfs 1748980 0 1748980 0% /tmp
tmpfs 1748980 172 1748808 1% /var/volatile
tmpfs 1748980 0 1748980 0% /var/volatile/tmp
tmpfs 349796 0 349796 0% /run/user/0
root@s32g274ardb2:/sbin#

 

Could you please advise on how to resolve this issue?

Thank you.

 

 

0 件の賞賛
返信
1 返信

1,126件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

For the available documentation under the S32G2 product, we don't see any information on regards on rootfs size increasement. We do apologize.

What we are seeing is that under the following community threads information is provided that could be useful:

Solved: How to increase the Memory size of Dom0 and Domu in S32G goldvip image - NXP Community

S32G Gold Box - AVB(openavnu) - NXP Community

Aside from this, we are not seeing much information.

Again, we do apologize.

Please, let us know.

0 件の賞賛
返信