Reset handler for BSP image

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Reset handler for BSP image

689 次查看
Abhiram_m_s
Contributor I

Hello,
We were configuring our boot-loader to boot both the cores simultaneously. We are not able to find the reset handler address and the RAM entry point address of the BSP image which we built. Can you tell us where to find the address of mentioned above.

Thank you.
Regards.
Abhiram M S

0 项奖励
回复
1 回复

668 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Which BSP version are you using? Commonly, this information is provided under the TF-A build process, similar to the one shown under AN13750 available under the S32G2 product page (link: S32G2 Safe and Secure Vehicle Network Processor | NXP Semiconductors) [Page 12, Enabling Multicore Application on S32G2 using S32G2 Platform Software Integration, Rev. 0, 11/2022]:

DanielAguirre_0-1717595859824.png

Please, let us know.

0 项奖励
回复