Reset handler for BSP image

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Reset handler for BSP image

690 Views
Abhiram_m_s
Contributor I

Hello,
We were configuring our boot-loader to boot both the cores simultaneously. We are not able to find the reset handler address and the RAM entry point address of the BSP image which we built. Can you tell us where to find the address of mentioned above.

Thank you.
Regards.
Abhiram M S

0 Kudos
Reply
1 Reply

669 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Which BSP version are you using? Commonly, this information is provided under the TF-A build process, similar to the one shown under AN13750 available under the S32G2 product page (link: S32G2 Safe and Secure Vehicle Network Processor | NXP Semiconductors) [Page 12, Enabling Multicore Application on S32G2 using S32G2 Platform Software Integration, Rev. 0, 11/2022]:

DanielAguirre_0-1717595859824.png

Please, let us know.

0 Kudos
Reply