Question about MCAL LLCE Driver Timeout Setting

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question about MCAL LLCE Driver Timeout Setting

1,401件の閲覧回数
zyz
Contributor III

zyz_0-1749713248847.pngzyz_0-1749713248847.png



In the EB configuration, the default timeout value for LLCE is set to 1 second. We intend to reduce it (e.g., to 10ms) to avoid prolonged blocking in abnormal conditions, which may impact business responsiveness.

However, upon reviewing the LLCE driver code, we noticed this parameter is used in multiple places, some involving interactions with the S32G's LLCE core. Thus, we are uncertain about the minimum safe threshold to avoid potential errors.

Could you please clarify:

  1. What is the minimum recommended timeout value to ensure stability?

  2. Are there any constraints or best practices to follow when adjusting this parameter to prevent adverse effects on the LLCE core?

0 件の賞賛
返信
4 返答(返信)

1,351件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @zyz 

Thanks for your reply.

I understand your point, but by checking it internally, it is confirmed that these timeout values in MCAL depend on customer application request, usually we do not provide any recommand value. I apologize.

From the experience, these values depends on the customer application requirements/protocol/spec/standard(like AUTOSAR,etc.), it varies for different use cases.

 

BR

Chenyin

0 件の賞賛
返信

1,350件の閲覧回数
zyz
Contributor III

Hi,chenyin_h

I understand what you mean, but in scenarios like the one below, I don't see how it relates to the customer's application requirements.
zyz_0-1749783513070.pngzyz_0-1749783513070.png

 

0 件の賞賛
返信

1,383件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @zyz 

Thanks for your post.

There are max/min values existed, which are shown below, but no recommended values from RTD's perspective, the timeout value itself depend on the customer application request.

chenyin_h_0-1749725644851.pngchenyin_h_0-1749725644851.png

 

BR

Chenyin

 

0 件の賞賛
返信

1,375件の閲覧回数
zyz
Contributor III

I understand this parameter should be configured per user requirements, but we can only evaluate it based on our specific needs. Since multiple driver interactions with the LLCE core depend on this parameter, we cannot assess the appropriateness of the timeout values for these scenarios. We're concerned that setting it too small may cause frequent LLCE response timeouts.

 

0 件の賞賛
返信