Question about AN13423

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question about AN13423

Jump to solution
3,367 Views
IP_EMBK
Contributor I

Hi,

I'm trying to follow the steps outlined in AN13423: Using CAN2CAN, CAN2ETH and ETH2CAN Features of LLCE on S32G - Application Note .

Paragraph 3.1 suggests to download the latest release form September 2021 -S32G_LLCE_GATEWAY_1.0.2_HF2_D2109.exe however the latest version available for download is S32G2XX_LLCE_GATEWAY_1.0.1_HF1_D2106.exe. 

IP_EMBK_0-1645651846447.png

 

Could you please publish version 1.0.2_HF2_D2109?

Thanks

Igor

0 Kudos
Reply
1 Solution
3,347 Views
bpe
NXP Employee
NXP Employee

Use online Automotive Software Package Manager to obtain the software you need:

 

bpe_0-1645778533593.png

 

Best Regards,
Platon

 

View solution in original post

0 Kudos
Reply
1 Reply
3,348 Views
bpe
NXP Employee
NXP Employee

Use online Automotive Software Package Manager to obtain the software you need:

 

bpe_0-1645778533593.png

 

Best Regards,
Platon

 

0 Kudos
Reply