QSPI secboot failed with SDK BSP43 secboot image on RDB3

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

QSPI secboot failed with SDK BSP43 secboot image on RDB3

5,195件の閲覧回数
hittzt
Senior Contributor I

Hi,

 

I tested secure boot on RDB3 board with SDK BSP43 release images, but it failed when test qspi secure boot feature, and I attached the whole log of test.

 

Would you please help to check the issue?

 

Thanks,

Zhantao

0 件の賞賛
返信
12 返答(返信)

4,909件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @hittzt 

Thanks for your reply.

If still issues found in your newly generated project, thanks for sharing the full log/reproducing steps for it, I could directly work on debugging it.

 

BR

Chenyin

0 件の賞賛
返信

4,960件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @hittzt 

Thanks for the reply,

May I know if the same "bl2_w_dtb.s32-qspi-sdk" is used in your continuous tests? how many tests made? What is the proportion of failure cases?

 

BR

Chenyin

0 件の賞賛
返信

4,920件の閲覧回数
hittzt
Senior Contributor I

Yes, I used the same bl2 binary for about 5 times, it failed in last test, then I saved the failure message.

I will created a totally new BSP43 project to test again.

 

Thanks,

Zhantao

0 件の賞賛
返信

4,986件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @hittzt 

You are welcome.

Sorry that I do not find issues during several times tests on it, when I am willing to checking your log but found that the log you mentioned seems not attached?

 

BR
Chenyin

0 件の賞賛
返信

4,968件の閲覧回数
hittzt
Senior Contributor I

Oh, the log is attached now.

 

Thanks,

Zhantao

0 件の賞賛
返信

5,067件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @hittzt 

Thanks for you confirmation.

Regarding to flashcp, from BSP UM, it is suggested using the script included in the rootfs, and actually mtd_debug is used, I suggest checking if there are implementation differences between the two applications.(mtd_debug and flashcp)

So currently there is no issue for secure boot itself? sorry I did not reproduce the issue you mentioned from my side(After secure boot, power off and power on).

 

BR

Chenyin

0 件の賞賛
返信

5,000件の閲覧回数
hittzt
Senior Contributor I

Hi @chenyin_h,

 

Sorry for reply so late.

I tested the case several times again, recently, and the result is that, most success, but failure also happened.

The failure log is attached.

 

Thanks,

Zhantao

0 件の賞賛
返信

5,127件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @hittzt 

Thanks for the reply.

My logs attached for your reference.

 

BR

Chenyin

 

 

0 件の賞賛
返信

5,094件の閲覧回数
hittzt
Senior Contributor I

Hi @chenyin_h,

 

Thanks for your log, it is helpful.

 

And did you try to test the case by using linux command flashcp to write the flash and enable the secure boot?

As the original log I attached, it failed when I write the flash using flashcp command, so I want to find the reason.

And I tested the case using your steps, and the secure boot passed indeed, but when I tried to power down and power up the board after, it hang there without nothing messages.

And I am still working on it to find the reason.

 

Thanks,

Zhantao

タグ(1)
0 件の賞賛
返信

5,141件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @hittzt 

Sorry for the delay.

I tested it on local board and it seems correct, would you mind checking the following steps:

1. Build the images by adding secboot to the conf/local.conf

2. Use the mtd write command under u-boot to update the bl2_w_dtb.s32-qspi that built from Yocto

3. When using hse-secboot to enable secure boot, just copy 3 files needed from Yocto build to the board, then run the hse-secboot.

 

BR

Chenyin

 

 

0 件の賞賛
返信

5,136件の閲覧回数
hittzt
Senior Contributor I

Hi @chenyin_h ,

 

Thanks for your reply.

Yes, I add the secboot feature in my conf/local.conf, and the test steps as I attached previously. Could you please use my steps to check it again and give your whole log, then I can compare the differences.

And I will test it with your steps to see the status again.

 

Thanks,

Zhantao

0 件の賞賛
返信

5,165件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @hittzt 

Thanks for the post.

I will check it on my side, and will update you later if any findings made

 

BR

Chenyin

0 件の賞賛
返信