Pytorch and Tensorflow on S32G- GoldVip

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Pytorch and Tensorflow on S32G- GoldVip

2,471 Views
Balakrishna971
Contributor II

Hi Team,

I want to run my ML model on Goldbox, I see that Goldvip has a library available eIQ Auto which provides the Pytorch/Keras 2.x which internally uses the Tensorflow, please help me to understand where these libraries are available and how to enable them in my development of ML model deployment. 

 

Thanks,

Bala

0 Kudos
Reply
4 Replies

2,418 Views
gergely-simon
NXP Employee
NXP Employee

Hi Bala and Daniel,

If you have any technical queries on this topic, I am happy to follow-up here, just let me know the details of any potential issue.

Thanks,

Gergely

0 Kudos
Reply

2,454 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

The eIQ package is available under the "Automotive Software Package Manager" either on the S32G3 product page (link: S32G3 Safe and Secure Vehicle Network Processor | NXP Semiconductors) or the S32G2 one. Given it is a "Premium Software" and requires an NDA, you need to contact your NXP sales representative for them to follow the needed process to give you access.

Please, let us know.

0 Kudos
Reply

2,452 Views
Balakrishna971
Contributor II

Thanks for the response. Does Goldvip need this NDA to enable the premium software? There are few sample demos like battery management system which uses the ML prediction.  I'm just wondering how this is running and I hop, if I want to run a new model all the required libraries must be available in Goldvip right?

0 Kudos
Reply

2,450 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Some files are provided as pre-compiled binaries, which do not require access to the libraries/packages.

Not all of GoldVIP packages are under NDA, and those who are, you could still not have access to the Premium Software, due to some of them having extra cost. This will be told to you by your NXP sales.

If you want access to the eIQ package itself, this is under NDA and is a Premium Software, for which contacting your NXP sales is the correct step.

Please, let us know.

0 Kudos
Reply